Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Differential routing / meander issues
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 7 replies
  • Subscribers 189 subscribers
  • Views 2613 views
  • Users 0 members are here
  • eagle
  • meander
Related

Differential routing / meander issues

e14 Contributor
e14 Contributor over 11 years ago

I'm trying to use the Meander function to route a differential pair. The pair is named D7_P and D7_N. Using the "run length d7*" command I can see that one trace is 234 mm long and one trace is 238 mm long. I use the command "meander 238mm" and select the pair. I click on either P and N and the move the mouse so both traces meander until the percents read "100.0% 100.0%." However, as is obvious from what the traces are doing and confirmed by "run length d7*" the wrong trace is being extended. The result of the new "run length d7*" is now something like 241 and 252 - the meander made the difference BIGGER!

 

So, am I doing something obviously wrong? I will say that I do have some intermediate pads involves (i.e. this is USB and there is an ESD chip connected to both traces). Does this screw things up? Is this just something I have to wing by hand? Please help!

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    I have read all of the posts, so I will re-phrase my question: I have a differential pair, D_N and D_P. Eagle recognizes them as a differential pair and routed them as a pair. "run length d*" shows the length difference is 4mm and tells me that the longer of the two wires is 240mm. HOWEVER when I execute "meander 240mm" BOTH traces are meandered. I cannot "meander ("increase") the length of the trace that is shorter alone." I cannot simply "increase the length of one trace" because it won't let me. And the final insult is that Eagle, in meandering / increasing the length of both traces, makes the longer trace "extra long" because it appears to have their lengths / ratios backwards. This is the main issue for me: the output of Meander 240 is NOT a pair with the same length.

     

    I can post a picture of what is happening if it would help. If there is an easy way to tell eagle "meander just one trace of a differential pair" I would use that immediately. I can't figure out how to route just one trace. And when Eagle helpfully does both it adds extra length to the _wrong_ trace.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    I have read all of the posts, so I will re-phrase my question: I have a differential pair, D_N and D_P. Eagle recognizes them as a differential pair and routed them as a pair. "run length d*" shows the length difference is 4mm and tells me that the longer of the two wires is 240mm. HOWEVER when I execute "meander 240mm" BOTH traces are meandered. I cannot "meander ("increase") the length of the trace that is shorter alone." I cannot simply "increase the length of one trace" because it won't let me. And the final insult is that Eagle, in meandering / increasing the length of both traces, makes the longer trace "extra long" because it appears to have their lengths / ratios backwards. This is the main issue for me: the output of Meander 240 is NOT a pair with the same length.

     

    I can post a picture of what is happening if it would help. If there is an easy way to tell eagle "meander just one trace of a differential pair" I would use that immediately. I can't figure out how to route just one trace. And when Eagle helpfully does both it adds extra length to the _wrong_ trace.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • clem57
    0 clem57 over 11 years ago in reply to e14 Contributor

    A picture would help.