EAGLE User Support (English) bottom smd pads
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
  • State Verified Answer
  • Replies 10 replies
  • Answers 1 answer
  • Subscribers 181 subscribers
  • Views 1306 views
  • Users 0 members are here
  • smd
  • libary
Related

bottom smd pads

Former Member
Former Member over 10 years ago

Hallo,

 

I try to create a SMD package by a script. It is a edge mounted connector, so it has SMD pads both on top and bottom.

SMD '1' 2 0.5 R90 (-3 -1); works perfect,

but

SMD '2' 2 0.5 MR90 (-3 -1); works not - the mirrow flag will not work in the SMD command, as described in HELP. But when i use INFO, I can set the mirrow flag.

Pressing the middle mouse button change the layer, but do not set the mirrow flag. What must I do to change the layer in a script?

 

I'm using eagle 6.5 - but @7.2 it is the same.

 

best regards

Marc

  • Sign in to reply
  • Cancel

Top Replies

  • Former Member
    Former Member over 10 years ago +1
    Thanks that's working
Parents
  • Former Member
    0 Former Member over 10 years ago

    Thanks that's working image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 10 years ago in reply to Former Member

    grid mm;

    smd

    layer 16

    smd 1 0.5 R90 '1'(0 0)

    layer 1

    smd 2 0.5 R90 '2'(0 0)

    ...

     

    I tried this, too. But for testing by copying in the command line:

    layer 16; smd 1 0.5 R90 '1' (0 0); layer 1; smd 2 0.5 R90 '2' (0 0);

    ... but it's not working image

     

    In a script it works! image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 10 years ago in reply to Former Member

    On 18/05/2015 6:53 p.m., Marc Wunschmann wrote:

    grid mm;

    smd

    layer 16

    smd 1 0.5 R90 '1'(0 0)

    layer 1

    smd 2 0.5 R90 '2'(0 0)

    ..

     

    I tried this, too. But for testing by copying in the command line:

    layer 16; smd 1 0.5 R90 '1' (0 0); layer 1; smd 2 0.5 R90 '2' (0 0);

    .. but it's not working image

     

    In a script it works! image

     

    You would be forgiven for thinking that scripts are simply a file

    version of what you would otherwise type at the control line. There are

    many subtitle differences with scripts. They will do what you can type

    at the control line but there is additional functionality and behaviour

    that a script affords when running. It is needed and a number of the

    ULPs depend these differences to function.

     

    HTH

    Warren

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • autodeskguest
    0 autodeskguest over 10 years ago in reply to Former Member

    On 18/05/2015 6:53 p.m., Marc Wunschmann wrote:

    grid mm;

    smd

    layer 16

    smd 1 0.5 R90 '1'(0 0)

    layer 1

    smd 2 0.5 R90 '2'(0 0)

    ..

     

    I tried this, too. But for testing by copying in the command line:

    layer 16; smd 1 0.5 R90 '1' (0 0); layer 1; smd 2 0.5 R90 '2' (0 0);

    .. but it's not working image

     

    In a script it works! image

     

    You would be forgiven for thinking that scripts are simply a file

    version of what you would otherwise type at the control line. There are

    many subtitle differences with scripts. They will do what you can type

    at the control line but there is additional functionality and behaviour

    that a script affords when running. It is needed and a number of the

    ULPs depend these differences to function.

     

    HTH

    Warren