EAGLE User Support (English) bottom smd pads
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
  • State Verified Answer
  • Replies 10 replies
  • Answers 1 answer
  • Subscribers 180 subscribers
  • Views 1298 views
  • Users 0 members are here
  • smd
  • libary
Related

bottom smd pads

Former Member
Former Member over 10 years ago

Hallo,

 

I try to create a SMD package by a script. It is a edge mounted connector, so it has SMD pads both on top and bottom.

SMD '1' 2 0.5 R90 (-3 -1); works perfect,

but

SMD '2' 2 0.5 MR90 (-3 -1); works not - the mirrow flag will not work in the SMD command, as described in HELP. But when i use INFO, I can set the mirrow flag.

Pressing the middle mouse button change the layer, but do not set the mirrow flag. What must I do to change the layer in a script?

 

I'm using eagle 6.5 - but @7.2 it is the same.

 

best regards

Marc

  • Sign in to reply
  • Cancel

Top Replies

  • Former Member
    Former Member over 10 years ago +1
    Thanks that's working
Parents
  • autodeskguest
    0 autodeskguest over 10 years ago

    On 13/05/15 14:35, Marc Wunschmann wrote:

    Hallo,

     

    I try to create a SMD package by a script. It is a edge mounted

    connector, so it has SMD pads both on top and bottom.

    SMD '1' 2 0.5 R90 (-3 -1); works perfect,

    but

    SMD '2' 2 0.5 MR90 (-3 -1); works not - the mirrow flag will not work in

    the SMD command, as described in HELP. But when i use INFO, I can set

    the mirrow flag.

     

    Indeed. However, there is another way:

     

    SMD '2' 2 0.5 R90 (-3 -1);

    MIRROR (-3 -1);

    SMD '1' 2 0.5 R90 (-3 -1);

     

    If you have the pads at the same coordinates on both sides then you will

    need to place the bottom side pads first, mirror them, then place the

    top side.

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • autodeskguest
    0 autodeskguest over 10 years ago

    On 13/05/15 14:35, Marc Wunschmann wrote:

    Hallo,

     

    I try to create a SMD package by a script. It is a edge mounted

    connector, so it has SMD pads both on top and bottom.

    SMD '1' 2 0.5 R90 (-3 -1); works perfect,

    but

    SMD '2' 2 0.5 MR90 (-3 -1); works not - the mirrow flag will not work in

    the SMD command, as described in HELP. But when i use INFO, I can set

    the mirrow flag.

     

    Indeed. However, there is another way:

     

    SMD '2' 2 0.5 R90 (-3 -1);

    MIRROR (-3 -1);

    SMD '1' 2 0.5 R90 (-3 -1);

     

    If you have the pads at the same coordinates on both sides then you will

    need to place the bottom side pads first, mirror them, then place the

    top side.

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer