EAGLE User Support (English) bottom smd pads
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
  • State Verified Answer
  • Replies 10 replies
  • Answers 1 answer
  • Subscribers 180 subscribers
  • Views 1296 views
  • Users 0 members are here
  • smd
  • libary
Related

bottom smd pads

Former Member
Former Member over 10 years ago

Hallo,

 

I try to create a SMD package by a script. It is a edge mounted connector, so it has SMD pads both on top and bottom.

SMD '1' 2 0.5 R90 (-3 -1); works perfect,

but

SMD '2' 2 0.5 MR90 (-3 -1); works not - the mirrow flag will not work in the SMD command, as described in HELP. But when i use INFO, I can set the mirrow flag.

Pressing the middle mouse button change the layer, but do not set the mirrow flag. What must I do to change the layer in a script?

 

I'm using eagle 6.5 - but @7.2 it is the same.

 

best regards

Marc

  • Sign in to reply
  • Cancel

Top Replies

  • Former Member
    Former Member over 10 years ago +1
    Thanks that's working
Parents
  • Former Member
    0 Former Member over 10 years ago

    Am 13.05.2015 um 15:35 schrieb Marc Wunschmann:

    Hallo,

     

    I try to create a SMD package by a script. It is a edge mounted

    connector, so it has SMD pads both on top and bottom.

    SMD '1' 2 0.5 R90 (-3 -1); works perfect,

    but

    SMD '2' 2 0.5 MR90 (-3 -1); works not - the mirrow flag will not work in

    the SMD command, as described in HELP. But when i use INFO, I can set

    the mirrow flag.

    Pressing the middle mouse button change the layer, but do not set the

    mirrow flag. What must I do to change the layer in a script?

     

    I'm using eagle 6.5 - but @7.2 it is the same.

     

    best regards

    Marc

     

     

    HELP SMD -->>  The orientation (see description in ADD) may be any angle

    in the range R0...R359.9. The S and M flags can't be used here.

                                     =====================================

     

    You must use:

    SMD 2 0.5 R90 '2' (-3 -1);

    CHANGE LAYER 16 (-3 -1);

     

     

    ***

    Um das Original zu lesen, und auch zuverlässig angehängte Dateien

    bereitstellen zu können, benutzen Sie news.cadsoft.de und einen

    funktionierenden News-Reader wie Thunderbird!

    ***

    Mit freundlichen Grüßen / Best regards

     

    Alfred Zaffran

    --

    ______________________________________________________________

    Alfred Zaffran              Support

    CadSoft Computer GmbH       Hotline:   08635-698930

    Pleidolfweg 15              FAX:       08635-698940

    84568 Pleiskirchen          eMail: <alf@cadsoft.de>

                                 Web:   <www.cadsoft.de>

    Registergericht: Amtsgericht Traunstein HRB 5573

    Geschaeftsfuehrer: Mark Whiteling

    ______________________________________________________________

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 10 years ago

    Am 13.05.2015 um 15:35 schrieb Marc Wunschmann:

    Hallo,

     

    I try to create a SMD package by a script. It is a edge mounted

    connector, so it has SMD pads both on top and bottom.

    SMD '1' 2 0.5 R90 (-3 -1); works perfect,

    but

    SMD '2' 2 0.5 MR90 (-3 -1); works not - the mirrow flag will not work in

    the SMD command, as described in HELP. But when i use INFO, I can set

    the mirrow flag.

    Pressing the middle mouse button change the layer, but do not set the

    mirrow flag. What must I do to change the layer in a script?

     

    I'm using eagle 6.5 - but @7.2 it is the same.

     

    best regards

    Marc

     

     

    HELP SMD -->>  The orientation (see description in ADD) may be any angle

    in the range R0...R359.9. The S and M flags can't be used here.

                                     =====================================

     

    You must use:

    SMD 2 0.5 R90 '2' (-3 -1);

    CHANGE LAYER 16 (-3 -1);

     

     

    ***

    Um das Original zu lesen, und auch zuverlässig angehängte Dateien

    bereitstellen zu können, benutzen Sie news.cadsoft.de und einen

    funktionierenden News-Reader wie Thunderbird!

    ***

    Mit freundlichen Grüßen / Best regards

     

    Alfred Zaffran

    --

    ______________________________________________________________

    Alfred Zaffran              Support

    CadSoft Computer GmbH       Hotline:   08635-698930

    Pleidolfweg 15              FAX:       08635-698940

    84568 Pleiskirchen          eMail: <alf@cadsoft.de>

                                 Web:   <www.cadsoft.de>

    Registergericht: Amtsgericht Traunstein HRB 5573

    Geschaeftsfuehrer: Mark Whiteling

    ______________________________________________________________

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Former Member
    0 Former Member over 10 years ago in reply to Former Member

    Thanks @all for the answers!!!!

    I have only one question left. Why has the SMD pad a "mirrow flag" which I only can see and modify by INFO?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 10 years ago in reply to Former Member

    To move a chip from one side of the board to the other!

    C