Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) What are the displayable attributes for a symbol ?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 7 replies
  • Subscribers 188 subscribers
  • Views 2854 views
  • Users 0 members are here
  • attributes
  • schematic
  • question
Related

What are the displayable attributes for a symbol ?

e14 Contributor
e14 Contributor over 11 years ago

Of course we can display >NAME and >VALUE on a schematic.

BUT are there other attributes that can be made displayed ?

... and if yes, what are their name ? Or is it as simple as using the attribute name used in a device (I fear it is not) ?

Thanks for any suggestion or how-to.

Jacques

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    0 autodeskguest over 11 years ago

    Hi!

     

    It's all in the documentation: HELP TEXT

     

    Rene

     

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 11 years ago in reply to autodeskguest
    >NAMEComponent name (ev.+gate name) 1)
    >VALUEComp. value/type 1)
    >PARTComponent name 2)
    >GATEGate name 2)
    >DRAWING_NAMEDrawing name
    >LAST_DATE_TIMETime of the last modification
    >PLOT_DATE_TIMETime of the plot creation
    >SHEETSheet number of schematic 3)
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 11 years ago in reply to clem57

    Hello,

     

    you should have added a note that this is not the complete list.

     

    Rene

     

     

    Am 14.05.2015 um 12:56 schrieb Clem Martins:

    | >NAME | Component name (ev.+gate name) 1) |

    | >VALUE | Comp. value/type 1) |

    | >PART | Component name 2) |

    | >GATE | Gate name 2) |

    | >DRAWING_NAME | Drawing name |

    | >LAST_DATE_TIME | Time of the last modification |

    | >PLOT_DATE_TIME | Time of the plot creation |

    | >SHEET | Sheet number of schematic 3) |

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/149769

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • kikoun
    0 kikoun over 11 years ago in reply to autodeskguest

    hi,

    You can also display your own personal attribute. If you define a attribute named 'ABC' in your device, then the text '>ABC' in your symbol (also work for your package) will display the value of the ABC attribute, even if the value is set in the schematic. You can have different display option see 'help text':

     

    If a symbol or package drawing shall display an attribute of the actual part or element, a text with the name of that attribute, marked with the '>' character, can be used. By default, only the actual value of the given attribute will be displayed. If the attribute name is followed by one of the special characters '=', '~' or '!', the actual display is as follows:

     

    >ABC

    123

    >ABC=

    ABC = 123

    >ABC~

    ABC

    >ABC!

    nothing

    Note that for each attribute name there should be only one such text in any given symbol or package! If there is more than one such text in a symbol or package that all reference the same attribute name, only one of them will be displayed when the part using this symbol or package is smashed.

     

    Note that you also can use that with global attributes. For example, I define a global attribute with a PCB reference number named 'GLOB_PCB_REFNUM'. I use some symbols a packages in which I put a '>GLOB_PCB_REFNUM' text. One of them is a package I made to add some text information on all Gerber layer.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • kikoun
    0 kikoun over 11 years ago in reply to autodeskguest

    hi,

    You can also display your own personal attribute. If you define a attribute named 'ABC' in your device, then the text '>ABC' in your symbol (also work for your package) will display the value of the ABC attribute, even if the value is set in the schematic. You can have different display option see 'help text':

     

    If a symbol or package drawing shall display an attribute of the actual part or element, a text with the name of that attribute, marked with the '>' character, can be used. By default, only the actual value of the given attribute will be displayed. If the attribute name is followed by one of the special characters '=', '~' or '!', the actual display is as follows:

     

    >ABC

    123

    >ABC=

    ABC = 123

    >ABC~

    ABC

    >ABC!

    nothing

    Note that for each attribute name there should be only one such text in any given symbol or package! If there is more than one such text in a symbol or package that all reference the same attribute name, only one of them will be displayed when the part using this symbol or package is smashed.

     

    Note that you also can use that with global attributes. For example, I define a global attribute with a PCB reference number named 'GLOB_PCB_REFNUM'. I use some symbols a packages in which I put a '>GLOB_PCB_REFNUM' text. One of them is a package I made to add some text information on all Gerber layer.