EAGLE User Support (English) Exported .drl file same drill size problem
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
  • State Not Answered
  • Replies 0 replies
  • Subscribers 177 subscribers
  • Views 279 views
  • Users 0 members are here
Related

Exported .drl file same drill size problem

Former Member
Former Member over 10 years ago

Hi.. I'm trying to export the .drl file but the factory said the drill are all the same size..

 

Trying to view the file and import it into 350CAM it says "tool numbers with no site: 1,2,3,4,5,6,7,8,9,10,11

 

 

The strange is... When I open the drillcfg.ulp file, choose mm it returns:

T01 0.50mm

T02 0.60mm

T03 0.61mm

T04 0.70mm

T05 0.80mm

T06 0.81mm

T07 1.00mm

T08 1.10mm

T09 1.12mm

T10 1.20mm

T11 3.20mm

 

 

But when it export the  drl file and import into CAM350 it return the "no size" error.

 

 

Does anybody know now to solve it?

 

Thank you a lot.