EAGLE User Support (English) Make ULP exit in the Board window with a desired tool selected?
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
  • State Not Answered
  • Replies 10 replies
  • Subscribers 179 subscribers
  • Views 1005 views
  • Users 0 members are here
Related

Make ULP exit in the Board window with a desired tool selected?

hbridge99
hbridge99 over 10 years ago

Hi EagleCAD support,

 

 

1) In a ulp or script, where does the program end up after  running the exit() script?

 

2) Is there some logic to this I am missing?

 

3) Is there a way in a ulp/script to return to the board (or schematic) window with a specified tool selected.

 

4) Can you point me to the very latest scripting and user language guides?

 

5 Is there a reason these guides are not in the docs folder?

 

hbridge99

  • Sign in to reply
  • Cancel

Top Replies

  • autodeskguest
    autodeskguest over 10 years ago in reply to hbridge99 +1
    On 20/06/2015 10:03 a.m., Paul Badger wrote: The window still doesn't activate though. Is there a way to change the focus to the board? It's really weird - it sets the tools correctly but without activating…
  • hbridge99
    hbridge99 over 10 years ago in reply to autodeskguest +1
    OSX 10.9.5 I notice other people are complaining about OSX graphics issues in 10.9, 10.10. Thanks for the help. I'm signing off this issue. In the grand scheme of all the things that are awkward, missing…
Parents
  • autodeskguest
    0 autodeskguest over 10 years ago

    Paul Badger wrote on Fri, 19 June 2015 10:03

    Hi EagleCAD support,

     

     

    1) In a ulp or script, where does the program end up after  running

    the

    exit() script?

     

    2) Is there some logic to this I am missing?

     

    3) Is there a way in a ulp/script to return to the board (or

    schematic)

    window with a specified tool selected.

     

    4) Can you point me to the very latest scripting and user language

    guides?

     

    5 Is there a reason these guides are not in the docs folder?

     

    hbridge99

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/153052

     

     

    1. The script will run to its end if no problems are encountered. So it

    will end up where you code it to. If you want to start a ulp in the borad

    editor and end up in the schematic editor, for example, you can do that.

     

    2. Maybe missing knowledge.

     

    3. Sure, generally leaving the semi colon off the end of a command will

    keep that command active. End your ulp with exit("move") and the move

    command will be active.

     

    4. These are extracted from the HELP on occasions by Richard H so you don't

    need then really. They contain only the info that is in the HELP. A new

    version is only needed when a new Eagle version has had a change to the

    User Language. Check the release notes to get an indication of how often

    that happens

     

    5. Up to Cadsoft to decide if more is desirable there. Personally I would

    never use it but it may bring comfort to those starting out and feel they

    would like a pdf version of the User Language section  in the HELP.

     

    The best thing to do is study the simple examples that come with Eagle.

     

    All the best

    Warren

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • autodeskguest
    0 autodeskguest over 10 years ago

    Paul Badger wrote on Fri, 19 June 2015 10:03

    Hi EagleCAD support,

     

     

    1) In a ulp or script, where does the program end up after  running

    the

    exit() script?

     

    2) Is there some logic to this I am missing?

     

    3) Is there a way in a ulp/script to return to the board (or

    schematic)

    window with a specified tool selected.

     

    4) Can you point me to the very latest scripting and user language

    guides?

     

    5 Is there a reason these guides are not in the docs folder?

     

    hbridge99

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/153052

     

     

    1. The script will run to its end if no problems are encountered. So it

    will end up where you code it to. If you want to start a ulp in the borad

    editor and end up in the schematic editor, for example, you can do that.

     

    2. Maybe missing knowledge.

     

    3. Sure, generally leaving the semi colon off the end of a command will

    keep that command active. End your ulp with exit("move") and the move

    command will be active.

     

    4. These are extracted from the HELP on occasions by Richard H so you don't

    need then really. They contain only the info that is in the HELP. A new

    version is only needed when a new Eagle version has had a change to the

    User Language. Check the release notes to get an indication of how often

    that happens

     

    5. Up to Cadsoft to decide if more is desirable there. Personally I would

    never use it but it may bring comfort to those starting out and feel they

    would like a pdf version of the User Language section  in the HELP.

     

    The best thing to do is study the simple examples that come with Eagle.

     

    All the best

    Warren

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.