EAGLE User Support (English) Reaching parts in ulp
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
  • State Suggested Answer
  • Replies 2 replies
  • Answers 1 answer
  • Subscribers 179 subscribers
  • Views 426 views
  • Users 0 members are here
  • ulp
  • attribute
Related

Reaching parts in ulp

electrodevab
electrodevab over 10 years ago

Hi,

 

I am trying to write an ulp but ran into trouble.

 

Currently in the ULP I have an array containing strings with component names from the schematic. (compArray[i])

 

In my ULP I need to go into these (in the array) components and add attributes with a predefined name and value. How do I access each component and its property to add the attrubutes?

 

Have a nice day,

 

Best regards,

Tomas Bergh

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    0 autodeskguest over 10 years ago

    On 24.06.2015 08:15, Tomas Bergh wrote:

    Hi,

     

    I am trying to write an ulp but ran into trouble.

     

    Currently in the ULP I have an array containing strings with component

    names from the schematic. (compArray[i])

     

    In my ULP I need to go into these (in the array) components and add

    attributes with a predefined name and value. How do I access each

    component and its property to add the attrubutes?

     

    ULP can only do read only functions on the design, but it can exit with

    a string containing commands, so you simple have to build a large string

    with all the commands that is required to change the attributes, and at

    the end of the ULP, pass the commands with the function exit(string).

    For multiple commands, separate them with semicolon.

     

    I usually build a command array and exit(strjoin(commands,';'));

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • electrodevab
    0 electrodevab over 10 years ago in reply to autodeskguest

    Thank you!

    It seems like this is a feasible way for getting around the first issue.

    Unfortunately Eagle is expecting a mouseclick (for placing the visible attribute) after using the attribute command (ex. attribute R100 attribName attribValue)

    In my code I used this: commands[i] = "attribute" + " " + compArray[i] + " " + attribName + " " + attribValue)

    So I am stuck here again. It also seems like that the attribute is visible by default.

    Best regards,

    Tomas Bergh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • electrodevab
    0 electrodevab over 10 years ago in reply to autodeskguest

    Thank you!

    It seems like this is a feasible way for getting around the first issue.

    Unfortunately Eagle is expecting a mouseclick (for placing the visible attribute) after using the attribute command (ex. attribute R100 attribName attribValue)

    In my code I used this: commands[i] = "attribute" + " " + compArray[i] + " " + attribName + " " + attribValue)

    So I am stuck here again. It also seems like that the attribute is visible by default.

    Best regards,

    Tomas Bergh