EAGLE User Support (English) How to check drill sizes in mm (production board)
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
  • Replies 4 replies
  • Subscribers 179 subscribers
  • Views 1572 views
  • Users 0 members are here
Related

How to check drill sizes in mm (production board)

autodeskguest
autodeskguest over 16 years ago

I have a design I've created and I would like

to send my first one off for production .

 

So I need to be able to check what the drill

sizes are prior to Gerber / Excellon file production.

 

Is there a simple way to force only three drill

sizes e.g. 0.3mm vias, 0.8mm pads, 1.0mm

for connector blocks - this is to cut down the

price of course.

 

How do I do this from the board file ??

 

Florian

 

 

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 16 years ago

    I'll defer to experts in this area, but I have this idea...

    To get prototypes made with a minimum number of drill sizes, I suspect the "T" codes can be changed. In the Excellon (.drd) file, there are X-Y coordinates grouped by drill sizes. For example:

     

    T01

    X43888Y23435

    X48808Y22915

     

    At the front of the Excellon file are the T01, T01... definitions. For example:

     

    T01C0.0120

    T02C0.0240

    T03C0.0320

    T04C0.0400

    T05C0.0500

     

    In the "Drill Station Info File" (.dri) is information about the T01, T02... in plain English (or German, I suspect). For Example:

     

    Drills used:

     

    Code  Size       used

     

    T01   0.0120inch   145

    T02   0.0240inch     8

    T03   0.0320inch    26

    T04   0.0400inch    50

    T05   0.0500inch     1

     

    So I suspect the Excellon file can be edited (in a plain text editor) to change the drill sizes. Hence in my example, the .032 may be changed to .040 and T03 becomes "T03C0.0400" in the Excellon file.

     

    If you try this with a board house, let us know if it works.

     

    --

    Jeff Rockel

    WI, USA

    --

    Browser access to CadSoft Support Forums at http://www.eaglecentral.ca

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 16 years ago

    I'll defer to experts in this area, but I have this idea...

    To get prototypes made with a minimum number of drill sizes, I suspect the "T" codes can be changed. In the Excellon (.drd) file, there are X-Y coordinates grouped by drill sizes. For example:

     

    T01

    X43888Y23435

    X48808Y22915

     

    At the front of the Excellon file are the T01, T01... definitions. For example:

     

    T01C0.0120

    T02C0.0240

    T03C0.0320

    T04C0.0400

    T05C0.0500

     

    In the "Drill Station Info File" (.dri) is information about the T01, T02... in plain English (or German, I suspect). For Example:

     

    Drills used:

     

    Code  Size       used

     

    T01   0.0120inch   145

    T02   0.0240inch     8

    T03   0.0320inch    26

    T04   0.0400inch    50

    T05   0.0500inch     1

     

    So I suspect the Excellon file can be edited (in a plain text editor) to change the drill sizes. Hence in my example, the .032 may be changed to .040 and T03 becomes "T03C0.0400" in the Excellon file.

     

    If you try this with a board house, let us know if it works.

     

    --

    Jeff Rockel

    WI, USA

    --

    Browser access to CadSoft Support Forums at http://www.eaglecentral.ca