EAGLE User Support (English) How to check drill sizes in mm (production board)
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
  • Replies 4 replies
  • Subscribers 179 subscribers
  • Views 1560 views
  • Users 0 members are here
Related

How to check drill sizes in mm (production board)

autodeskguest
autodeskguest over 16 years ago

I have a design I've created and I would like

to send my first one off for production .

 

So I need to be able to check what the drill

sizes are prior to Gerber / Excellon file production.

 

Is there a simple way to force only three drill

sizes e.g. 0.3mm vias, 0.8mm pads, 1.0mm

for connector blocks - this is to cut down the

price of course.

 

How do I do this from the board file ??

 

Florian

 

 

 

  • Sign in to reply
  • Cancel
Parents
  • Richard_H
    Richard_H over 16 years ago

    Jeff rockel schrieb:

    I'll defer to experts in this area, but I have this idea...

    To get prototypes made with a minimum number of drill sizes, I suspect

    the "T" codes can be changed. In the Excellon (.drd) file, there are X-Y

    coordinates grouped by drill sizes. For example:

     

    T01

    X43888Y23435

    X48808Y22915

     

    At the front of the Excellon file are the T01, T01... definitions. For

    example:

     

    T01C0.0120

    T02C0.0240

    T03C0.0320

    T04C0.0400

    T05C0.0500

     

    In the "Drill Station Info File" (.dri) is information about the T01,

    T02... in plain English (or German, I suspect). For Example:

     

    Drills used:

     

    Code  Size       used

     

    T01   0.0120inch   145

    T02   0.0240inch     8

    T03   0.0320inch    26

    T04   0.0400inch    50

    T05   0.0500inch     1

     

    So I suspect the Excellon file can be edited (in a plain text editor) to

    change the drill sizes. Hence in my example, the .032 may be changed to

    .040 and T03 becomes "T03C0.0400" in the Excellon file.

    If you try this with a board house, let us know if it works.

     

     

    This will work, but don't forget that the width of the copper

    ring around the drill hole will change!

     

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

    CadSoft Support -- hotline@cadsoft.de

    FAQ: http://www.cadsoft.de/faq.htm

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 16 years ago in reply to Richard_H

    On Thu, 23 Jul 2009 16:35:02 +0200, Richard Hammerl <ric@cadsoft.de>

    wrote:

     

    So I suspect the Excellon file can be edited (in a plain text editor) to

    change the drill sizes. Hence in my example, the .032 may be changed to

    .040 and T03 becomes "T03C0.0400" in the Excellon file.

    If you try this with a board house, let us know if it works.

     

     

    This will work, but don't forget that the width of the copper

    ring around the drill hole will change!

     

    So, it is probably safe to make any holes smaller, because that will

    only produce more of the copper ring.  But making the hole larger

    might make the copper ring dangerously small, or maybe even

    non-existent.

     

     

    Robert Scott

    Real-Time Specialties

    Ypsilanti, Michigan

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 16 years ago in reply to Richard_H

    On Thu, 23 Jul 2009 16:35:02 +0200, Richard Hammerl <ric@cadsoft.de>

    wrote:

     

    So I suspect the Excellon file can be edited (in a plain text editor) to

    change the drill sizes. Hence in my example, the .032 may be changed to

    .040 and T03 becomes "T03C0.0400" in the Excellon file.

    If you try this with a board house, let us know if it works.

     

     

    This will work, but don't forget that the width of the copper

    ring around the drill hole will change!

     

    So, it is probably safe to make any holes smaller, because that will

    only produce more of the copper ring.  But making the hole larger

    might make the copper ring dangerously small, or maybe even

    non-existent.

     

     

    Robert Scott

    Real-Time Specialties

    Ypsilanti, Michigan