EAGLE User Support (English) Rename 0-Length Wire Created by Symbol Pin on top of Another
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
  • Replies 1 reply
  • Subscribers 180 subscribers
  • Views 214 views
  • Users 0 members are here
Related

Rename 0-Length Wire Created by Symbol Pin on top of Another

autodeskguest
autodeskguest over 16 years ago

Hello,

 

I have a case where I need to rename a net from a command line.  Normally I can do that, but this net is actually auto created because the a pin of one symbol overlaps with a pin of another symbol.  So it's a zero length wire that you can only see if you move one of the symbols.

 

But I need to do this in a script and I can't figure out how to.  I tried turning off the symbol layer and then grouping the area, but it complains that it is an empty group even though there is a wire there of 0 length.

 

So how do I do this?  I need to assume that I don't know the name of that auto-generated net before hand for my solution.

 

FYI, EAGLE 5.6 on Mac is what I'm using in case there is a bug underneath this.

 

Cheers,

 

James.

--

James Morrison  ~~~  Stratford Digital

 

email:  james@eaglecentral.ca

web: http://www.eaglecentral.ca

 

Specialising in CadSoft EAGLE

  • Online Sales to North America

  • Electronic Design Services

  • EAGLE Enterprise Toolkit

--

Browser access to CadSoft Support Forums at http://www.eaglecentral.ca

 

  • Sign in to reply
  • Cancel
  • Richard_H
    Richard_H over 16 years ago

    James Morrison schrieb:

    Hello,

     

    I have a case where I need to rename a net from a command line.

    Normally I can do that, but this net is actually auto created because

    the a pin of one symbol overlaps with a pin of another symbol.  So it's

    a zero length wire that you can only see if you move one of the symbols.

     

    But I need to do this in a script and I can't figure out how to.  I

    tried turning off the symbol layer and then grouping the area, but it

    complains that it is an empty group even though there is a wire there of

    0 length.

     

    So how do I do this?  I need to assume that I don't know the name of

    that auto-generated net before hand for my solution.

     

    FYI, EAGLE 5.6 on Mac is what I'm using in case there is a bug

    underneath this.

     

    Cheers,

     

    James.

     

     

    If the pins are ending at the same position the net line is not

    reachable (as you already wrote). What you could do is to place a

    JUNCTION at this position first and then NAME the net.

     

    Maybe this helps?

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

    CadSoft Support -- hotline@cadsoft.de

    FAQ: http://www.cadsoft.de/faq.htm