EAGLE User Support (English) Symbol without package error
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
  • Replies 0 replies
  • Subscribers 179 subscribers
  • Views 120 views
  • Users 0 members are here
Related

Symbol without package error

Former Member
Former Member over 15 years ago

Hello

 

I'm very new at using Eagle.  I'm evaluating the software so we can use it

to do RF substrates and the like.  Right now I'm trying to convert a few

simple projects over to see how/if it will work for us.  One "problem" I've

had is this error I get while using a simple RF port.  The symbol is just a

marker to where the RF input is so it doesn't actually have a layout

(package) that goes with it.  I suppose it is similar to a ground but it's

not meant to connect to other RF ports that are used in the same schematic

like a ground or VCC would.  I can see other uses of an RF port tying them

to a coax connector or some such but in this case we are just using it as a

non-package reference.  Any help with this would be appreciated.

 

jom

--

Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.