EAGLE User Support (English) Re: Minor upgrades
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
  • Replies 0 replies
  • Subscribers 177 subscribers
  • Views 230 views
  • Users 0 members are here
Related

Re: Minor upgrades

Former Member
Former Member over 15 years ago

Am 18.12.2010 07:53, schrieb Eagle:

Il 26/04/2009 12:10, Marco Trapanese ha scritto:

>> Hello,

>>

>> the default install path of EAGLE is something like:

>>

>> C:\Program Files\EAGLE-5.3.0

>>

>> When I launch the setup of a newer version (e.g. the latest 5.5.0) it

>> wants to install to a different location, such as:

>>

>> C:\Program Files\EAGLE-5.5.0

>>

>>

>> Ok, I could uninstall the old version and then install the newer.

>> Otherwise I could use a generic path (e.g. C:\Program Files\EAGLE).

>>

>> But why CadSoft doesn't provide a simple upgrade utility?

>>

>> Marco

Same problem from 5.6 to 5.10 Wath suggest?

Osap

 

You can choose any place to install eagle, even over the existing

program. I would NOT want eagle to install a new version over my

existing one for a few reasons. The update may fail and spoil the

existing one or there is a new bug in it and there is hopefully a back

up. With a compare tool I can check easy for new libraries, ulps etc.

which is not possible if the update is just dumped over the existing one.

 

--

Mit freundlichen Grüßen / With best regards

 

Joern Paschedag