EAGLE User Support (English) Problem connecting Power Pads to GND polygon
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
  • Replies 7 replies
  • Subscribers 178 subscribers
  • Views 907 views
  • Users 0 members are here
Related

Problem connecting Power Pads to GND polygon

autodeskguest
autodeskguest over 16 years ago

I am designing a board that includes several kinds of ICs

with "Power Pads" under the IC package that need

to be grounded.  For some of the ICs, the GND polygon

connects to the Power Pad as it should.  For other

ICs, the GND polygon is not connecting to the Power Pad.

Examining the devices in the library, they appear to be

constructed and labeled the same way.  I can't see

a difference in labeling, pin declaration, or grounding

between the ones that connect to ground and the ones

that don't.

 

Can you suggest what might be different between the

ICs or the libraries to cause this?

 

Thank you,

--- Graham

 

==

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 16 years ago

    Is the polygon width set to a low number, like zero, to help it get into

    the spaces?

     

    also, maybe it should just be connected with a via( or as many vias as

    will fit in the pad) rather than trying to get in between the pads, it

    sounds like a thermal connection that needs a lot of copper to work

    properly.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 16 years ago

    Is the polygon width set to a low number, like zero, to help it get into

    the spaces?

     

    also, maybe it should just be connected with a via( or as many vias as

    will fit in the pad) rather than trying to get in between the pads, it

    sounds like a thermal connection that needs a lot of copper to work

    properly.