Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) how does one construct edge connectors?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 185 subscribers
  • Views 2265 views
  • Users 0 members are here
Related

how does one construct edge connectors?

autodeskguest
autodeskguest over 16 years ago

Is there a shortcut to making edge connectors on PC boards?  Or do I

have to just bite the bullet and draw the parts freehand?  If so how do

I add the lands/pads/copper to both sides?  This is for a board to be

pugged into a 15 pin edge connector.  See attachment.

 

Thanks,

Jim.

 

Attachments:
image
  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 16 years ago

    Paul Romanyszyn wrote:

    Jim Lynch wrote:

    Carsten wrote:

    Snip

    Hi!

     

    Learning by doing. That's the only way. image (The first one is the

    hardest, but it's done realy easy in eagle.

    You have to place SMD pads along the edge of the PCB, matching the

    contacts of your connector. The PCB has to be milled to fit into the

    connector. Next steps have to be discussed with the board house: How

    to draw the chamfering of the PCB edge. And if connector gold plating

    is required, ".

     

    Carsten

     

    OK so use SMD pads.  I guess I could build a component consisting of

    15 SMD pads so I could use it on more than one board.  I'm not sure I

    understand what you mean by "how the

    > additional traces to short all connector pins must look like".

     

    Can you explain it a little better?  I didn't think shorts were

    desirable.  image

     

    Thanks,

    Jim.

    If you are putting plating on the fingers depending on the process and

    material it may require the pins to be shorted together. This short will

    be removed when the bevel cut is done. ie Check with board house as to

    requirements.

    Ah, I understand.  Thanks.

     

    If you are going to be using a standard size card for future work it may

    be good to add the board outline and if required mounting holes to the

    part.

    I had toyed with that idea, do you save it in the library just like a

    component?

    Paul R.

     

    Jim.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 16 years ago

    Paul Romanyszyn wrote:

    Jim Lynch wrote:

    Carsten wrote:

    Snip

    Hi!

     

    Learning by doing. That's the only way. image (The first one is the

    hardest, but it's done realy easy in eagle.

    You have to place SMD pads along the edge of the PCB, matching the

    contacts of your connector. The PCB has to be milled to fit into the

    connector. Next steps have to be discussed with the board house: How

    to draw the chamfering of the PCB edge. And if connector gold plating

    is required, ".

     

    Carsten

     

    OK so use SMD pads.  I guess I could build a component consisting of

    15 SMD pads so I could use it on more than one board.  I'm not sure I

    understand what you mean by "how the

    > additional traces to short all connector pins must look like".

     

    Can you explain it a little better?  I didn't think shorts were

    desirable.  image

     

    Thanks,

    Jim.

    If you are putting plating on the fingers depending on the process and

    material it may require the pins to be shorted together. This short will

    be removed when the bevel cut is done. ie Check with board house as to

    requirements.

    Ah, I understand.  Thanks.

     

    If you are going to be using a standard size card for future work it may

    be good to add the board outline and if required mounting holes to the

    part.

    I had toyed with that idea, do you save it in the library just like a

    component?

    Paul R.

     

    Jim.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
No Data