Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Re: Package pad size different when placed   on PCB
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 188 subscribers
  • Views 330 views
  • Users 0 members are here
Related

Re: Package pad size different when placed   on PCB

autodeskguest
autodeskguest over 16 years ago

dingebre wrote on Thu, 18 March 2010 03:44

I got the package designed and had to use a "diameter" very close to

the "drill size" to keep adequate clearance for the pins.

 

But you also used oblong pads, which made the clearance problem worse.  It

looks like circular pads would help in this case.

 

Quote:

When I bring the package into the device editor window and onto the

PCB, the pad defaults back to the auto size and the mounting tab pads

overlap the pin pads. What am I doing wrong?

 

I'm guessing the DRC settings are overriding the library settings.  Make

sure the minimum width is set small enough to allow for this part, and that

restring and the like aren't overridden.  Somewhere there is a checkbox

called something like "From library" or "Use library settings".  Make sure

it's checked.

--

Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

 

  • Sign in to reply
  • Cancel
  • autodeskguest
    autodeskguest over 16 years ago in reply to e14 Contributor

    dingebre wrote on Thu, 18 March 2010 17:08

    Changing the pads to round solved the overlap problem, thanks. However,

    I never could find out how to override the restring settings for a single

    part and changing the restring parameters did not correct the overlap.

    maybe a bug?

     

    Highly unlikely.

     

    I just checked, and the override I was thinking about applies to pad

    shapes, not sizes.  I guess that makes sense as you can't have it both

    ways.  Either .008 (or whatever) is the minimum acceptable width or it

    isn't.  Note that you can set this per net with CLASS, and DRC enforces the

    minimums.

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 16 years ago in reply to e14 Contributor

    dingebre wrote on Thu, 18 March 2010 09:11

    Olin wrote on Thu, 18 March 2010 07:09

    dingebre wrote on Thu, 18 March 2010 03:44

    I got the package designed and had to use a "diameter" very

    close to the "drill size" to keep adequate clearance for the pins.

     

    But you also used oblong pads, which made the clearance problem

    worse.  It looks like circular pads would help in this case.

     

    Quote:

    When I bring the package into the device editor window and onto

    the PCB, the pad defaults back to the auto size and the mounting tab

    pads overlap the pin pads. What am I doing wrong?

     

    I'm guessing the DRC settings are overriding the library settings.

    Make sure the minimum width is set small enough to allow for this part,

    and that restring and the like aren't overridden.  Somewhere there is a

    checkbox called something like "From library" or "Use library

    settings".  Make sure it's checked.

     

    Thanks Olin. I was thinking the DRC rules were doing something, but the

    help file wasn't helping...

     

    David

     

     

    Hi Olin,

     

    Changing the pads to round solved the overlap problem, thanks. However, I

    never could find out how to override the restring settings for a single

    part and changing the restring parameters did not correct the overlap.

    maybe a bug?

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 16 years ago

    Olin wrote on Thu, 18 March 2010 07:09

    dingebre wrote on Thu, 18 March 2010 03:44

    I got the package designed and had to use a "diameter" very close

    to the "drill size" to keep adequate clearance for the pins.

     

    But you also used oblong pads, which made the clearance problem worse.

    It looks like circular pads would help in this case.

     

    Quote:

    When I bring the package into the device editor window and onto the

    PCB, the pad defaults back to the auto size and the mounting tab pads

    overlap the pin pads. What am I doing wrong?

     

    I'm guessing the DRC settings are overriding the library settings.

    Make sure the minimum width is set small enough to allow for this part,

    and that restring and the like aren't overridden.  Somewhere there is a

    checkbox called something like "From library" or "Use library settings".

    Make sure it's checked.

     

     

    Thanks Olin. I was thinking the DRC rules were doing something, but the

    help file wasn't helping...

     

    David

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.