Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Adding Sheets Re-ordering pages with finished   layout
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 179 subscribers
  • Views 742 views
  • Users 0 members are here
Related

Adding Sheets Re-ordering pages with finished   layout

autodeskguest
autodeskguest over 15 years ago

What:

This is the recipe for adding more sheets or re-ordering your existing

sheets for a project after you've already completed or done some layout.

 

Motivation:

I completed my first project that was faily complex with about 200

components and a torturous layout with nasty board dimensions.  Being an

Eagle noob I did it all on one schematic sheet.  On my second project, that

had even more components, I realized that printing out multiple sheets and

patch working them together sux, so I figured out Eagle's multi-page aspect

and am quite pleased with it and the results.

  But, looking back at the first third of the job I was disgusted with the

unprofessional single schematic page and decided to break it into multiple

pages.

 

As you know with Eagle's automatic updating of the layout, whenever things

change on the schematic - they change on the layout.  This process can be

highly destructive to an existing layout. It will rip up traces or

re-number parts.

 

Couple the cross annotation with the auto part numbering and havoc can

follow.

 

To pull this off successfully you need to follow this recipe.

 

 

Recipe:

1) Make one or two backups of your existing schematic and the board files.

Something like: ExistingNameHACK1 and ExistingNameHACK2.  Using "Save as"

 

2) After 1) above, you should be sitting on: "ExistingNameHACK2".

 

3) Close the existing board: "ExistingNameHACK2.brd".  This suspends the

the automatic updating, freezing your layout.

 

4) In the schematic you want to FILE>EXPORT>Partslist to

"ExistingNameHACK2.partslist"  Note where it lands.

 

5) Open "ExistingNameHACK2.partslist" in your favored editor.

 

6) Starting at the top of the partslist look at the "Part" column.  You

will see for instance C1,C2,C3......  If there are less than about 10 of a

type part, check them for all values being there - NONE can be missing. If

there are none missing move on down to the next type of "Part".  If there

is one part in the sequence missing then go onto the schematic and copy any

same-type part that you see to add another one.  This will fill in the

missing values.

 

Go down the partslist until these are all taken care of.  If there are more

than 10 values of a type of part, DO NOT trust your eye.  Just copy a

same-part adding it to the schematic.  Do this until you see the next added

part is numbered higher than the highest numbered one of the same type in

partslist.  Once you get one higher, UNDO and move down partslist to the

next Part.  Typically Resistors and Capacitors would certainly get the

blind - add treatment.  If the first add is a number higher than the

highest on partslist just UNDO and move on.

 

7) Now you likely have a little group of added parts on the schematic up it

some corner from 6).  Good, leave them there, never to mingle with the

rest.

 

8) Add as many pages as you think you'll need.  DRAW>FRAME putting in

frames, if you desire, on each of the new pages. I start them exactly on

the new page's X and run them out to half an inch of my printer's page size

Ex: (16.5" x 10.5"). This shows how much room you have to keep all the new

page's circuitry in your printer's paper size.

 

9) Look at your one page schematic and decide how you want to break it up

into a logical several pages.   Since this is just to fix a single page

situation don't knock off a nasty chunk that requires a bunch of signals

moving to multiple pages as it will be horribly tedious and easy to screw

up.

 

For example, you may want to move the displays to a new page and the power

supply to yet another page.

 

Move these areas into groups that you can hack out when you're ready.  Now

use the label command to label each signal that will span from the first

page to one of the new pages. Typically you will have a signal called, for

example, "N$37". On the same net add another label - it will be the same.

 

Cut the net somewhere convenient between the two labels.  Now, using the

"NAME" function rename both sides something descriptive like "CLK".

 

10) Repeat 9) until all nets that will be severed, to break up the monster

page, are done.

 

11) Now using Eagle's psychotic cut and paste method, GROUP>CUT>rightclick

on screen to save the sub-area we're moving into the paste buffer.  Now

'pick' the DELETE button and right click to delete the same GROUPed parts.

pffft! They're gone - existing only in the paste buffer.  Those preventing

renumbering of these parts when they're PASTEd.

 

12) Go to the new page and PASTE.  You now have the moved circuitry on the

new page - with no renumbering.

 

13) Repeat 9) thru 12) until you're satisfied with your newly broken-up

schematic.

 

14) Go back to the first page and blitz all the components you had to add

to fill the Part listings.  This prevented ANY renumbering.

 

15) This is a good time to SAVE.

 

16) Open up "ExistingNameHACK2.brd".  There will be squawking about "No

Annotation because their are inconsistencies!!!"  Fear not this is

expected.

 

17) What has happened is that traces on the board were all previously named

from the net names on the schematic.  Recall that we just put useful names

on the nets we had to cut to 'multi' the schematic.  The inconsistency is

that now the existing traces don't match the new names we just assigned.

 

On the schematic page run the ERC, the Electrical Rule Checker. You will

get a bunch of pretty lavender Consistency Errors.   You will immediately

see the new names you assigned paired up with the old net names still

residing on the layout's traces. "N$37", etc.,etc.

 

Minimize the schematic somewhere and move the ERC window to the side. Click

on an Inconsistency.  This boxes one pin on a contested trace on the board.

Again using NAME select the the PIN or Trace.  Looking at the ERC list

reNAME the trace to the name you recently gave the net on the schematic.

 

18) Repeat 17) until you've done all the inconsistencies.  If they're

listed twice you can ignore the second complaint. Once you've reNAMEd them

all run the ERC again.  There should be none!  If there is, just address

them.  Do this until there are none left.

 

19) Save.

 

20) Examine your layout. You should see no changes from the original.  If

this is the case you've been successful.  P A R T Y  T I M E!

 

You can Save as back to the original name or the original name with some

minor addition. "Multi" or *ms".

 

 

Caveat.  There is some aspect about Eagle and gates spread around different

sheets. I am too much a noob to know what ramifications this would have

with the above process.  Perhaps someone can add that.

 

 

 

 

--

Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

 

  • Sign in to reply
  • Cancel
  • kcadsoft
    kcadsoft over 15 years ago

    On 02.04.2010 23:30, Keith Cress wrote:

    What:

    This is the recipe for adding more sheets or re-ordering your existing

    sheets for a project after you've already completed or done some layout.

     

     

    Or, if you're using version 5, just move the selected group to the

    desired sheet image

    See "Help/Editor Commands/MOVE/Move part of a sheet to an other sheet".

     

    Klaus Schmidinger

    --

    _______________________________________________________________

     

    Klaus Schmidinger                       Phone: +49-8635-6989-10

    CadSoft Computer GmbH                   Fax:   +49-8635-6989-40

    Pleidolfweg 15                          Email:   kls@cadsoft.de

    D-84568 Pleiskirchen, Germany           URL:     www.cadsoft.de

    _______________________________________________________________

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 15 years ago

    Indeed!!!   :blush:

     

    Why didn't you tell me before I did it!!

     

    Sigh.. OK, well I gave the 'old school' method to provide historical

    validation for the V5 functional addition.

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.