EAGLE User Support (English) 5.8 Not Remembering Which Libraries Are In Use
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
  • Replies 4 replies
  • Subscribers 177 subscribers
  • Views 617 views
  • Users 0 members are here
Related

5.8 Not Remembering Which Libraries Are In Use

autodeskguest
autodeskguest over 15 years ago

Since upgrading to 5.8, Eagle doesn't seem to remember which of my

libraries I've selected as "Use"

 

I'm running Eagle on Mac OS X 10.6.3, and have some libraries local

("Applications/EAGLE/lbr/") and some libraries on a network share when

I'm at work. ("/Volumes/Network Drive/EAGLELibs/")

 

I can go through and "Use" libraries, quit Eagle, re-launch it and the

change doesn't stick.  Nothing in a folder greater than one level deep

(i.e. "lbr/5.8/19inch.lbr" will stay "Use"d and libraries.  Nothing one

level deep (i.e. "lbr/Nic.lbr") will stay de-"Use"d.

 

Where does Eagle store the list of libraries that are in use? Maybe I

could set things up and lock the file to stop Eagle buggering it up.

It's a royal pain to go through every folder and "Use all" again.  (Why

can't I make multiple selections in the list? Why does Eagle let me Use

libraries that are in old formats and it can't use?  Why isn't "Use all"

recursive? Why is the sort order some bizarre

folders-first-capitals-before-lower-case thing instead of alphabetical?)

 

In a related matter, when I boot Eagle without having the network share

mounted, it complains about missing include directories, and offers to

create them.  The default action is to create them, which would make

directories in the /Volumes/ directory.  This is bad behaviour -

creating directories in /Volumes means that when the network share is

mounted, the system either has to overwrite (potentially destroying user

data) or, as is the case, mount with a different path.  Eagle will then

be stuck silently pointing at the folder it created instead of the

network share.

 

Cheers,

Nic Jones,

Ocean Controls

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 15 years ago

    (comments in line)

     

    Jorge Garcia wrote:

    When you open EAGLE without a project and you create a new project by

    default all libraries will be available. However, if EAGLE opens with a

    project then it will first read the EAGLE.epf file checking which

    libraries were in use for that particular project, if while working on a

    project you drop some of the libraries then, when you open that project

    EAGLE will remember the libraries you were using.

     

    Thanks for the informative reply.  However, this isn't the behaviour I'm

    seeing.  Even when I open EAGLE by doubling clicking on a board /

    schematic the behaviour is the same - libraries one level deep are

    activated, anything else isn't.

     

    It doesn't seem to matter if the network share is mounted or not, and

    I've tried opening the schematic / board, changing things, saving it,

    quitting and launching (by double-clicking on the schematic or board).

     

    Under what conditions does EAGLE update the .epf file?

     

    To answer your other concern, you don't have to create that new

    directory EAGLE offers to make, simply click the red X in Windows to

    close the screen that has popped the error message.

     

    None of the dialogue boxes have close buttons (nor should they - the

    question presented is yes/no, and closing the window that way allows the

    user's intentions to be ambiguous).  They have "No" and "Yes" buttons,

    with the "Yes" sometimes indicated as the default (and sometimes being

    default but not indicated as such)

     

    The problem is that the default behaviour is highly undesirable when the

    directory in question is in /Volumes/ on Mac OS X (and, I presume, other

    specific locations on other operating systems)

     

    Regards,

    Nic Jones,

    Ocean Controls

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 15 years ago

    (comments in line)

     

    Jorge Garcia wrote:

    When you open EAGLE without a project and you create a new project by

    default all libraries will be available. However, if EAGLE opens with a

    project then it will first read the EAGLE.epf file checking which

    libraries were in use for that particular project, if while working on a

    project you drop some of the libraries then, when you open that project

    EAGLE will remember the libraries you were using.

     

    Thanks for the informative reply.  However, this isn't the behaviour I'm

    seeing.  Even when I open EAGLE by doubling clicking on a board /

    schematic the behaviour is the same - libraries one level deep are

    activated, anything else isn't.

     

    It doesn't seem to matter if the network share is mounted or not, and

    I've tried opening the schematic / board, changing things, saving it,

    quitting and launching (by double-clicking on the schematic or board).

     

    Under what conditions does EAGLE update the .epf file?

     

    To answer your other concern, you don't have to create that new

    directory EAGLE offers to make, simply click the red X in Windows to

    close the screen that has popped the error message.

     

    None of the dialogue boxes have close buttons (nor should they - the

    question presented is yes/no, and closing the window that way allows the

    user's intentions to be ambiguous).  They have "No" and "Yes" buttons,

    with the "Yes" sometimes indicated as the default (and sometimes being

    default but not indicated as such)

     

    The problem is that the default behaviour is highly undesirable when the

    directory in question is in /Volumes/ on Mac OS X (and, I presume, other

    specific locations on other operating systems)

     

    Regards,

    Nic Jones,

    Ocean Controls