Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) NAME command in ULP
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 16 replies
  • Subscribers 189 subscribers
  • Views 3039 views
  • Users 0 members are here
Related

NAME command in ULP

rachaelp
rachaelp over 10 years ago

Hello,

 

I've using NAME within a ULP to automatically rename some busses/wires. It

works great when there is just one occurrence of a wire on a sheet but as

soon as there is a second I get a pop-up asking if I want to change just

the selected segment or all segments in the sheet. Looking at the docs I

can't see a way to make this happen automatically without prompting, does

anybody else know of a way to stop this prompt showing up?

 

If not then maybe the command needs an enhancement to allow the following

optional parameter for naming busses/wires:

 

NAME new_name (x y) T

 

where T = This segment, E = Every segment on sheet and A = All segments on

all sheets

 

Best Regards,

 

Rachael

--

Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

 

  • Sign in to reply
  • Cancel
Parents
  • rachaelp
    rachaelp over 10 years ago

    Morten Leikvoll wrote on Wed, 18 May 2016 08:05

    On 15.05.2016 23:35, Rachael wrote:

    Hello,

     

    I've using NAME within a ULP to automatically rename some

    busses/wires. It

    works great when there is just one occurrence of a wire on a sheet

    but as

    soon as there is a second I get a pop-up asking if I want to

    change just

    the selected segment or all segments in the sheet. Looking at the

    docs I

    can't see a way to make this happen automatically without

    prompting, does

    anybody else know of a way to stop this prompt showing up?

     

    If not then maybe the command needs an enhancement to allow the

    following

    optional parameter for naming busses/wires:

     

    NAME new_name (x y) T

     

    where T = This segment, E = Every segment on sheet and A = All

    segments on

    all sheets

     

    I support this suggestion. In fact I flagged this issue many years

    ago.

    All the commands with the potential of resulting in a requester should

     

    have these options. Currently only the yes/no requesters can be

    pre-answered with the SET CONFIRM, but this doesnt work with other

    requesters.

     

     

    So I just tried the SET CONFIRM option in my script and it does get rid of

    the nag, it would seem YES equates to the E option in my above example and

    I suspect NO would equate to the T (I haven't tried it) but sadly there is

    no way to make this work across all sheets with this option.

     

    It's also a sledge hammer approach to turn off all the warnings for the

    entire script with a blanket YES or NO auto confirmation. You could keep

    changing it in the script for every time you need to do something

    different, but I think my suggestion to be able to specify exactly how it

    should be handled for every occurrence of such commands within a script is

    much more powerful and much safer. In the docs it even gives a big warning

    about the dangers of using SET CONFIRM so it would seem sensible for

    CadSoft to enhance all such commands to provide a much more flexible,

    easier to use and safer option.

     

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • rachaelp
    rachaelp over 10 years ago

    Morten Leikvoll wrote on Wed, 18 May 2016 08:05

    On 15.05.2016 23:35, Rachael wrote:

    Hello,

     

    I've using NAME within a ULP to automatically rename some

    busses/wires. It

    works great when there is just one occurrence of a wire on a sheet

    but as

    soon as there is a second I get a pop-up asking if I want to

    change just

    the selected segment or all segments in the sheet. Looking at the

    docs I

    can't see a way to make this happen automatically without

    prompting, does

    anybody else know of a way to stop this prompt showing up?

     

    If not then maybe the command needs an enhancement to allow the

    following

    optional parameter for naming busses/wires:

     

    NAME new_name (x y) T

     

    where T = This segment, E = Every segment on sheet and A = All

    segments on

    all sheets

     

    I support this suggestion. In fact I flagged this issue many years

    ago.

    All the commands with the potential of resulting in a requester should

     

    have these options. Currently only the yes/no requesters can be

    pre-answered with the SET CONFIRM, but this doesnt work with other

    requesters.

     

     

    So I just tried the SET CONFIRM option in my script and it does get rid of

    the nag, it would seem YES equates to the E option in my above example and

    I suspect NO would equate to the T (I haven't tried it) but sadly there is

    no way to make this work across all sheets with this option.

     

    It's also a sledge hammer approach to turn off all the warnings for the

    entire script with a blanket YES or NO auto confirmation. You could keep

    changing it in the script for every time you need to do something

    different, but I think my suggestion to be able to specify exactly how it

    should be handled for every occurrence of such commands within a script is

    much more powerful and much safer. In the docs it even gives a big warning

    about the dangers of using SET CONFIRM so it would seem sensible for

    CadSoft to enhance all such commands to provide a much more flexible,

    easier to use and safer option.

     

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.