Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) NAME command in ULP
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 16 replies
  • Subscribers 189 subscribers
  • Views 3031 views
  • Users 0 members are here
Related

NAME command in ULP

rachaelp
rachaelp over 10 years ago

Hello,

 

I've using NAME within a ULP to automatically rename some busses/wires. It

works great when there is just one occurrence of a wire on a sheet but as

soon as there is a second I get a pop-up asking if I want to change just

the selected segment or all segments in the sheet. Looking at the docs I

can't see a way to make this happen automatically without prompting, does

anybody else know of a way to stop this prompt showing up?

 

If not then maybe the command needs an enhancement to allow the following

optional parameter for naming busses/wires:

 

NAME new_name (x y) T

 

where T = This segment, E = Every segment on sheet and A = All segments on

all sheets

 

Best Regards,

 

Rachael

--

Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 10 years ago

    On 19.05.2016 14:30, Richard Hammerl wrote:

    Am 19.05.2016 um 11:16 schrieb Morten Leikvoll:

    On 19.05.2016 10:55, Richard Hammerl wrote:

    I think this could be an enhancement of the SET CONFIRM command.

    We will check this....

     

    Now, THAT you have to explain. I think the rest of us would say no. The

    inline option is much better. It does not need to be backward compatible

    as long as no explicit selection opens the requester as before.

     

     

     

    The inline option with the NAME command? It's a bit tricky there

    because of the current syntax.

    You can for example use  NAME oldname newname   or   NAME name (x y)

     

    To add such options as Rachael suggested is possible, but IMHO not

    so elegant. Think also of signal polygons in the board? There we would

    need additional options like P for Polygon only , or W for whole signal

    or something like that....

    We get a number of letters that have to be distinguisable from the

    names.

     

    On the other hand for SET CONFIRM we could add some options like

    OPT1, OPT2, OPT3 and preselect/address/confirm the wanted option

    of the dialog. This would work for all dialogs that offer more options

    to choose. It fits better in the current structure of EAGLE.

     

    For example:

    NAME net

    OPT1  this segment               set confirm opt1; name GND (0 1);

    OPT2  all segments on sheet      set confirm opt2; name GND (0 1);

    OPT3  all segments on all sheets set confirm opt3; name GND (0 1);

     

    NAME polygon

    OPT1 polygon only         set confirm opt1; name GND (0 1);

    OPT2 whole signal         set confirm opt2; name GND (0 1);

     

    And we would be prepared for future dialogs as well.  image

     

    Surely there must be some reserved character that can be used to avoid

    mixup with any names? Like the character ':', so you could define

    commands like:

     

    NAME :allsheets:  :thisseg: (x y) :includepolygons:;

     

     

    This is very easy to interpret for the commant interpreter.

    As shown, I do prefer having some name instead of single character or

    numbers for the selections. They will also work for future added keywords.

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 10 years ago

    On 19.05.2016 14:30, Richard Hammerl wrote:

    Am 19.05.2016 um 11:16 schrieb Morten Leikvoll:

    On 19.05.2016 10:55, Richard Hammerl wrote:

    I think this could be an enhancement of the SET CONFIRM command.

    We will check this....

     

    Now, THAT you have to explain. I think the rest of us would say no. The

    inline option is much better. It does not need to be backward compatible

    as long as no explicit selection opens the requester as before.

     

     

     

    The inline option with the NAME command? It's a bit tricky there

    because of the current syntax.

    You can for example use  NAME oldname newname   or   NAME name (x y)

     

    To add such options as Rachael suggested is possible, but IMHO not

    so elegant. Think also of signal polygons in the board? There we would

    need additional options like P for Polygon only , or W for whole signal

    or something like that....

    We get a number of letters that have to be distinguisable from the

    names.

     

    On the other hand for SET CONFIRM we could add some options like

    OPT1, OPT2, OPT3 and preselect/address/confirm the wanted option

    of the dialog. This would work for all dialogs that offer more options

    to choose. It fits better in the current structure of EAGLE.

     

    For example:

    NAME net

    OPT1  this segment               set confirm opt1; name GND (0 1);

    OPT2  all segments on sheet      set confirm opt2; name GND (0 1);

    OPT3  all segments on all sheets set confirm opt3; name GND (0 1);

     

    NAME polygon

    OPT1 polygon only         set confirm opt1; name GND (0 1);

    OPT2 whole signal         set confirm opt2; name GND (0 1);

     

    And we would be prepared for future dialogs as well.  image

     

    Surely there must be some reserved character that can be used to avoid

    mixup with any names? Like the character ':', so you could define

    commands like:

     

    NAME :allsheets:  :thisseg: (x y) :includepolygons:;

     

     

    This is very easy to interpret for the commant interpreter.

    As shown, I do prefer having some name instead of single character or

    numbers for the selections. They will also work for future added keywords.