Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Airwires
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 189 subscribers
  • Views 477 views
  • Users 0 members are here
Related

Airwires

stevekale
stevekale over 10 years ago

Hi

 

I have been laid low by a board which passed DRC and ERC (board and circuit were the same) but which had an uncompleted trace - an airwire.  I am very surprised that DRC/ERC didn't flag this up.  I see now that when I run the rats nest tool it will tell me how many airwires remain but of course it doesn't tell where they are.

 

Are there any tips to avoid such problems in the future?

 

Regards

 

Steve

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 10 years ago

    Am 15.07.2016 um 16:47 schrieb Steve Kale:

    Hi

     

    I have been laid low by a board which passed DRC and ERC (board and circuit were the same) but which had an uncompleted trace - an airwire.  I am very surprised that DRC/ERC didn't flag this up.  I see now that when I run the rats nest tool it will tell me how many airwires remain but of course it doesn't tell where they are.

     

    Are there any tips to avoid such problems in the future?

     

    Regards

     

    Steve

     

    --

    To view any images and attachments in this post, visit:

    https://www.element14.com/community/message/201504

     

     

    RATSNEST and DRC are two separate things. There are intentions to

    show the number of airwires also when checking for errors.....

     

    Basically you should always do a RATSNEST when you think you have

    finished your design. Of course, you should use RATSNESt also when you

    are working on the layout. So the airwires will be recalculated and

    you have also options to hide signals for the routing process

    --> HELP RATSNEST for more...

     

    If you are searching for the left airwire in your design you could

    go to Options/Set/Misc and set the "Catch factor" to 100%.

    Now WINDOW FIT; , activate the ROUTE command and click into the

    drawing. The airwire will be catched by the mouse cursor.

     

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/training/faq/

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • stevekale
    stevekale over 10 years ago in reply to autodeskguest

    Thanks for the tips regarding searching for airwires.  I still find it rather extraordinary that airwires don't produce DRC/ERC errors and that the board and schematic can be regarded as consistent when there is incomplete routing.  Doesn't make any sense at all.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • stevekale
    stevekale over 10 years ago in reply to autodeskguest

    Thanks for the tips regarding searching for airwires.  I still find it rather extraordinary that airwires don't produce DRC/ERC errors and that the board and schematic can be regarded as consistent when there is incomplete routing.  Doesn't make any sense at all.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • rachaelp
    rachaelp over 10 years ago in reply to stevekale

    Steve Kale wrote:

     

    Thanks for the tips regarding searching for airwires. I still find it rather extraordinary that airwires don't produce DRC/ERC errors and that the board and schematic can be regarded as consistent when there is incomplete routing. Doesn't make any sense at all.

    Hi Steve,

     

    An air wire isn't a error, it's just a net you haven't routed yet therefore the schematic and layout are consistent regardless of whether it's been completely routed. An example of it being inconsistent would be if you changed something in the schematic without the layout being loaded so it didn't reflect this change, then they are inconsistent. I'd be happy for DRC to add a note (not error) reporting the number of air wires remaining but it's so quick to hit "Ratsnest" that it's really not an issue for me.

     

    A better place to show a more obvious message would possibly be in the CAM processor if you were trying to export gerbers when the routing was incomplete. It's fine to do this if you just want a quick ballpark quote but I can see it being useful for some people if it were highlighted at this point. All these issues can easily be solved by having a simple pre-manufacturing checklist which you complete before submitting your final data to the board house though.

     

    Best Regards,

     

    Rachael