Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Generic TSSOP14 package.
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1 reply
  • Subscribers 183 subscribers
  • Views 541 views
  • Users 0 members are here
  • paclages.
  • generic
Related

Generic TSSOP14 package.

Former Member
Former Member over 10 years ago

HI there,

Although I've been in Electronic design and prototyping for many years, I'm new to Eagle.

 

I'm trying to generate a circuit using some Maxim IC's that are not in your parts list (very extensive I have to say).

 

The main problem I'm having is that there is a Reference Package item for a TSSOP14 in the board editor but I can't find one in the schematic editor.

 

Is there such a package in the schematic editor?

 

If so, where?

 

Also, if I place a TSSOP14 package in the board editor, the Grid Snap function will NOT allow me to place tracks or signal paths to the pins.

 

Is there a way to switch OFF Grid Snap? I CAN'T FIND THIS IN THE HELP MENU.

 

I look forward to any reply.

  • Sign in to reply
  • Cancel
  • autodeskguest
    autodeskguest over 10 years ago

    On 16/10/15 08:40, Sandy Smith wrote:

    HI there,

    Although I've been in Electronic design and prototyping for many years,

    I'm new to Eagle.

     

    I'm trying to generate a circuit using some Maxim IC's that are not in

    your parts list (very extensive I have to say).

     

    The main problem I'm having is that there is a Reference Package item

    for a TSSOP14 in the board editor but I can't find one in the schematic

    editor.

     

    No, there won't be, because TSSOP14 is a package, not a symbol.

     

    This should be familiar to you in principle, as you've been "in

    Electronic design for many years", but the terminology Eagle uses may

    not be. When you design your circuit, you start with a schematic in

    which all components are represented by "symbols", which probably don't

    look anything like the physical component but represent its function.

    Then, having completed the schematic, you design a board that implements

    it. At this point you need to decide on "packages" for the components -

    are you using through hole or SMD, wide SO or TSSOP, etc. Depending on

    the component, this might also affect which "pins" (schematic symbol,

    functional connections) appear on which "pads" (physical connections on

    the package). This mapping is maintained, for each "device", in its

    library entry. Devices consist of one or more schematic symbols (all

    present in an instance of the device, but may not all be the same -

    think 7400 quad NAND gate vs. a relay) coupled to one or more board

    packages (only one of which is chosen).

     

    Is there such a package in the schematic editor?

     

    No, see above. You need to create a device, in a library of your own, to

    represent the Maxim IC in question, with both schematic symbol and

    TSSOP14 (and possibly other) package(s).

     

     

    If so, where?

     

    Also, if I place a TSSOP14 package in the board editor, the Grid Snap

    function will NOT allow me to place tracks or signal paths to the pins.

     

    You can start and end routed tracks on pads that are off-grid, if the

    pads belong to a package that belongs to a device that appears on the

    schematic, with a net connected to the corresponding pin.

     

    Is there a way to switch OFF Grid Snap? I CAN'T FIND THIS IN THE HELP

    MENU.

     

    You can set the grid to anything you want, or you can set the "alternate

    grid" to very fine and place with the ALT key down.

     

     

    • Cancel
    • Vote Up 0 Vote Down