EAGLE User Support (English) Preventing a trace with via from linking to plane
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
  • Replies 11 replies
  • Subscribers 181 subscribers
  • Views 930 views
  • Users 0 members are here
Related

Preventing a trace with via from linking to plane

stevekale
stevekale over 9 years ago

I'm not sure I'm going to explain this very well but here goes....

 

I have a board in which I have bypass caps filtering the supply to an op amp.  The "V-" of the op amp supply is GND and GND is a plane on an internal layer. However rather than just using a via to connect the low side of the bypass caps to the GND plane I'd like to force a routing to the via which connects the op amp V- pin to the GND plane. This would be straightforward except I need another via to make the routing on the top rather than bottom layer (where the op amp is sitting) and as soon as I place the via to get to the top layer it connects to the GND plane. How can I isolate this via from GND?

 

Thanks in advance

 

Steve

 

Btw I can only use vias that go through the entire board

  • Sign in to reply
  • Cancel
  • stevekale
    stevekale over 9 years ago

    Thanks for the tip re polygon cutouts.  I'm sure that will come in handy in the future.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<