Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) how to detect brd/sch has unsaved changes from ulp
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 189 subscribers
  • Views 471 views
  • Users 0 members are here
Related

how to detect brd/sch has unsaved changes from ulp

autodeskguest
autodeskguest over 10 years ago

Hi all,

 

does anyone know a method how a ulp can detect if there are unsaved

changes in a board, schematic or library?

--

 

Lorenz

 

  • Sign in to reply
  • Cancel
Parents
  • rachaelp
    rachaelp over 10 years ago

    I don't think there is any status information that can be obtained from ULP directly, I just went through the docs again and couldn't see anything. You could probably do it by having a ULP that initially exits with the WRITE command to save the current design to a temporary location and calls back to itself (or a second ULP) and then calls system() to run a diff command to determine if there are any changes between the two. It's a not particularly clean way to do things but it would probably work. Maybe somebody else can think of something cleaner.

     

    Best Regards,

     

    Rachael

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • rachaelp
    rachaelp over 10 years ago

    I don't think there is any status information that can be obtained from ULP directly, I just went through the docs again and couldn't see anything. You could probably do it by having a ULP that initially exits with the WRITE command to save the current design to a temporary location and calls back to itself (or a second ULP) and then calls system() to run a diff command to determine if there are any changes between the two. It's a not particularly clean way to do things but it would probably work. Maybe somebody else can think of something cleaner.

     

    Best Regards,

     

    Rachael

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • dukepro
    dukepro over 10 years ago in reply to rachaelp

     

    Rachel is correct.

     

    I have been asking for a "dirty" flag in both the board and schematic

    classes for years.

     

    If you're trying to make sure a file is saved, the best way to do it is

    to test for an argument to your ULP.  The absence of the argument

    indicates that the file has NOT been saved.  The ULP can then save the

    file and re-execute itself with the argument appended.  The second pass

    through the ULP would indicate that the file has already been saved and

    is thus not dirty.

     

    Below is an excerpt from a ULP that does exactly that:

     

        //

        // A separate instance of Eagle will be invoked from the command line

        // to produce gerber files.  As such, it does not have access to objects

        // in this process's memory space and can only read from the disk.

        //

        // Therefore, it is imperative to make sure this board is saved

        before allowing

        // this program to continue.

        //

        // Make sure the board is saved after any drill changes

        //

        string file;

        if(argv[1] != "saved") {

            board(B) {

                file = B.name;

            }

            // For the unix/linux/mac world, test will work.

            // For Windoze, something else will have to figure out if

            // the file is writable.

            if (system("test -w " + file) == 0) {

                // By here, the file is writable.  Save it and restart this

        script.

                exit("write;\nrun camprep saved;\n");

            } else {

                if (dlgMessageBox("!

    " + file + "

    "
    + "

    The board file is not writable."
    + "

     

    CAM files will be built from last saved version.",

                    "&Continue", "&Abort") != 0) {

                    exit(0);

                }

            }

        }

        ...

     

    HTH,

        - Chuck

     

     

     

    On 09/12/2016 07:42 AM, rachaelp wrote:

    I don't think there is any status information that can be returned from ULP directly, I just went through the docs again and couldn't see anything. You could probably do it by having a ULP that initially exits with the WRITE command to save the current design to a temporary location and calls back to itself (or a second ULP) and then calls system() to run a diff command to determine if there are any changes between the two. It's a not particularly clean way to do things but it would probably work. Maybe somebody else can think of something cleaner.

     

    Best Regards,

     

    Rachael

     

    --

    To view any images and attachments in this post, visit:

    https://www.element14.com/community/message/205576

     

     

    Attachments:
    1805.att1.html.zip