Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Why do I need to draw the same symbol N times?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 16 replies
  • Subscribers 189 subscribers
  • Views 2811 views
  • Users 0 members are here
Related

Why do I need to draw the same symbol N times?

autodeskguest
autodeskguest over 10 years ago

More often than not the same chip is available in different packages,

quite often with different number of pins and the packages with fewer

pins omit some of the lesser used signals.

 

Currently, you need to create a different symbol for every package: if

you have a chip that comes in 5 different packages, with a few pin

differences, you need a symbol drawn for ABC1234-SOIC, ABC1234-BGA,

ABC1234-TSOP and so on. It's the same damn chip, just on some packages

some pins are missing.

 

I wonder if I'm alone with the wish of having just one symbol, with

every possible signal drawn. Then, when it gets placed to the schematic

with a package selected, the not bonded pins grey out and don't allow

wires to be connected to them?

--

Zoltán Kócsi

Bendor Research Pty. Ltd.

 

 

  • Sign in to reply
  • Cancel
  • autodeskguest
    autodeskguest over 10 years ago in reply to autodeskguest

    On 27.09.2016 18:36, Jorge Garcia wrote:

    Hi All,

     

    This is definitely a pretty split topic it would be hard to make a

    suggestion either way.

     

    To answer the original question, the way I would handle this is a I

    would create one symbol which would represent the smallest( the one with

    the fewest pads) of the packages.

     

    I would create a device for the smallest package using just that symbol.

     

    Let's say that the next package up has 4 extra pins. I would create a

    new symbol with just those 4 pins. When I go to make the device for this

    package, I would add this symbol plus the symbol with the 4 extra pins.

     

    Repeat this for as many packages as necessary. Basically, instead of

    subtracting pins from the largest package configuration, we add pins to

    the lowest. You can adjust the add levels to make the two symbols come

    in together.

     

    I don't like the idea of greying out pins in the schematic or x-ing them

    out in some way. I think it makes the schematic untidy and adds

    unnecessary additional info.

     

    hth,

    Jorge Garica

     

     

     

    I don't want to suggest a complete solution for this, but rather throw

    in options.

     

    Devices may consist of several symbols, and maybe a symbol could

    be optional for each package. Like if a mcu/fpga or similar comes in

    packages without a set of IO, you can put that package specific IO in a

    separate symbol and connect it to those packages that has it. This would

    keep some of the symbol-package consistancy check that exist today.

     

    On the other hand, I'd like to see changes to pin directions wich has

    been discussed across several topics before. This includes the current

    problematic sup/pwr directions and an additional "project dependant

    programmable" directions (for fpga/mcu). I think this can be solved

    easily by introducing new io directions, and keep the current ones as is.

     

    Since I am a FPGA man, I'd also see the need for symbols to change

    visible pin text depending on usage. The symbols gets very large if you

    want to include every special function of a single pin. To give an

    example, for an Altera Arria10 fpga, in a 1517pin package, a single pin

    (G20) has one of these functions, depending on configuration/project usage:

    -PLL_2L_CLKOUT0p (lvds clock output from a pll, positive pin)

    -PLL_2L_CLKOUT0 (single end clock output from the above pll)

    -PLL_2L_FB0 (feedback input to the above pll)

    -LVDS2L_15p, with no soft CDR support, for dedicated LVDS high speed io.

    -DQ4 for a 4 bit DDR memory lane

    -DQ2 for a 8 bit DDR memory lane

    -DQ1 for a 16 bit DDR memory lane

    -DQ0 for a 32 bit DDR memory lane

    To further complicate this, the IO's may even have special functions

    before it is configured, so the function of the io in some design may be

    double.

     

    Now try to get all that into a single symbol. Of course that is not

    practical. This suggests the need for "symbol" configuration, and it

    will be needed pr pin. Also note that every project specific function

    have a assigned direction, wich would be nice if it could go into the

    ERC. But tbh, I think this is a bit far into the future, but nice to

    keep in mind when looking ahead.

     

    For now, I draw application specific symbols.

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 10 years ago in reply to autodeskguest

    On 27.09.2016 18:36, Jorge Garcia wrote:

    Hi All,

     

    This is definitely a pretty split topic it would be hard to make a

    suggestion either way.

     

    To answer the original question, the way I would handle this is a I

    would create one symbol which would represent the smallest( the one with

    the fewest pads) of the packages.

     

    I would create a device for the smallest package using just that symbol.

     

    Let's say that the next package up has 4 extra pins. I would create a

    new symbol with just those 4 pins. When I go to make the device for this

    package, I would add this symbol plus the symbol with the 4 extra pins.

     

    Repeat this for as many packages as necessary. Basically, instead of

    subtracting pins from the largest package configuration, we add pins to

    the lowest. You can adjust the add levels to make the two symbols come

    in together.

     

    I don't like the idea of greying out pins in the schematic or x-ing them

    out in some way. I think it makes the schematic untidy and adds

    unnecessary additional info.

     

    hth,

    Jorge Garica

     

     

     

    I don't want to suggest a complete solution for this, but rather throw

    in options.

     

    Devices may consist of several symbols, and maybe a symbol could

    be optional for each package. Like if a mcu/fpga or similar comes in

    packages without a set of IO, you can put that package specific IO in a

    separate symbol and connect it to those packages that has it. This would

    keep some of the symbol-package consistancy check that exist today.

     

    On the other hand, I'd like to see changes to pin directions wich has

    been discussed across several topics before. This includes the current

    problematic sup/pwr directions and an additional "project dependant

    programmable" directions (for fpga/mcu). I think this can be solved

    easily by introducing new io directions, and keep the current ones as is.

     

    Since I am a FPGA man, I'd also see the need for symbols to change

    visible pin text depending on usage. The symbols gets very large if you

    want to include every special function of a single pin. To give an

    example, for an Altera Arria10 fpga, in a 1517pin package, a single pin

    (G20) has one of these functions, depending on configuration/project usage:

    -PLL_2L_CLKOUT0p (lvds clock output from a pll, positive pin)

    -PLL_2L_CLKOUT0 (single end clock output from the above pll)

    -PLL_2L_FB0 (feedback input to the above pll)

    -LVDS2L_15p, with no soft CDR support, for dedicated LVDS high speed io.

    -DQ4 for a 4 bit DDR memory lane

    -DQ2 for a 8 bit DDR memory lane

    -DQ1 for a 16 bit DDR memory lane

    -DQ0 for a 32 bit DDR memory lane

    To further complicate this, the IO's may even have special functions

    before it is configured, so the function of the io in some design may be

    double.

     

    Now try to get all that into a single symbol. Of course that is not

    practical. This suggests the need for "symbol" configuration, and it

    will be needed pr pin. Also note that every project specific function

    have a assigned direction, wich would be nice if it could go into the

    ERC. But tbh, I think this is a bit far into the future, but nice to

    keep in mind when looking ahead.

     

    For now, I draw application specific symbols.

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rachaelp
    rachaelp over 10 years ago in reply to autodeskguest

    Jorge Garcia wrote on Tue, 27 September 2016 17:36

    Hi All,

     

    This is definitely a pretty split topic it would be hard to make a

    suggestion either way.

     

    To answer the original question, the way I would handle this is a I

    would create one symbol which would represent the smallest( the one

    with

    the fewest pads) of the packages.

     

    I would create a device for the smallest package using just that

    symbol.

     

    Let's say that the next package up has 4 extra pins. I would create a

    new symbol with just those 4 pins. When I go to make the device for

    this

    package, I would add this symbol plus the symbol with the 4 extra

    pins.

     

    Repeat this for as many packages as necessary. Basically, instead of

    subtracting pins from the largest package configuration, we add pins to

     

    the lowest. You can adjust the add levels to make the two symbols come

     

    in together.

     

    I don't like the idea of greying out pins in the schematic or x-ing

    them

    out in some way. I think it makes the schematic untidy and adds

    unnecessary additional info.

     

    hth,

    Jorge Garica

     

     

    I'm sort of in agreement with you regarding the negatives of greying out or

    x-ing out the pins, but then for a lot of cases adding extra symbol parts

    just for the additional pins could quickly lead to a messy schematics too

    and you may not be able to group pins how you would like.

     

    So the only other solution I can think of would be to have the ability to

    specify a symbol variant based on the "master" symbol which could then have

    pins removed / renamed / added as necessary. Then anything in the master

    symbol which was unrelated to the changes on the variants would be

    inherited such that any changes to these parts of the master symbol would

    occur in the variant symbols. This would remove the issue of having

    multiple copies of a single symbol to maintain.

     

    There are several other use cases for having the ability to specify

    multiple symbols (I covered one of these in one of my earliest posts on

    this forum) but the way of using the feature would probably need to be

    slightly tweaked. It would be good if there was a way to support multiple

    symbols which could cover all use cases.

     

    Best Regards,

     

    Rachael

     

     

     

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 10 years ago in reply to rachaelp

    Hi All,

     

    This is definitely a pretty split topic it would be hard to make a

    suggestion either way.

     

    To answer the original question, the way I would handle this is a I

    would create one symbol which would represent the smallest( the one with

    the fewest pads) of the packages.

     

    I would create a device for the smallest package using just that symbol.

     

    Let's say that the next package up has 4 extra pins. I would create a

    new symbol with just those 4 pins. When I go to make the device for this

    package, I would add this symbol plus the symbol with the 4 extra pins.

     

    Repeat this for as many packages as necessary. Basically, instead of

    subtracting pins from the largest package configuration, we add pins to

    the lowest. You can adjust the add levels to make the two symbols come

    in together.

     

    I don't like the idea of greying out pins in the schematic or x-ing them

    out in some way. I think it makes the schematic untidy and adds

    unnecessary additional info.

     

    hth,

    Jorge Garica

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dukepro
    dukepro over 10 years ago in reply to autodeskguest

    On 09/25/2016 05:32 PM, Olin Lathrop wrote:

    zoltan wrote on Sun, 25 September 2016 01:53

    Hence my request: I'd like to

    draw only one symbol and assign a package, even if the symbol has

    more pins than the package. Then the schematics could grey out or even

    completely hide the pins that are not available on the package.

     

    By the time you specify which pins should be greyed out, you might as well

    have made the minor modifications from the symbol with a little more or

    little less pins.  If you're only changing a few pins, there isn't really a

    problem to solve here.

     

    Olin,

     

    The implication of extra work is not entirely accurate.  This has

    already been discussed in at least one thread that I started titled

    "Allow and Hide Unconnected Pins." in this newsgroup on December 20th of

    2014

     

    In my case, I was dealing with the MSP430 family of microcontrollers.

    Others have run into this problem on Xylinx, Atmel, and others.  This

    addresses instances where everything on the glass is the same.  The

    difference is that on smaller packages with fewer pins, some pads on the

    die are not wired to pins on the package.

     

    (back to Eagle's definition of pads and pins...)

    It is a reasonable request to create one device, draw one set of symbols

    for the most extensive package, and on smaller packages either grey out

    the pin on the symbol, or put an "x" at the connect point for those pins

    that have not been connected to a pad.

     

    At this time, Eagle does not permit one to choose a package that has

    fewer pads than the device's symbols have pins.

     

    There is no extra work involved - the relationship between pads on the

    package and pins on the symbol established in the library editor must be

    done regardless of whether are more pins than pads, more pads than pins,

    or an equal number of each.

     

    Jorge,  Is there any chance of refreshing this request?

     

     

     

    You don't want Eagle to just assume that you intentionally used a symbol

    with too many pins and not show you the remaining ones.  That would

    circumvent useful error checking.

     

    I also don't want Eagle to assume that using a package without enough

    pads is prohibited.

     

    An alert box in the library editor can verify the choice.

     

     

      Also, if a different chip has fewer

    pins, you most likely want to draw the symbol differently.  You may want to

    make it a little smaller, change some of the labeling inside the symbol,

    etc.

     

    You actually make a good argument for having the choice available to

    reuse a larger symbol, or design separate symbols.  It would be nice to

    have the ability to use a smaller package.  Whether one chooses to use

    that feature is up to the designer.

     

    There are many cases where one might start out a uC design with a

    smaller package, and promote to a larger package as the design

    develops.  Feature creep can cause this.

     

    On more than one occasion I have designed embedded systems to accept

    multiple packages of the same IC.  This allows the same design to

    survive unavailability of parts.  i.e. If I can get by with a QFP48,

    I'll also overlay the same package with a QFP64, or QFP80.  If the

    optimal 48-pin package is out of stock, production can drop in a 64 and

    keep rolling.

     

    Sure, it takes up a bit more real estate, but it beats having to spin

    another board and qualify it while production is waiting.

     

    A good example is a voltage regulator.  The simple 3-pin variety can be

    drawn more simply and smaller than one with a shutdown input, for example.

    I wouldn't want the simple 3-pin version burdened with a greyed out

    shutdown input.  I also wouldn't want it drawn bigger with inexplicable

    extra space in the 3-pin usage case.

     

    If the symbols are similar except for a few pins, then there isn't really a

    problem here.  Copy and edit works fine.  If the symbols are substantially

    different, then you're going to have to do some work for each case one way

    or the other.

     

    I think you're overestimating the work involved.  The proposed feature

    reduces work - one does not have to create a separate device for each of

    the very similar symbols that also have to be created.  The idea is one

    device, one set of symbols, and variations in package connections.

     

    In my suggestion in December of 2014, I stated that the unused pins (on

    the symbol) should not be shown.  I later refined this to state that

    these pins should either be greyed, or have an "x" at the connection

    point, or both.  As you pointed out, it can introduce errors if the pins

    are simply not shown.

     

    Regards,

        - Chuck

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 10 years ago in reply to autodeskguest

    On Sun, 25 Sep 2016 17:32:32 -0400

    Olin Lathrop <eagle9304@embedinc.com> wrote:

     

    By the time you specify which pins should be greyed out, you might as

     

    Um, all of them which I did not assign to a package pin? What else

    should I specify in some time-consuming manner?

     

    You don't want Eagle to just assume that you intentionally used a

    symbol with too many pins and not show you the remaining ones. That

    would circumvent useful error checking.

     

    So, maybe a message box asking me whether I really want to assign this

    package to this chip could be a good solution?

     

    Also, if a different chip

    has fewer pins, you most likely want to draw the symbol differently.

     

    Most definitely not, especially not for microcontrollers or FPGAs or

    anything with 20 or 50 or 100 or 200 or more pins of which a few

    percentage may or may not be present on any particular package variant.

    It is not a different chip, it is the same chip, except that some of

    its pins on the silicon are not connected to package pins.

     

    A good example is a voltage regulator.  The simple 3-pin variety can

    be drawn more simply and smaller than one with a shutdown input, for

    example. I wouldn't want the simple 3-pin version burdened with a

    greyed out shutdown input.  I also wouldn't want it drawn bigger with

    inexplicable extra space in the 3-pin usage case.

     

    And how about the 24-pin variety (a switch mode), which is also

    available in a 21 pin variety, being exactly the same except that a

    normally left open pin, only used for synchronising multiple chips, is

    not available (the other 3 missing pins are the ground pins, which are

    now all on the central tab under the chip)?

     

    Quote:

    In the software world copy-paste-massage-ing code is one of the

    cardinal

    sins, and rightly so,

     

    Exactly.  This is the same thing.  Just like with software, you copy

    and paste, then make a few minor edits to adapt to details of the

    situation.

     

    I don't think you understood what you quoted and said 'Exactly' to.

    Cardinal sin means something that one should never, ever do. It has

    religious origins, the 'cardinal sins' are the '7 deadly sins' of

    Christianity, like murder. Copy-paste-massage is known to be the source

    of bugs too numerous to mention and is generally considered a very bad

    way of doing software.

    --

    Zoltán Kócsi

    Bendor Research Pty. Ltd.

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 10 years ago in reply to autodeskguest

    zoltan wrote on Sun, 25 September 2016 01:53

    Hence my request: I'd like to

    draw only one symbol and assign a package, even if the symbol has

    more pins than the package. Then the schematics could grey out or even

    completely hide the pins that are not available on the package.

     

     

    By the time you specify which pins should be greyed out, you might as well

    have made the minor modifications from the symbol with a little more or

    little less pins.  If you're only changing a few pins, there isn't really a

    problem to solve here.

     

    You don't want Eagle to just assume that you intentionally used a symbol

    with too many pins and not show you the remaining ones.  That would

    circumvent useful error checking.  Also, if a different chip has fewer

    pins, you most likely want to draw the symbol differently.  You may want to

    make it a little smaller, change some of the labeling inside the symbol,

    etc.

     

    A good example is a voltage regulator.  The simple 3-pin variety can be

    drawn more simply and smaller than one with a shutdown input, for example.

    I wouldn't want the simple 3-pin version burdened with a greyed out

    shutdown input.  I also wouldn't want it drawn bigger with inexplicable

    extra space in the 3-pin usage case.

     

    If the symbols are similar except for a few pins, then there isn't really a

    problem here.  Copy and edit works fine.  If the symbols are substantially

    different, then you're going to have to do some work for each case one way

    or the other.

     

    Quote:

    In the software world copy-paste-massage-ing code is one of the

    cardinal

    sins, and rightly so,

     

     

    Exactly.  This is the same thing.  Just like with software, you copy and

    paste, then make a few minor edits to adapt to details of the situation.

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 10 years ago

    On Fri, 23 Sep 2016 08:47:48 +0200

    Morten Leikvoll <mleikvol@yahoo.nospam> wrote:

     

    You dont need to redraw the symbol. You just create a new component

    and add the symbol + all the packages that work with this symbol at

    the same component, then connect them correctly. This works, even if

    some packages have more gnd/shield pins, cause every package is

    connected separately.

     

    As Rik Steenwinkel pointed out, that doesn't work with very many chips.

    Microcontrollers, FPGAs, power supply chips being ominous examples.

    Micros more often than not drop/gain a few port pins between package

    variants. FPGAs ditto. Power supply chips often drop rarely used

    feature pins. SPI FLASH chips tend to have a 'BUSY' signal on the higher

    pincount package, which is dropped if you go to the smallest

    pincount/footprint one. So the list is quite long.

     

    In my original post I was specifically talking about packages with

    different pin counts and signal pins going missing in the smaller

    package.

     

    But currently (7.x), if the symbol differs slightly betweeen

    packages, you have to copy/make a new symbol, and add/remove pins.

     

    Exactly. As it has always been the case. Hence my request: I'd like to

    draw only one symbol and assign a package, even if the symbol has

    more pins than the package. Then the schematics could grey out or even

    completely hide the pins that are not available on the package.

     

    In the software world copy-paste-massage-ing code is one of the cardinal

    sins, and rightly so, why am I forced to do it with my hardware?

    --

    Zoltán Kócsi

    Bendor Research Pty. Ltd.

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rachaelp
    rachaelp over 10 years ago in reply to autodeskguest

    Stoneshop wrote on Fri, 23 September 2016 09:54

    Not in my version (7.3.0 standard). You can duplicate devices and

    packages, but not symbols.

     

     

    Yes they added a lot of new features to the library manager throughout the

    7.x releases and I can't remember where that was added. If it's an issue

    for you at least you have the option of going to a newer release as you

    have a v7 license.

     

    Best Regards,

     

    Rachael

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rachaelp
    rachaelp over 10 years ago

    zoltan wrote on Fri, 23 September 2016 05:29

    I wonder if I'm alone with the wish of having just one symbol, with

    every possible signal drawn. Then, when it gets placed to the

    schematic

    with a package selected, the not bonded pins grey out and don't allow

    wires to be connected to them?

     

     

    Morten Leikvoll wrote on Fri, 23 September 2016 07:47

    But currently (7.x), if the symbol differs slightly betweeen packages,

     

    you have to copy/make a new symbol, and add/remove pins. Sometimes it

    would have been nice if unconnected pins at the symbol were hidden at

    the schematics, if they are not user/connected to the chosen package.

     

     

    Yes I think this would be nice. For a lot of cases the existing system

    works fine but being able to have a single device which deals with the

    entire part in all its variants rather than having to have duplicate parts

    with slightly different symbols would be a big benefit in terms of having

    much tidier and easier to use libraries. I like the idea of greying out or

    hiding unconnected pins but sometimes that might not be enough as a variant

    can possibly change a pin function (i.e. it bonds the pin to another

    function internally). For this reason I think being able to specify

    alternative symbols within the device as well as alternative packages would

    be a big benefit too.

     

    Best Regards,

     

    Rachael

     

     

     

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
>