Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) SHOW command
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 187 subscribers
  • Views 453 views
  • Users 0 members are here
Related

SHOW command

autodeskguest
autodeskguest over 10 years ago

Eagle 6.4.

 

I have a bunch of signals which are named like D[0], D[1] and so on.

Interestingly, if I tell Eagle to 'show D[0]' it tells me that it can't

find that signal. On the other hand, if I click on the trace (or the

line on the schematics) and ask its info, it merrily tells me that its

name is D[0].

 

Note that these signals are part of a bus but on the schematics they

are not drawn as part of a bus. It was simply not practical, as they

are not on adjacent pins of the symbols. Thus, as far as Eagle is aware,

these are just independent signals, named D[0] and D[1] and so on.

 

Are there some special rules for the '[]' characters in signal names?

--

Zoltán Kócsi

Bendor Research Pty. Ltd.

 

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 10 years ago

    You shouldnt use those brackets in names.. (I'm a bit puzzled that it

    is allowed at all..!?)

     

    Yup, * and ? are also allowed. On the other hand, escaping the special

    characters in the search works:

     

    show D\[4\]

     

    will indeed find D[4]

     

    Use D0,D1,... Then you can use show D[01] to

    show them both.

     

    I used D[0] and the like because that's the way they are named in the

    FPGA's Verilog source and that's the way the DOS OrCad named bus

    members, like 4 decades ago image (Mind you, that ancient schematics

    editor had a couple of extra useful features that Eagle still lacks.)

     

    In any case, the moral of the story, as always, is: RTFM.

     

    Thanks for the help!

    --

    Zoltán Kócsi

    Bendor Research Pty. Ltd.

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 10 years ago

    You shouldnt use those brackets in names.. (I'm a bit puzzled that it

    is allowed at all..!?)

     

    Yup, * and ? are also allowed. On the other hand, escaping the special

    characters in the search works:

     

    show D\[4\]

     

    will indeed find D[4]

     

    Use D0,D1,... Then you can use show D[01] to

    show them both.

     

    I used D[0] and the like because that's the way they are named in the

    FPGA's Verilog source and that's the way the DOS OrCad named bus

    members, like 4 decades ago image (Mind you, that ancient schematics

    editor had a couple of extra useful features that Eagle still lacks.)

     

    In any case, the moral of the story, as always, is: RTFM.

     

    Thanks for the help!

    --

    Zoltán Kócsi

    Bendor Research Pty. Ltd.