EAGLE User Support (English) LTSpice import coming to Mac and Linux-Progress Reports
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
  • Replies 25 replies
  • Subscribers 181 subscribers
  • Views 2630 views
  • Users 0 members are here
Related

LTSpice import coming to Mac and Linux-Progress Reports

autodeskguest
autodeskguest over 9 years ago

Hello All,

 

As mentioned in another thread, I've taken on the task of updating the

LTSpice ULP to work under Linux and Mac. In the other thread I committed

to posting at least once a week on my progress.

 

My goal with this thread besides keeping everyone informed of the

progress, is to document the basic process of updating an existing ULP

and to collect my thoughts as I go through the process.

 

With that out of the way here's what I got so far:

 

This is a large ULP consisting of approx. 4600 lines. Almost 5 times

larger than the biggest ULP I've worked on to date (dxfimport approx.

1000 lines).

 

Alfred, the original author of this ULP deserves a lot of credit for

writing this, it took him almost a year of work IIRC to get it done. The

code is pretty well commented (much of it in German image ) and after

looking through it I've formed a basic idea of how it's structured.

 

In order to make it more manageable, I've split the ULP into sections

using Alfred's comments as a guide. Here's the table of contents:

 

Lines                    Contents

-


               -


1-300               Documentation

300-693               Global Variables

     533-656              Syntax Definition Symbol

695-847               File Functions

849-4140          Export-Import Functions

     889-1874              Export

     1877-4024              Import

     2247-2862          Parse Library Lines

     2865-3858          Parse Schematic Lines

     3859-4024          Import Setup Menu

     4026-4140              Export Menu

4142-4596          Main

     4232-4337              main export

     4339-4596              main import

     4365-4488          import a library

     4490-4573          import a schematic

     4574-4596              main diagnostic

 

 

My plan for now is to traverse these main sections searching for

functions that are OS dependent and then see how I can change them to

not be.

 

I figure that a lot of the code will be unchanged since the functions

that process the contents of the LTSpice file will run directly inside

EAGLE. That's what I'm hoping anyway.

 

Best Regards,

Jorge Garcia

 

  • Sign in to reply
  • Cancel

Top Replies

  • autodeskguest
    autodeskguest over 9 years ago +1
    Hello Everyone, Sorry for missing last week's update, we had to close part of the week due to hurricane Matthew. If you were impacted by this hurricane, then wish you a speedy return to normalcy and that…
  • dukepro
    dukepro over 9 years ago in reply to autodeskguest +1
    On 10/12/2016 06:09 PM, Jorge Garcia wrote: Now I'd like to ask for your opinions on how to proceed. I'm currently trying to determine what the best implementation would be. On one hand I was thinking…
  • autodeskguest
    autodeskguest over 9 years ago in reply to dukepro +1
    Bottom line, I suggest using OS-specific files. To go one further, I would suggest that the OS detection not be done in the main file, but instead be done in a separate file: ltspice.ulp: ... #include…
Parents
  • autodeskguest
    autodeskguest over 9 years ago

    Hello Everyone,

     

    Sorry for missing last week's update, we had to close part of the week

    due to hurricane Matthew. If you were impacted by this hurricane, then

    wish you a speedy return to normalcy and that your families are all OK.

     

    At this point, I've gone through each of the ULP sections and listed the

    functions that I'm certain will have to be re-written or changed. The

    damage isn't too bad, there are 10 functions which will likely have to

    be rewritten or heavily modified. There are also two global variables

    which may need to be changed.

     

    Here's a breakdown:

     

    Lines                Description

    -


                   -


    0661-0672            testsyscommand- Function used to debug, currently

                          uses windows commandline parameters.

     

    0675                 SearchStartDrive- global variable

     

    0677                 SearchLastDrive- global variable

     

    0688-0692            Just an if statement that checks

                          if the ULP is running under Win.

     

    0701-0713            check_windows_root

     

    0746-0847            file_search

     

    1248-1283            readconfig & saveconfig

     

    1342-1349            makedir-only supports window

     

    1914-1919            imp_dirname- assumes windows dir.

     

    3850-3856            call_system

     

    4064-4077            dosfilecopy

     

    4146-4229            Beginning of main, needs to be

                          cleaned up.

     

    4310-4321            Ex_WaitOnHandshake

     

     

    At this point, I know the beginning of main is probably going to require

    the most work. I want to implement a dialog that will allow users to

    specify all of the paths needed by the ULP, should the ULP fail to find

    them automatically. This adds flexibility for different user setups and

    should be more resilient across the three operating systems.

     

    Now I'd like to ask for your opinions on how to proceed. I'm currently

    trying to determine what the best implementation would be. On one hand I

    was thinking I could these OS dependent functions from the main ULP. I

    would then create three different include files one for each OS in which

    each of these functions is adjusted for the needs of the OS. At the

    beginning of the main ULP is would detect what OS it's running under and

    then only include those function definitions. Logistically this seems

    easier to manage to me.

     

    The other option would be to modify these functions in place and use

    something like a switch statement within these functions to run the OS

    specific code. This has the advantage of keeping everything in one file.

     

    What would you guys recommend? Feel free to suggest any other approach

    you think might be suitable.

     

    Thanks everyone for your attention.

     

    Best Regards,

    Jorge Garcia

     

     

     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • rachaelp
    rachaelp over 9 years ago in reply to autodeskguest

    Hi Jorge,

     

    I think of the suggested options I would prefer having separate files for OS specific versions of things and then including the appropriate one in a single OS detection section rather than having to make each function more complicated checking which OS in many places. It'll make the code tidier this way and a lot more manageable.

     

    Alternatively if a lot of the OS specific functions are only OS specific because of a small part of their functionality and you can boil the OS specific tasks down to a common set of functionality then maybe you can create a library that does these tasks and deals with the OS specific stuff in the background, leaving the majority of the actual function code completely untouched. Then you could substitute those calls in many functions if they were doing similar things and it might speed up your task quite a lot.

     

    Best Regards,

     

    Rachael

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • rachaelp
    rachaelp over 9 years ago in reply to autodeskguest

    Hi Jorge,

     

    I think of the suggested options I would prefer having separate files for OS specific versions of things and then including the appropriate one in a single OS detection section rather than having to make each function more complicated checking which OS in many places. It'll make the code tidier this way and a lot more manageable.

     

    Alternatively if a lot of the OS specific functions are only OS specific because of a small part of their functionality and you can boil the OS specific tasks down to a common set of functionality then maybe you can create a library that does these tasks and deals with the OS specific stuff in the background, leaving the majority of the actual function code completely untouched. Then you could substitute those calls in many functions if they were doing similar things and it might speed up your task quite a lot.

     

    Best Regards,

     

    Rachael