EAGLE User Support (English) LTSpice import coming to Mac and Linux-Progress Reports
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
  • Replies 25 replies
  • Subscribers 181 subscribers
  • Views 2640 views
  • Users 0 members are here
Related

LTSpice import coming to Mac and Linux-Progress Reports

autodeskguest
autodeskguest over 9 years ago

Hello All,

 

As mentioned in another thread, I've taken on the task of updating the

LTSpice ULP to work under Linux and Mac. In the other thread I committed

to posting at least once a week on my progress.

 

My goal with this thread besides keeping everyone informed of the

progress, is to document the basic process of updating an existing ULP

and to collect my thoughts as I go through the process.

 

With that out of the way here's what I got so far:

 

This is a large ULP consisting of approx. 4600 lines. Almost 5 times

larger than the biggest ULP I've worked on to date (dxfimport approx.

1000 lines).

 

Alfred, the original author of this ULP deserves a lot of credit for

writing this, it took him almost a year of work IIRC to get it done. The

code is pretty well commented (much of it in German image ) and after

looking through it I've formed a basic idea of how it's structured.

 

In order to make it more manageable, I've split the ULP into sections

using Alfred's comments as a guide. Here's the table of contents:

 

Lines                    Contents

-


               -


1-300               Documentation

300-693               Global Variables

     533-656              Syntax Definition Symbol

695-847               File Functions

849-4140          Export-Import Functions

     889-1874              Export

     1877-4024              Import

     2247-2862          Parse Library Lines

     2865-3858          Parse Schematic Lines

     3859-4024          Import Setup Menu

     4026-4140              Export Menu

4142-4596          Main

     4232-4337              main export

     4339-4596              main import

     4365-4488          import a library

     4490-4573          import a schematic

     4574-4596              main diagnostic

 

 

My plan for now is to traverse these main sections searching for

functions that are OS dependent and then see how I can change them to

not be.

 

I figure that a lot of the code will be unchanged since the functions

that process the contents of the LTSpice file will run directly inside

EAGLE. That's what I'm hoping anyway.

 

Best Regards,

Jorge Garcia

 

  • Sign in to reply
  • Cancel

Top Replies

  • autodeskguest
    autodeskguest over 9 years ago +1
    Hello Everyone, Sorry for missing last week's update, we had to close part of the week due to hurricane Matthew. If you were impacted by this hurricane, then wish you a speedy return to normalcy and that…
  • dukepro
    dukepro over 9 years ago in reply to autodeskguest +1
    On 10/12/2016 06:09 PM, Jorge Garcia wrote: Now I'd like to ask for your opinions on how to proceed. I'm currently trying to determine what the best implementation would be. On one hand I was thinking…
  • autodeskguest
    autodeskguest over 9 years ago in reply to dukepro +1
    Bottom line, I suggest using OS-specific files. To go one further, I would suggest that the OS detection not be done in the main file, but instead be done in a separate file: ltspice.ulp: ... #include…
Parents
  • autodeskguest
    autodeskguest over 9 years ago

    Hello Everyone,

     

    Sorry for missing last week's update, we had to close part of the week

    due to hurricane Matthew. If you were impacted by this hurricane, then

    wish you a speedy return to normalcy and that your families are all OK.

     

    At this point, I've gone through each of the ULP sections and listed the

    functions that I'm certain will have to be re-written or changed. The

    damage isn't too bad, there are 10 functions which will likely have to

    be rewritten or heavily modified. There are also two global variables

    which may need to be changed.

     

    Here's a breakdown:

     

    Lines                Description

    -


                   -


    0661-0672            testsyscommand- Function used to debug, currently

                          uses windows commandline parameters.

     

    0675                 SearchStartDrive- global variable

     

    0677                 SearchLastDrive- global variable

     

    0688-0692            Just an if statement that checks

                          if the ULP is running under Win.

     

    0701-0713            check_windows_root

     

    0746-0847            file_search

     

    1248-1283            readconfig & saveconfig

     

    1342-1349            makedir-only supports window

     

    1914-1919            imp_dirname- assumes windows dir.

     

    3850-3856            call_system

     

    4064-4077            dosfilecopy

     

    4146-4229            Beginning of main, needs to be

                          cleaned up.

     

    4310-4321            Ex_WaitOnHandshake

     

     

    At this point, I know the beginning of main is probably going to require

    the most work. I want to implement a dialog that will allow users to

    specify all of the paths needed by the ULP, should the ULP fail to find

    them automatically. This adds flexibility for different user setups and

    should be more resilient across the three operating systems.

     

    Now I'd like to ask for your opinions on how to proceed. I'm currently

    trying to determine what the best implementation would be. On one hand I

    was thinking I could these OS dependent functions from the main ULP. I

    would then create three different include files one for each OS in which

    each of these functions is adjusted for the needs of the OS. At the

    beginning of the main ULP is would detect what OS it's running under and

    then only include those function definitions. Logistically this seems

    easier to manage to me.

     

    The other option would be to modify these functions in place and use

    something like a switch statement within these functions to run the OS

    specific code. This has the advantage of keeping everything in one file.

     

    What would you guys recommend? Feel free to suggest any other approach

    you think might be suitable.

     

    Thanks everyone for your attention.

     

    Best Regards,

    Jorge Garcia

     

     

     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • dukepro
    dukepro over 9 years ago in reply to autodeskguest

    On 10/12/2016 06:09 PM, Jorge Garcia wrote:

     

    Now I'd like to ask for your opinions on how to proceed. I'm currently

    trying to determine what the best implementation would be. On one hand

    I was thinking I could these OS dependent functions from the main ULP.

    I would then create three different include files one for each OS in

    which each of these functions is adjusted for the needs of the OS. At

    the beginning of the main ULP is would detect what OS it's running

    under and then only include those function definitions. Logistically

    this seems easier to manage to me.

     

    The other option would be to modify these functions in place and use

    something like a switch statement within these functions to run the OS

    specific code. This has the advantage of keeping everything in one file.

     

    There are two primary reasons for separating code into different files.

    The first is isolation.  By having separate compilation units, must of

    the code internal to functions is hidden from callers, thereby offering

    a layer of security by denying other compilation units access to the

    inner workings of the function.  The second primary (can one even have a

    "second" primary?) reason is maintainability.  By having all related

    variables and code in one source file makes it much easier to maintain.

     

    However, specific to Eagle, ULP is not a compiled language.  It's a

    scripting language that is interpreted at run time.  It does not support

    linkages to external modules.  This somewhat nullifies the first reason

    for having separate files leaving maintainability as the only motivation

    for separate files.  That unto itself is enough reason for separate files.

     

    With that in mind, the downside of having separate files is

    distribution.  A file is not being distrubted any more; instead a

    package of files is being distributed.  Separate files would best be

    distributed as a compressed archive, such as zip, 7z, or tar/gzip.  It

    is a good bet that all of us have used compressed archives in one form

    or another.  So, I don't see that as enough motivation to abandon

    separate files and use an all-in-one ULP.

     

    Bottom line, I suggest using OS-specific files.  To go one further, I

    would suggest that the OS detection not be done in the main file, but

    instead be done in a separate file:

     

        ltspice.ulp:

     

            ...

            #include "oslib.ulp"

            ...

     

        oslib.ulp:

     

            string osStr;

            osStr = detect_os();

            // osStr now contains either "win", "lin", or "mac"

            #include "system-" + osStr + ".ulp"

            #include "filecopy-" + osstr + ".ulp"

            ...

     

    But, this isn't going to work.  First, #include requires a string

    constant.  Second, #include is not a statement - it's a preprocessor

    directive.  Consider the following construct:

     

        int cmd;

        cmd = 2;

     

        if (cmd == 1) {

                #include "true.ulp"

        } else {

                #include "false.ulp"

        }

     

    One might expect that this example of conditional includes would include

    only "false.ulp".  But because #include is a preprocessor directive,

    Eagle will try to include BOTH of the files.  Additionally, Eagle

    doesn't have any preprocessor conditionals that would allow:

     

        #if OS == OS_WIN

            #include "filecopy-win.ulp"

            #include "system-win.ulp"

        #elseif OS == OS_MAC

            #include "filecopy-mac.ulp"

            #include "system-mac.ulp"

        #elseif OS == OS_LIN

            #include "filecopy-lin.ulp"

            #include "system-lin.ulp"

        #else

            #error "invalid value for OS"

        #endif

     

     

    So, that's out as well.

     

    Two things left to do... I'll talk about the ugly one first.

     

    Consider a function called filecopy that does something different for

    each OS:

     

        filecopy.ulp:

        int filecopy(string to, string from) {

            int rc;

            if (os == OS_WIN) {

                rc = ... do windows copy here

            } else if (os == OS_MAC || os == OS_LIN) {

                rc = ... copy mac files here

            }

            return rc;

        }

     

    Yuck.  This means that code for all supported OS's must be in memory.

     

    A cleaner method is to determine the OS at install time, not at run

    time.  The distribution ZIP file (and I use "ZIP" generically, of

    course) would contain the main ulp, then three nested zip files - one

    for each OS.  The use would determine which os-specific zip file to

    unzip.  The ULP files within each os-specific zip would contain a

    collection of ULP's that abstract the nuances of each OS to a common

    interface.

     

        JGprog.zip:

            JGprog.ulp

            oslib-lin.zip

            oslib-win.zip

            oslib-mac.zip

     

    There are several benefits to this approach:

     

     

    • The detection of the underlying OS is determined once at install

        time by the user.

     

    • Code for only a single OS is included from JGprog.ulp.

     

    • CPU cycles are not wasted when determining which os-specific code

        should be executed.

     

     

    Jorge, What you're building here is a library that abstracts os-specific

    functions.  With a little bit of planning, this library can be designed

    to be extensible, and used by other ULP's.

     

    Of course, there are as many opinions as there are engineers.  My

    preceding monologue was not meant to put the reader to sleep, but

    instead it was meant to consider an approach that had not yet been

    mentioned, and that at least bears discussion.

     

    HTH,

        - Chuck

     

     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • rachaelp
    rachaelp over 9 years ago in reply to dukepro

    Chuck Huber wrote:

     

    A cleaner method is to determine the OS at install time, not at run time. The distribution ZIP file (and I use "ZIP" generically, of course) would contain the main ulp, then three nested zip files - one for each OS. The use would determine which os-specific zip file to unzip. The ULP files within each os-specific zip would contain a collection of ULP's that abstract the nuances of each OS to a common interface.

     

    JGprog.zip:

    JGprog.ulp

    oslib-lin.zip

    oslib-win.zip

    oslib-mac.zip

     

    There are several benefits to this approach:

     

     

    • The detection of the underlying OS is determined once at install time by the user.

     

    • Code for only a single OS is included from JGprog.ulp.

     

    • CPU cycles are not wasted when determining which os-specific code should be executed.

    Yes, this please! Well a combination of this and what I (and subsequently Chuck) said. I'd still pull the OS specific stuff out into it's own generic and much more useful OS abstraction lib and then use calls to that library from the ULP functions that need to make OS specific calls. Then do as Chuck suggests above and make it deal with installing the correct OS specific library at install time.

     

    Best Regards,

     

    Rachael

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 9 years ago in reply to dukepro

    Bottom line, I suggest using OS-specific files.  To go one further, I

    would suggest that the OS detection not be done in the main file, but

    instead be done in a separate file:

     

        ltspice.ulp:

     

            ...

            #include "oslib.ulp"

            ...

     

        oslib.ulp:

     

            string osStr;

            osStr = detect_os();

            // osStr now contains either "win", "lin", or "mac"

            #include "system-" + osStr + ".ulp"

            #include "filecopy-" + osstr + ".ulp"

            ...

     

    But, this isn't going to work.  First, #include requires a string

    constant.  Second, #include is not a statement - it's a preprocessor

    directive.  Consider the following construct:

     

        int cmd;

        cmd = 2;

     

        if (cmd == 1) {

                #include "true.ulp"

        } else {

                #include "false.ulp"

        }

     

    One might expect that this example of conditional includes would include

    only "false.ulp".  But because #include is a preprocessor directive,

    Eagle will try to include BOTH of the files.  Additionally, Eagle

    doesn't have any preprocessor conditionals that would allow:

     

        #if OS == OS_WIN

            #include "filecopy-win.ulp"

            #include "system-win.ulp"

        #elseif OS == OS_MAC

            #include "filecopy-mac.ulp"

            #include "system-mac.ulp"

        #elseif OS == OS_LIN

            #include "filecopy-lin.ulp"

            #include "system-lin.ulp"

        #else

            #error "invalid value for OS"

        #endif

     

     

    So, that's out as well.

     

    Hi Chuck,

     

    Aghhh!!! I totally didn't realize that the ULP language didn't support

    preprocessor if, elseif. Well, it's better to figure that out now rather

    then when I'm knee deep in the implementation.

     

    A cleaner method is to determine the OS at install time, not at run

    time.  The distribution ZIP file (and I use "ZIP" generically, of

    course) would contain the main ulp, then three nested zip files - one

    for each OS.  The use would determine which os-specific zip file to

    unzip.  The ULP files within each os-specific zip would contain a

    collection of ULP's that abstract the nuances of each OS to a common

    interface.

     

        JGprog.zip:

            JGprog.ulp

            oslib-lin.zip

            oslib-win.zip

            oslib-mac.zip

     

    There are several benefits to this approach:

     

     

    • The detection of the underlying OS is determined once at install

        time by the user.

     

    • Code for only a single OS is included from JGprog.ulp.

     

    • CPU cycles are not wasted when determining which os-specific code

        should be executed.

     

    I'm not too concerned about distribution since this would ship with all

    three main distributions of EAGLE.

     

    I'm also not sure if I want to go as far as creating a framework that

    would handle os-specific functionality for ULPs. I do think that is a

    really good idea but not something I want to add to the scope of the

    current project.

     

    I agree that the best way to proceed right now is going to be to split

    the ULP into a few files to make everything manageable and that is going

    to be the approach I follow from here on in.

     

    I'm going to go figure out git now, my goal for next week is to have

    this project up on github so that more eyes can look at the code and to

    open the possibility for collaboration should anyone want to give me a hand.

     

    Thanks everyone.

     

    Best Regards,

    Jorge Garcia

     

     

     

     

     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • dukepro
    dukepro over 9 years ago in reply to autodeskguest

    On 10/13/2016 03:13 PM, Jorge Garcia wrote:

    ...

    Additionally, Eagle

    doesn't have any preprocessor conditionals that would allow:

     

        #if OS == OS_WIN

            #include "filecopy-win.ulp"

            #include "system-win.ulp"

        #elseif OS == OS_MAC

            #include "filecopy-mac.ulp"

            #include "system-mac.ulp"

        #elseif OS == OS_LIN

            #include "filecopy-lin.ulp"

            #include "system-lin.ulp"

        #else

            #error "invalid value for OS"

        #endif

     

     

    So, that's out as well.

     

    Hi Chuck,

     

    Aghhh!!! I totally didn't realize that the ULP language didn't support

    preprocessor if, elseif. Well, it's better to figure that out now

    rather then when I'm knee deep in the implementation.

     

    I should qualify that... There are no /documented/ conditional

    directives.  That's as of the 7.2 ULP docs.

     

    A cleaner method is to determine the OS at install time, not at run

    time.  The distribution ZIP file (and I use "ZIP" generically, of

    course) would contain the main ulp, then three nested zip files - one

    for each OS.  The use would determine which os-specific zip file to

    unzip.  The ULP files within each os-specific zip would contain a

    collection of ULP's that abstract the nuances of each OS to a common

    interface.

     

        JGprog.zip:

            JGprog.ulp

            oslib-lin.zip

            oslib-win.zip

            oslib-mac.zip

     

    There are several benefits to this approach:

     

     

    • The detection of the underlying OS is determined once at install

        time by the user.

     

    • Code for only a single OS is included from JGprog.ulp.

     

    • CPU cycles are not wasted when determining which os-specific code

        should be executed.

     

    I'm not too concerned about distribution since this would ship with

    all three main distributions of EAGLE.

     

    Okay.  I was thinking more in terms of a package that one would download

    from cadsoft (or whatever it may be called today).

     

     

    I'm also not sure if I want to go as far as creating a framework that

    would handle os-specific functionality for ULPs. I do think that is a

    really good idea but not something I want to add to the scope of the

    current project.

     

    I understand.  My intent was not to suggest an expansion of the scope of

    this project, but merely to consider that what you write today may be

    extended and modified by individual users in years to come to include

    os-specific functionality that is not required by this LTSpice project.

     

    For instance, I might want to take what you write, and add a

    schematic().jumpThroughFlamingHoops() function.  While jumping through

    hoops may be common to all os's, igniting the flames may be implemented

    differently on windows than it is on mac or linux.

     

    Perhaps my metaphor is somewhat out there, though I can think of several

    times in the distant past that I had to fight the urge to set my Windows

    computer on fire.

     

    I guess the point is that as the separation of functions is designed, it

    would be helpful to consider a structure that makes it easy to extend.

     

    Enjoy,

        - Chuck

     

     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • dukepro
    dukepro over 9 years ago in reply to autodeskguest

    On 10/13/2016 03:13 PM, Jorge Garcia wrote:

    ...

    Additionally, Eagle

    doesn't have any preprocessor conditionals that would allow:

     

        #if OS == OS_WIN

            #include "filecopy-win.ulp"

            #include "system-win.ulp"

        #elseif OS == OS_MAC

            #include "filecopy-mac.ulp"

            #include "system-mac.ulp"

        #elseif OS == OS_LIN

            #include "filecopy-lin.ulp"

            #include "system-lin.ulp"

        #else

            #error "invalid value for OS"

        #endif

     

     

    So, that's out as well.

     

    Hi Chuck,

     

    Aghhh!!! I totally didn't realize that the ULP language didn't support

    preprocessor if, elseif. Well, it's better to figure that out now

    rather then when I'm knee deep in the implementation.

     

    I should qualify that... There are no /documented/ conditional

    directives.  That's as of the 7.2 ULP docs.

     

    A cleaner method is to determine the OS at install time, not at run

    time.  The distribution ZIP file (and I use "ZIP" generically, of

    course) would contain the main ulp, then three nested zip files - one

    for each OS.  The use would determine which os-specific zip file to

    unzip.  The ULP files within each os-specific zip would contain a

    collection of ULP's that abstract the nuances of each OS to a common

    interface.

     

        JGprog.zip:

            JGprog.ulp

            oslib-lin.zip

            oslib-win.zip

            oslib-mac.zip

     

    There are several benefits to this approach:

     

     

    • The detection of the underlying OS is determined once at install

        time by the user.

     

    • Code for only a single OS is included from JGprog.ulp.

     

    • CPU cycles are not wasted when determining which os-specific code

        should be executed.

     

    I'm not too concerned about distribution since this would ship with

    all three main distributions of EAGLE.

     

    Okay.  I was thinking more in terms of a package that one would download

    from cadsoft (or whatever it may be called today).

     

     

    I'm also not sure if I want to go as far as creating a framework that

    would handle os-specific functionality for ULPs. I do think that is a

    really good idea but not something I want to add to the scope of the

    current project.

     

    I understand.  My intent was not to suggest an expansion of the scope of

    this project, but merely to consider that what you write today may be

    extended and modified by individual users in years to come to include

    os-specific functionality that is not required by this LTSpice project.

     

    For instance, I might want to take what you write, and add a

    schematic().jumpThroughFlamingHoops() function.  While jumping through

    hoops may be common to all os's, igniting the flames may be implemented

    differently on windows than it is on mac or linux.

     

    Perhaps my metaphor is somewhat out there, though I can think of several

    times in the distant past that I had to fight the urge to set my Windows

    computer on fire.

     

    I guess the point is that as the separation of functions is designed, it

    would be helpful to consider a structure that makes it easy to extend.

     

    Enjoy,

        - Chuck