Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) How do I create a library with a device from a schematic and a board
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 10 replies
  • Subscribers 191 subscribers
  • Views 4668 views
  • Users 0 members are here
Related

How do I create a library with a device from a schematic and a board

dwaring
dwaring over 9 years ago

I want to add a device to my project. It is a BMP180 barometer board from Adafruit. I have the .sch and .brd from the vendor. The board is complete and wired, but when I use the ULP script to export the library I get a library that has no device which represents the board itself, just the components. So there is no connection between the library that was created and the original board. There is no way for me to use this library to add the board to my project. Am I missing something here? What is the point of exporting the library if all you get is the individual parts and the the layout?

 

I am using Eagle 7.7.0

  • Sign in to reply
  • Cancel
Parents
  • rachaelp
    rachaelp over 9 years ago

    David Waring wrote:

     

    I want to add a device to my project. It is a BMP180 barometer board from Adafruit. I have the .sch and .brd from the vendor. The board is complete and wired, but when I use the ULP script to export the library I get a library that has no device which represents the board itself, just the components. So there is no connection between the library that was created and the original board. There is no way for me to use this library to add the board to my project. Am I missing something here? What is the point of exporting the library if all you get is the individual parts and the the layout?

     

    I am using Eagle 7.7.0

    The library export is simply to allow parts used within a board to be exported so they can be used elsewhere or updated within the design if all you have is the .sch and .brd. Otherwise it would be difficult to take an existing design and update it without having to recreate components from scratch if you don't have access to the original libraries.

     

    If you want to create a device which adds the appropriate footprints to allow you to incorporate the Adafruit board into another design then you have to create the library part for that yourself. Creating your own library parts is a fairly simple task and there are loads of good tutorials on how to do it (Adafruit have quite a good tutorial) and there is the EAGLE help too.

     

    Best Regards,

     

    Rachael

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dwaring
    dwaring over 9 years ago in reply to rachaelp

    It seems strange to me that this is true. I can understand how exporting a schematic will allow the things on it to be reused, but if a schematic and a board have been created, then the board itself is obviously a device that could be used in some other board. For example Adafruit goes to the trouble of providing a schematic and board for their barometer, but this can't be used by someone who is trying to put that barometer onto a printed circuit, when that seems like the only reason someone who purchased that barometer would have for the Eagle files. It seems like all the information is there so why not create a device for the board when exporting the library. Again, am I missing something?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 9 years ago in reply to dwaring

    David Waring wrote on Tue, 15 November 2016 13:35

    It seems strange to me that this is true. I can understand how

    exporting a schematic will allow the things on it to be reused, but if a

    schematic and a board have been created, then the board itself is

    obviously a device that could be used in some other board. For example

    Adafruit goes to the trouble of providing a schematic and board for their

    barometer, but this can't be used by someone who is trying to put that

    barometer onto a printed circuit, when that seems like the only reason

    someone who purchased that barometer would have for the Eagle files. It

    seems like all the information is there so why not create a device for

    the board when exporting the library. Again, am I missing something?

     

     

    Hi

    Obviously you are missing something and that is to clearly describe what

    you wish to achieve.

    Reading between the lines I guess you are attempting one of the following.

    (1) You wish to take a barometer board and plug it into a socket on the

    board you are designing.

    (2) You wish to copy the layout of the Adafruit design onto your board and

    surround it with your additions.

     

    Let us know which of the above is your case and someone will be able to

    describe how you should proceed.

     

    The Eagle files are provided in the 'open' world so you have the

    information about the design, no more.  With them you could build a board

    yourself from scratch, rather than buy the finished product from the

    source. Beyond that you can do whatever you want with them. There is no

    promise that you will be able to do what you think you should be able to do

    with them. You are limited by the way Eagle, or any other software,

    functions.

     

    HTH

    Warren

     

     

    --

    http://www.eaglecentral.ca :: The original and best browser access to CadSoft EAGLE support forums.  Supported by EAGLE licenses purchased through us :: http://www.eaglelicenses.com

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dwaring
    dwaring over 9 years ago in reply to autodeskguest

    Warren thanks for your concern but if you could not understand what I was trying to do it is solely because you did not read properly, as evidenced by the first response to my question which clearly understood. Obviously option 1 is what I described. I don't expect software to do just what I think it should do. But I do expect that if there was something that was 99% but just didn't quite do it and it seemed obvious I could try to find out why it didn't go 100% of the way and that is why I asked if there was something that I was missing that made this last step impossible.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • dwaring
    dwaring over 9 years ago in reply to autodeskguest

    Warren thanks for your concern but if you could not understand what I was trying to do it is solely because you did not read properly, as evidenced by the first response to my question which clearly understood. Obviously option 1 is what I described. I don't expect software to do just what I think it should do. But I do expect that if there was something that was 99% but just didn't quite do it and it seemed obvious I could try to find out why it didn't go 100% of the way and that is why I asked if there was something that I was missing that made this last step impossible.