Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) How do I create a library with a device from a schematic and a board
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 10 replies
  • Subscribers 191 subscribers
  • Views 4668 views
  • Users 0 members are here
Related

How do I create a library with a device from a schematic and a board

dwaring
dwaring over 9 years ago

I want to add a device to my project. It is a BMP180 barometer board from Adafruit. I have the .sch and .brd from the vendor. The board is complete and wired, but when I use the ULP script to export the library I get a library that has no device which represents the board itself, just the components. So there is no connection between the library that was created and the original board. There is no way for me to use this library to add the board to my project. Am I missing something here? What is the point of exporting the library if all you get is the individual parts and the the layout?

 

I am using Eagle 7.7.0

  • Sign in to reply
  • Cancel
Parents
  • rachaelp
    rachaelp over 9 years ago

    David Waring wrote:

     

    I want to add a device to my project. It is a BMP180 barometer board from Adafruit. I have the .sch and .brd from the vendor. The board is complete and wired, but when I use the ULP script to export the library I get a library that has no device which represents the board itself, just the components. So there is no connection between the library that was created and the original board. There is no way for me to use this library to add the board to my project. Am I missing something here? What is the point of exporting the library if all you get is the individual parts and the the layout?

     

    I am using Eagle 7.7.0

    The library export is simply to allow parts used within a board to be exported so they can be used elsewhere or updated within the design if all you have is the .sch and .brd. Otherwise it would be difficult to take an existing design and update it without having to recreate components from scratch if you don't have access to the original libraries.

     

    If you want to create a device which adds the appropriate footprints to allow you to incorporate the Adafruit board into another design then you have to create the library part for that yourself. Creating your own library parts is a fairly simple task and there are loads of good tutorials on how to do it (Adafruit have quite a good tutorial) and there is the EAGLE help too.

     

    Best Regards,

     

    Rachael

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dwaring
    dwaring over 9 years ago in reply to rachaelp

    It seems strange to me that this is true. I can understand how exporting a schematic will allow the things on it to be reused, but if a schematic and a board have been created, then the board itself is obviously a device that could be used in some other board. For example Adafruit goes to the trouble of providing a schematic and board for their barometer, but this can't be used by someone who is trying to put that barometer onto a printed circuit, when that seems like the only reason someone who purchased that barometer would have for the Eagle files. It seems like all the information is there so why not create a device for the board when exporting the library. Again, am I missing something?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rachaelp
    rachaelp over 9 years ago in reply to dwaring

    David Waring wrote:

     

    It seems strange to me that this is true.

    And yet it is, as evidenced by what you actually obtained by exporting the library....

    David Waring wrote:

     

    I can understand how exporting a schematic will allow the things on it to be reused, but if a schematic and a board have been created, then the board itself is obviously a device that could be used in some other board.

    And like any other device, you can create a library part for it yourself from the information which is available. In this case it's simple to open the board, work out where the holes and connectors are, and the board dimensions and then go create that as a library part. I dare say I could have done that in a fraction of the time it took for you to write your original post.

    David Waring wrote:

     

    For example Adafruit goes to the trouble of providing a schematic and board for their barometer, but this can't be used by someone who is trying to put that barometer onto a printed circuit, when that seems like the only reason someone who purchased that barometer would have for the Eagle files.

    As an example, someone could purchase a barometer from Adafruit and use it on a prototyping board hooked up to an Arduino to prototype an idea and then incorporate that design directly into a new PCB they were creating themselves in EAGLE by importing the .sch and .brd files into their own design.

    David Waring wrote:

     

    It seems like all the information is there so why not create a device for the board when exporting the library.

    It probably would be possible to write a ULP to create a library part from a board file but it wouldn't be fully automatic as EAGLE wouldn't necessarily be able to work out which parts on the supplied .brd would be external interfaces on the new "device" and it wouldn't know how to create the matching symbol in a usable way necessarily. It could certainly be assisted by a ULP that helped extract information but I don't think it could create a completely usable library part without user intervention. In most cases I suspect it'd just be quicker to create the library part yourself anyway.

    David Waring wrote:

     

    Again, am I missing something?

    Yes. See above.

     

    Best Regards,

     

    Rachael

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dwaring
    dwaring over 9 years ago in reply to rachaelp

    ... as EAGLE wouldn't necessarily be able to work out which parts on the supplied .brd would be external interfaces on the new "device" and it wouldn't know how to create the matching symbol in a usable way necessarily.

     

    That is the part that I was missing. Thank you.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • dwaring
    dwaring over 9 years ago in reply to rachaelp

    ... as EAGLE wouldn't necessarily be able to work out which parts on the supplied .brd would be external interfaces on the new "device" and it wouldn't know how to create the matching symbol in a usable way necessarily.

     

    That is the part that I was missing. Thank you.