Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) How to Measure Creepage Clearances
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 190 subscribers
  • Views 1871 views
  • Users 0 members are here
Related

How to Measure Creepage Clearances

rtzaudio
rtzaudio over 9 years ago

I have a client that is working to get a PCB through UL certification. I

need some way to measure the minimum clearance between any two nets. In

other words I might need to know the minimum clearance between any two

traces/polys (eg, whats the min clearance between +15V and +5V? for

example).

 

Is there any ULP or way to figure the minimum clearance between two

different net signals on a board? Any suggestions would be greatly

appreciated!

 

Best Regards,

 

Bob Starr

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 9 years ago

    Bob Starr schrieb:

    I have a client that is working to get a PCB through UL

    certification. I need some way to measure the minimum clearance

    between any two nets. In other words I might need to know the minimum

    clearance between any two traces/polys (eg, whats the min clearance

    between +15V and +5V? for example).

     

    That's not /exactly/ true. You don't need to (numerically) know the

    minimum distance, you just need to make sure that you don't fall below a

    specified minimum distance anywhere on the board.

     

    However, that makes using CLASS (as already suggested) the perfect

    solution. Simply enter your minimum distance requirements in the matrix,

    assign the nets to the proper classes and run DRC. If DRC does not

    complain, your layout is compliant.

     

    The matrix is simple to use: you just specify the minimum distances for

    signals within the same class and between their own and all other classes.

     

    These distance requirements are also used by polygon calculation, so you

    don't need to check them explicitly - provided you take care of using

    different RANKs where needed.

     

    Final word: enter slightly too large distances in the CLASS distance

    matrix to provide for manufacturing tolerances in the production.

     

    Tilmann

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rtzaudio
    rtzaudio over 9 years ago in reply to autodeskguest

    I found the following in the manual and trying to figure this out between the DRC clearance matrix:

     

    Clearance between net classes

    If a clearance is given in the form number:clearance, it defines the minimum clearance between signals in this net class and signals in the net class with the given number. The command

    CLASS 3 1:0.6mm 2:0.8mm

    defines a minimum clearance of 0.6mm between signals in net classes 1 and 3, and one of 0.8mm between signals in net classes 2 and 3. Note that the numbers in number:clearance must be less than or equal to the number of the net class itself ('3' in the above example), so

    CLASS 3 1:0.6mm 2:0.8mm 3:0.2mm

    would also be valid, whereas

    CLASS 3 1:0.6mm 2:0.8mm 3:0.2mm 4:0.5mm

    would not be allowed.

    A clearance value of '0' between two net classes means, there is no specific value. Then the higher value of the participating net classes will be used.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 9 years ago in reply to rtzaudio

    Bob Starr schrieb:

    I found the following in the manual and trying to figure this out

    between the DRC clearance matrix:

    .....

     

    Why don't you simply enter CLASS and then expand the matrix with the

    button in the lower right corner?

     

    Tilmann

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 9 years ago in reply to rtzaudio

    Bob Starr schrieb:

    I found the following in the manual and trying to figure this out

    between the DRC clearance matrix:

    .....

     

    Why don't you simply enter CLASS and then expand the matrix with the

    button in the lower right corner?

     

    Tilmann

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • rtzaudio
    rtzaudio over 9 years ago in reply to autodeskguest

    I was able to get the info I needed in the DRC matrix mode, now we'll see what the UL guy says.

     

    Thanks for the help, now I finally have a basic understanding of how to use matrix mode.

     

    Best Regards!

     

    Bob

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14candies
    e14candies over 9 years ago in reply to autodeskguest

    I asked a similar question not too long ago:

     

    Would be nice to have as part of the measuring tool--Eagle already has the

    capability built in, since it can run DRC rules.

     

    http://www.eaglecentral.ca/index.php/m/167295/be3518208fb87eb707150ee1fad3d02e/#msg_167295

     

     

    --

    http://www.eaglecentral.ca :: The original and best browser access to CadSoft EAGLE support forums.  Supported by EAGLE licenses purchased through us :: http://www.eaglelicenses.com