Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Cut net in schematic editor
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 188 subscribers
  • Views 574 views
  • Users 0 members are here
Related

Cut net in schematic editor

autodeskguest
autodeskguest over 9 years ago

Hi when using the cutting tool in the schematic editor, it would be nice

if the cuts could snap to the nearest grid point and each cut segment

not be shorter then 1 grid unit.

 

I think it would even be acceptable to just remove one net segment

between two adjacent grid points when the knife passes between them.

 

Since everything in this editor works off a common .1 grid it's a pain

to have line segments shorter. Lots of fix-up work required.

 

Glenn

 

  • Sign in to reply
  • Cancel
  • rachaelp
    rachaelp over 9 years ago in reply to autodeskguest

    Jorge Garcia wrote on Tue, 24 January 2017 20:46

    If you are talking about the slice tool, you can specify a width so so

    just set the width to be two grid points (0.2 inches) and I think you'll

    be set.

     

     

    HI Jorge,

     

    I've just tried this and as far as I can see there are two issues:

     

    First it doesn't appear there is anywhere to set this as a default so you

    can only specify it on the command line?

     

    Second, the slice does not snap to grid so when you do this is puts a 0.2in

    cut around wherever it happens to be sliced which is unlikely to be exactly

    on grid.

     

    Best Regards,

     

    Rachael

    --

    EAGLE support forums at http://www.eaglecentral.ca :: Where the EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 9 years ago

    On 1/23/2017 11:32 PM, Glenn Jones wrote:

    Hi when using the cutting tool in the schematic editor, it would be nice

    if the cuts could snap to the nearest grid point and each cut segment

    not be shorter then 1 grid unit.

     

    I think it would even be acceptable to just remove one net segment

    between two adjacent grid points when the knife passes between them.

     

    Since everything in this editor works off a common .1 grid it's a pain

    to have line segments shorter. Lots of fix-up work required.

     

    Glenn

     

    Hi Glenn,

     

    If you are talking about the slice tool, you can specify a width so so

    just set the width to be two grid points (0.2 inches) and I think you'll

    be set.

     

    Let me know if there's anything else I can do for you.

     

    Best Regards,

    Jorge Garcia