Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) EAGLE v8.0 causes icons to revert to classic style w hen subsequently opening v7.7
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 187 subscribers
  • Views 394 views
  • Users 0 members are here
Related

EAGLE v8.0 causes icons to revert to classic style w hen subsequently opening v7.7

rachaelp
rachaelp over 9 years ago

Hello,

 

I've been playing about with v8.0 over the last week but today went back to

v7.7 and was presented with a UI that had strange icons I didn't

recognise!

 

Upon checking the settings I found the "Classic icon style" checkbox was

ticked. I presume this is because v8.0 no longer has this so removed the

setting from the EAGLE config file causing it to default on in v7. Now for

some this might be seen as a pro for v8 as they don't like the new style

icons but I do and I don't want to have to keep changing the setting back

and restarting every time I switch from v8.0 to v7.7. Could you please fix

this for the next release?

 

It begs the question, are there any other settings which are accidentally

being altered which might be more subtle and not so easily spotted?

 

Can you please make sure that v8 preserves the integrity and backwards

compatibility of the config files?

 

Many thanks,

 

Rachael

--

EAGLE support forums at http://www.eaglecentral.ca :: Where the EAGLE community meets.

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 9 years ago

    rachaelp wrote on Tue, 24 January 2017 15:43

    Hello,

     

    I've been playing about with v8.0 over the last week but today went

    back to v7.7 and was presented with a UI that had strange icons I didn't

    recognise!

     

    Upon checking the settings I found the "Classic icon style" checkbox

    was ticked. I presume this is because v8.0 no longer has this so removed

    the setting from the EAGLE config file causing it to default on in v7.

    Now for some this might be seen as a pro for v8 as they don't like the

    new style icons but I do and I don't want to have to keep changing the

    setting back and restarting every time I switch from v8.0 to v7.7. Could

    you please fix this for the next release?

     

    It begs the question, are there any other settings which are

    accidentally being altered which might be more subtle and not so easily

    spotted?

     

    Can you please make sure that v8 preserves the integrity and backwards

    compatibility of the config files?

     

    Many thanks,

     

    Rachael

     

     

    It sounds like Autodesk didn't fix the problem that has plagued all major

    EAGLE upgrades--overwriting the .eaglerc file.  Is it really that hard to

    create .eagle8rc and use .eagle8rc for V8 so that new installations don't

    trounce over the file?

     

    When you install a brand new version (v7 -> v8) EAGLE should be smart

    enough to create the new version of the file and import all the settings

    from the older version that can be carried forward (perhaps after asking

    the user if they'd like to do this).

     

    With all the other files each user should keep those separate (libraries,

    custom ULP's, etc) so that upgrading won't effect them.  But we have no

    control over the .eaglerc file and that screws things up every time.  Yes,

    there is a command line option to use a new version but that is going to be

    missed by 99% of the people.  If EAGLE would just use a config file with

    the major version in the filename and the problem is solved.

     

    Cheers,

     

    James.

     

    --

    James Morrison  ~~~  Stratford Digital

    http://www.stratforddigital.ca

    --

    EAGLE support forums at http://www.eaglecentral.ca :: Where the EAGLE community meets.

     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 9 years ago in reply to autodeskguest

    With all the other files each user should keep those separate (libraries,

    custom ULP's, etc) so that upgrading won't effect them.  But we have no

    control over the .eaglerc file and that screws things up every time.  Yes,

    there is a command line option to use a new version but that is going to be

    missed by 99% of the people.  If EAGLE would just use a config file with

    the major version in the filename and the problem is solved.

     

    Cheers,

     

    James.

     

     

    Hi James,

     

    You beat me to it. I'll put in a request with a variant of your

    recommended solution so that this can be implemented soon.

     

    It's been too long for such a small issue that could be easily rectified.

     

    Best Regards,

    Jorge Garcia

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 9 years ago in reply to autodeskguest

    With all the other files each user should keep those separate (libraries,

    custom ULP's, etc) so that upgrading won't effect them.  But we have no

    control over the .eaglerc file and that screws things up every time.  Yes,

    there is a command line option to use a new version but that is going to be

    missed by 99% of the people.  If EAGLE would just use a config file with

    the major version in the filename and the problem is solved.

     

    Cheers,

     

    James.

     

     

    Hi James,

     

    You beat me to it. I'll put in a request with a variant of your

    recommended solution so that this can be implemented soon.

     

    It's been too long for such a small issue that could be easily rectified.

     

    Best Regards,

    Jorge Garcia