Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) mosfet dilemma
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1 reply
  • Subscribers 187 subscribers
  • Views 322 views
  • Users 0 members are here
Related

mosfet dilemma

msrinivasan19995
msrinivasan19995 over 9 years ago

guys i'm going to use  two 40v mosfet in synchronous mode of operation for my buck converter. I have chosen SON package type. I have doubt regarding its structure. It has 4 drain, 3 source, 1 gate. Can we use two mosfet in the same  single package or 2 different packages are required. I can't understand why different modules various drains and source are available for single package.I 'm sharing the IC which i'm going to use. Suggestions are welcome.

CSD18512Q5B 40V N-Channel NexFETTm Power MOSFET | TI.com

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 9 years ago

    On 01/28/2017 07:04 AM, srinivasan m wrote:

    Can we use two mosfet in the same  single package or 2 different packages are required.

    There is only one fet in that part-package. The extra leads are to

    increase current and thermal dissipation of the part.

     

    Paul

     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 9 years ago

    On 01/28/2017 07:04 AM, srinivasan m wrote:

    Can we use two mosfet in the same  single package or 2 different packages are required.

    There is only one fet in that part-package. The extra leads are to

    increase current and thermal dissipation of the part.

     

    Paul