Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Dual stacked combo dsub connector needed
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 9 replies
  • Subscribers 189 subscribers
  • Views 1180 views
  • Users 0 members are here
  • dual stacked db dsub
Related

Dual stacked combo dsub connector needed

steve@teradiode.com
steve@teradiode.com over 9 years ago

I am looking for an Eagle symbol and footprint for dual stacked combo dsub connectors specifically Norcomp  179-009-413R571179-009-413R571 which is a right angle DB9/DB9 plug/receptacle with female gender lower and male upper

Typically these dual stacked DB connectors have their upper connector pin positions further away from the board edge than the lower connector.  The upper set are located at the same distance from the board edge as as a version of a single DB connector with deeper backset distance.  So it would be possible to just take an existing single DB connector with deeper setback footprint and use that.

 

The lower connector also has a footprint matching a single DB connector with closer backset.  However, its mounting holes are aligned with the row of pins nearest the board edge instead of centered between the two rows (as in standard for single DB connectors).

http://www.norcomp.net/rohspdfs/Connectors/17Y/179/413/179-YYY-413R571.pdf

http://www.norcomp.net/rohspdfs/Connectors/17Y/179/413/179-YYY-413R571.pdf

Steve

  • Sign in to reply
  • Cancel
Parents
  • geralds
    geralds over 9 years ago

    Hi,

     

    search for con-subd.lbr in the library - there you'll find a connector from NorComp.

    Then there search for 182-009-MALE as reference.

     

    This allows you to build your connector with the given drawing diagram.
    (You can also copy it into your created lib file.)
    This reference helps in dimensioning and drawing the required reference lines.
    With these reference lines, you can set your footprint also the limit of this housing.

    Tip: You can draw your reference lines in a separate new layer and also switch between the grids.
    You need more than a 0.318 " grid (eg layer 200 or whatever you want ...)

     

    Sometimes it would be faster to create your own device and footprint.

     

    Regards,

    Gerald

    ---

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • steve@teradiode.com
    steve@teradiode.com over 9 years ago in reply to geralds

    Any pointers on how within the one component to have two sets of pins 1 through 9, one for top and one for bottom instead of pins 1 through 18 ?  So the references end up something like X1T-1..X1T-9 and X1B-1..X1B-9 ?

    Steve

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • steve@teradiode.com
    steve@teradiode.com over 9 years ago in reply to geralds

    Any pointers on how within the one component to have two sets of pins 1 through 9, one for top and one for bottom instead of pins 1 through 18 ?  So the references end up something like X1T-1..X1T-9 and X1B-1..X1B-9 ?

    Steve

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • rachaelp
    rachaelp over 9 years ago in reply to steve@teradiode.com

    Steve Parus wrote on Thu, 09 February 2017 17:44

    Any pointers on how within the one component to have two sets of pins 1

    through 9, one for top and one for bottom instead of pins 1 through 18

    ?  So the references end up something like X1T-1..X1T-9 and X1B-1..X1B-9

    ?

    Steve

     

    --

    To view any images and attachments in this post, visit:

    https://www.element14.com/community/message/215530

     

     

    Hi Steve,

     

    You can just name the pins T1 through T9 and B1 through B9.

     

    Best Regards,

     

    Rachael

    --

    EAGLE support forums at http://www.eaglecentral.ca :: Where the EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rachaelp
    rachaelp over 9 years ago in reply to steve@teradiode.com

    Steve Parus wrote on Thu, 09 February 2017 17:44

    Any pointers on how within the one component to have two sets of pins 1

    through 9, one for top and one for bottom instead of pins 1 through 18

    ?  So the references end up something like X1T-1..X1T-9 and X1B-1..X1B-9

    ?

    Steve

     

    --

    To view any images and attachments in this post, visit:

    https://www.element14.com/community/message/215530

     

     

    Hi Steve,

     

    You can just name the pins T1 through T9 and B1 through B9.

     

    Best Regards,

     

    Rachael

    --

    EAGLE support forums at http://www.eaglecentral.ca :: Where the EAGLE community meets.