Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Dual stacked combo dsub connector needed
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 9 replies
  • Subscribers 189 subscribers
  • Views 1180 views
  • Users 0 members are here
  • dual stacked db dsub
Related

Dual stacked combo dsub connector needed

steve@teradiode.com
steve@teradiode.com over 9 years ago

I am looking for an Eagle symbol and footprint for dual stacked combo dsub connectors specifically Norcomp  179-009-413R571179-009-413R571 which is a right angle DB9/DB9 plug/receptacle with female gender lower and male upper

Typically these dual stacked DB connectors have their upper connector pin positions further away from the board edge than the lower connector.  The upper set are located at the same distance from the board edge as as a version of a single DB connector with deeper backset distance.  So it would be possible to just take an existing single DB connector with deeper setback footprint and use that.

 

The lower connector also has a footprint matching a single DB connector with closer backset.  However, its mounting holes are aligned with the row of pins nearest the board edge instead of centered between the two rows (as in standard for single DB connectors).

http://www.norcomp.net/rohspdfs/Connectors/17Y/179/413/179-YYY-413R571.pdf

http://www.norcomp.net/rohspdfs/Connectors/17Y/179/413/179-YYY-413R571.pdf

Steve

  • Sign in to reply
  • Cancel
Parents
  • rachaelp
    rachaelp over 9 years ago

    Hi Steve,

     

    I don't know if there is such a part buried in the existing EAGLE libraries somewhere as I don't use them. If you've found a similar single connector you could start with that, copy it and then modify it to match your dual stacked connector.

     

    Alternatively, and IMHO the better way, is to just go ahead and create the library part yourself from scratch. Looking at the data sheet you linked it gives the recommended PCB footprint with all the dimensions needed so it will be fairly trivial to create from scratch. Are you familiar with creating EAGLE library parts yourself? If you aren't then go through the manual and look at some online tutorials. Adafruit and Dangerous Prototypes both do some reasonable guides to get people up and running with creating EAGLE libraries and there is always lots of help in these forums if you get stuck.

     

    Best Regards,

     

    Rachael

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • rachaelp
    rachaelp over 9 years ago

    Hi Steve,

     

    I don't know if there is such a part buried in the existing EAGLE libraries somewhere as I don't use them. If you've found a similar single connector you could start with that, copy it and then modify it to match your dual stacked connector.

     

    Alternatively, and IMHO the better way, is to just go ahead and create the library part yourself from scratch. Looking at the data sheet you linked it gives the recommended PCB footprint with all the dimensions needed so it will be fairly trivial to create from scratch. Are you familiar with creating EAGLE library parts yourself? If you aren't then go through the manual and look at some online tutorials. Adafruit and Dangerous Prototypes both do some reasonable guides to get people up and running with creating EAGLE libraries and there is always lots of help in these forums if you get stuck.

     

    Best Regards,

     

    Rachael