Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Dual stacked combo dsub connector needed
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 9 replies
  • Subscribers 189 subscribers
  • Views 1187 views
  • Users 0 members are here
  • dual stacked db dsub
Related

Dual stacked combo dsub connector needed

steve@teradiode.com
steve@teradiode.com over 9 years ago

I am looking for an Eagle symbol and footprint for dual stacked combo dsub connectors specifically Norcomp  179-009-413R571179-009-413R571 which is a right angle DB9/DB9 plug/receptacle with female gender lower and male upper

Typically these dual stacked DB connectors have their upper connector pin positions further away from the board edge than the lower connector.  The upper set are located at the same distance from the board edge as as a version of a single DB connector with deeper backset distance.  So it would be possible to just take an existing single DB connector with deeper setback footprint and use that.

 

The lower connector also has a footprint matching a single DB connector with closer backset.  However, its mounting holes are aligned with the row of pins nearest the board edge instead of centered between the two rows (as in standard for single DB connectors).

http://www.norcomp.net/rohspdfs/Connectors/17Y/179/413/179-YYY-413R571.pdf

http://www.norcomp.net/rohspdfs/Connectors/17Y/179/413/179-YYY-413R571.pdf

Steve

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 9 years ago

    Am 09.02.2017 um 17:30 schrieb Steve Parus:

    I am looking for an Eagle symbol and footprint for dual stacked combo dsub connectors specifically Norcomp  179-009-413R571179-009-413R571 which is a right angle DB9/DB9 plug/receptacle with female gender lower and male upper

    Typically these dual stacked DB connectors have their upper connector pin positions further away from the board edge than the lower connector.  The upper set are located at the same distance from the board edge as as a version of a single DB connector with deeper backset distance.  So it would be possible to just take an existing single DB connector with deeper setback footprint and use that.

     

    The lower connector also has a footprint matching a single DB connector with closer backset.  However, its mounting holes are aligned with the row of pins nearest the board edge instead of centered between the two rows (as in standard for single DB connectors).

    http://www.norcomp.net/rohspdfs/Connectors/17Y/179/413/179-YYY-413R571.pdf

    http://www.norcomp.net/rohspdfs/Connectors/17Y/179/413/179-YYY-413R571.pdf

    Steve

     

    --

    To view any images and attachments in this post, visit:

    https://www.element14.com/community/message/215526

     

     

    Check the con-subd library. Maybe you con modify something from  there.

     

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag

     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 9 years ago

    Am 09.02.2017 um 17:30 schrieb Steve Parus:

    I am looking for an Eagle symbol and footprint for dual stacked combo dsub connectors specifically Norcomp  179-009-413R571179-009-413R571 which is a right angle DB9/DB9 plug/receptacle with female gender lower and male upper

    Typically these dual stacked DB connectors have their upper connector pin positions further away from the board edge than the lower connector.  The upper set are located at the same distance from the board edge as as a version of a single DB connector with deeper backset distance.  So it would be possible to just take an existing single DB connector with deeper setback footprint and use that.

     

    The lower connector also has a footprint matching a single DB connector with closer backset.  However, its mounting holes are aligned with the row of pins nearest the board edge instead of centered between the two rows (as in standard for single DB connectors).

    http://www.norcomp.net/rohspdfs/Connectors/17Y/179/413/179-YYY-413R571.pdf

    http://www.norcomp.net/rohspdfs/Connectors/17Y/179/413/179-YYY-413R571.pdf

    Steve

     

    --

    To view any images and attachments in this post, visit:

    https://www.element14.com/community/message/215526

     

     

    Check the con-subd library. Maybe you con modify something from  there.

     

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag

     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • geralds
    geralds over 9 years ago in reply to autodeskguest

    Hi Joern,

    Yeah, you was a little bit faster....image I wrote at the same time as you posted.

     

    Gerald

    ---