EAGLE User Support (English) Wanted - PC borad or example schematics
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
  • Replies 48 replies
  • Subscribers 193 subscribers
  • Views 4966 views
  • Users 0 members are here
Related

Wanted - PC borad or example schematics

autodeskguest
autodeskguest over 9 years ago

 

Hi

 

Can anyone helP?

 

I'm looking for a CPU board with some rom(or flash or whatever) some ram and

USB I/O  but little or nothing else. (IE No video chips etc)

IE Minimal bare metal.

 

CPU to be as powerful as possible - If theres an X86-64 board that would be ideal.

I could use 32 or 64 bit CPU. Power is my key factor. (I dont want a

multiprocessor board or "network")

 

I'm happy to buy an existing board to meet my needs or could build one if

a suitable circuit example exists.

 

The only eagle design I can find is an atmel which is clearly no good to me.

 

Does anyone have any ideas?

 

Thanks

 

colin

 

 

 

  • Sign in to reply
  • Cancel

Top Replies

  • rachaelp
    rachaelp over 9 years ago in reply to autodeskguest +4
    colin[2] wrote: Everybody please - thank you - I'm done. Good for you! colin[2] wrote: Hopefully that answers the daft comment about "prejudice" earlier. also. Repeatedly demanding more information "so…
  • geralds
    geralds over 9 years ago in reply to balearicdynamics +4
    Hi, are sure that the Gizmo board helps? What if he want to build a space shuttle? He didn't describe concrete what he want neither for what he need the processor. Gerald ---
  • shabaz
    shabaz over 9 years ago in reply to autodeskguest +3
    Hi Colin, Everyone here has been trying to read sufficient engineering requirements from you, but the information is too vague to help in any meaningful way. In fact, your first post didn't quantify a…
Parents
  • dukepro
    dukepro over 9 years ago

    On 02/23/2017 07:20 AM, colin wrote:

     

    Hi

     

    Can anyone helP?

     

    I'm looking for a CPU board with some rom(or flash or whatever) some ram and

    USB I/O  but little or nothing else. (IE No video chips etc)

    IE Minimal bare metal.

     

    CPU to be as powerful as possible - If theres an X86-64 board that would be ideal.

    I could use 32 or 64 bit CPU. Power is my key factor. (I dont want a

    multiprocessor board or "network")

     

    I'm happy to buy an existing board to meet my needs or could build one if

    a suitable circuit example exists.

     

    The only eagle design I can find is an atmel which is clearly no good to me.

     

    Does anyone have any ideas?

     

    Thanks

     

    colin

     

     

     

    Take a look at Technologic Systems.  They have multiple configurations

    of ARM and Intel single board computers.  They are also willing to

    design a board of your choice.

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 9 years ago in reply to dukepro

    In article <o8mqeg$572$1@baboon.cadsoft.de>, chuck.huber@dukepro.com

    says...

     

     

    Thanks for both responses.

     

    I've taken a look at the suggestions but neither seems suitable.

    Either processors with everything including the kitchen sink crippling the silicon

    or just not enough oomph - (ARMS are too underpowered for my use I think -

    and seem extraordinarily complex to set up to try and be all things to all people)

     

    Unless I've missed something or missunderstood the very complex world

    of CPU's today nobody is buildng a powerful optimised processor.

    If I needed graphics output I could look at GPU's but again the current use

    seems to preclude just "processing"  The extra stuff just complicates matters.

     

    I guess I'm going t have to make massive compromises to get anything

    to work - but its a bit suprising.

     

    Unless I've missed something or missunderstood.

     

    but thanks again.

     

    colin

     

     

     

     

     

    On 02/23/2017 07:20 AM, colin wrote:

     

    Hi

     

    Can anyone helP?

     

    I'm looking for a CPU board with some rom(or flash or whatever) some ram and

    USB I/O  but little or nothing else. (IE No video chips etc)

    IE Minimal bare metal.

     

    CPU to be as powerful as possible - If theres an X86-64 board that would be ideal.

    I could use 32 or 64 bit CPU. Power is my key factor. (I dont want a

    multiprocessor board or "network")

     

    I'm happy to buy an existing board to meet my needs or could build one if

    a suitable circuit example exists.

     

    The only eagle design I can find is an atmel which is clearly no good to me.

     

    Does anyone have any ideas?

     

    Thanks

     

    colin

     

     

     

    Take a look at Technologic Systems.  They have multiple configurations

    of ARM and Intel single board computers.  They are also willing to

    design a board of your choice.

     

     

     

    --

     

    john

     

    =========================

    http://johntech.co.uk

     

    "Bleeding Edge Forum"

    http://johntech.co.uk/forum/

     

    =========================

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 9 years ago in reply to autodeskguest

    On 25/02/17 11:36, colin wrote:

    (ARMS are too underpowered for my use I think -

    and seem extraordinarily complex to set up to try and be all things to all people)

     

    Unless I've missed something or missunderstood the very complex world

    of CPU's today nobody is buildng a powerful optimised processor.

     

    I think you're being prejudiced and artificially limiting your options

    until you reach the conclusion your grumpiness desires.

     

    If you really need multi-gigahertz 64-bit multi-core then buy a PC. You

    can get CoreI7 miniITX boards. The presence of a (fairly minimal) GPU

    on-chip is NOT costing you anything in performance, any more than it

    disadvantages the gaming community who would sooner cut their own

    private parts out than countenance the use of an on-chip GPU instead of

    a massively over-priced graphics card.

     

    If your actual requirements are less intense - perhaps one GHz quad core

    32-bit - then there are some very reasonably priced (and not at ALL hard

    to set up) ARM devices available. And for a bonus, many of them don't

    have GPUs. Of course, you'll have to actually do some work to design

    those chips onto a board.

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 9 years ago in reply to autodeskguest

    On 25/02/17 11:36, colin wrote:

    (ARMS are too underpowered for my use I think -

    and seem extraordinarily complex to set up to try and be all things to all people)

     

    Unless I've missed something or missunderstood the very complex world

    of CPU's today nobody is buildng a powerful optimised processor.

     

    I think you're being prejudiced and artificially limiting your options

    until you reach the conclusion your grumpiness desires.

     

    If you really need multi-gigahertz 64-bit multi-core then buy a PC. You

    can get CoreI7 miniITX boards. The presence of a (fairly minimal) GPU

    on-chip is NOT costing you anything in performance, any more than it

    disadvantages the gaming community who would sooner cut their own

    private parts out than countenance the use of an on-chip GPU instead of

    a massively over-priced graphics card.

     

    If your actual requirements are less intense - perhaps one GHz quad core

    32-bit - then there are some very reasonably priced (and not at ALL hard

    to set up) ARM devices available. And for a bonus, many of them don't

    have GPUs. Of course, you'll have to actually do some work to design

    those chips onto a board.