EAGLE User Support (English) Wanted - PC borad or example schematics
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
  • Replies 48 replies
  • Subscribers 193 subscribers
  • Views 4966 views
  • Users 0 members are here
Related

Wanted - PC borad or example schematics

autodeskguest
autodeskguest over 9 years ago

 

Hi

 

Can anyone helP?

 

I'm looking for a CPU board with some rom(or flash or whatever) some ram and

USB I/O  but little or nothing else. (IE No video chips etc)

IE Minimal bare metal.

 

CPU to be as powerful as possible - If theres an X86-64 board that would be ideal.

I could use 32 or 64 bit CPU. Power is my key factor. (I dont want a

multiprocessor board or "network")

 

I'm happy to buy an existing board to meet my needs or could build one if

a suitable circuit example exists.

 

The only eagle design I can find is an atmel which is clearly no good to me.

 

Does anyone have any ideas?

 

Thanks

 

colin

 

 

 

  • Sign in to reply
  • Cancel

Top Replies

  • rachaelp
    rachaelp over 9 years ago in reply to autodeskguest +4
    colin[2] wrote: Everybody please - thank you - I'm done. Good for you! colin[2] wrote: Hopefully that answers the daft comment about "prejudice" earlier. also. Repeatedly demanding more information "so…
  • geralds
    geralds over 9 years ago in reply to balearicdynamics +4
    Hi, are sure that the Gizmo board helps? What if he want to build a space shuttle? He didn't describe concrete what he want neither for what he need the processor. Gerald ---
  • shabaz
    shabaz over 9 years ago in reply to autodeskguest +3
    Hi Colin, Everyone here has been trying to read sufficient engineering requirements from you, but the information is too vague to help in any meaningful way. In fact, your first post didn't quantify a…
Parents
  • dougw
    dougw over 9 years ago

    You could take a look at Olimex cards - they are open source with full cad files available.

    The A33-OLinuXino-4GB is a quad core ARM Cortex A7.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 9 years ago in reply to dougw

     

    Everybody ...

     

    Thank you all for the input.

    I appreciate the desire to help but

     

    I'm not looking for a for a microcontroler. quite the reverse really.

    I'm looking for a powerful CPU with no extraneous peripherals

    except  FPU and maybe some form of memory management would be

    ok.Nothing much. on a card I just need I/O and a bit of booting memory

    and some fast I/O - as fast as possible and a USB port prefereable v3.1.

    If nothing on the board  all processor pins socketed

    for access. (This would be the ideal scenario - just a fast processor board)

    Nothing clocked below 1Ghz is likely to be any use.

    I'm not sure about the itaniums - I'll look into that thanks.

    Things that need a PC are no use to me.

    Arm processors are not up to the job.

     

    colin

     

    ps. I've been asked to say please ignore he the johntech.co.uk site I dont have

    email there I'm just using their newsgroup gateway. Someone tried to mail

    me there apparently.

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 9 years ago in reply to autodeskguest

    Sounds like a rare animal.

    If you want a high end Intel chip, the next step after a CPU socket is to add a support chipset, but this is already a full blown PC with all sorts of peripheral I/O.

    Check out the quad Core i7 Kontron AM4024.

    There are a few military CPU modules, but they are targeted at specific systems to achieve a workable infrastructure.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • dougw
    dougw over 9 years ago in reply to autodeskguest

    Sounds like a rare animal.

    If you want a high end Intel chip, the next step after a CPU socket is to add a support chipset, but this is already a full blown PC with all sorts of peripheral I/O.

    Check out the quad Core i7 Kontron AM4024.

    There are a few military CPU modules, but they are targeted at specific systems to achieve a workable infrastructure.