Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Best way to design a stacked PCBs circuits
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 187 subscribers
  • Views 1537 views
  • Users 0 members are here
Related

Best way to design a stacked PCBs circuits

autodeskguest
autodeskguest over 9 years ago

Hello,

I'm going to develop a circuit that will be composed of two stacked PCB.

Several connectors will provide connections between the two layers.

 

I wonder which is the best approach in EAGLE to do this.

The simplest way is of course to make different projects, one for each PCB.

 

The mains drawbacks are:

 

  • lot of signals are the same (those that go with the connectors) so any

changes to their names or net classes must be repeated in the second

project as well

 

  • the same applies for the layout: the positions of mounting holes or

any milling layer must be kept in sync with the PCBs

 

  • last but not least, in the lower PCB I have several tall components.

In the higher PCB I need to provide slots for them. Doing that in

different project is a pain because I need to write down the position of

each one and move the related slots every time I change their placement

 

I hope there is a better way to design stacked PCB circuits!

Thanks

Marco

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 9 years ago

    On 02/27/17 08:42, Marco Trapanese wrote:

    Hello,

    I'm going to develop a circuit that will be composed of two stacked PCB.

    Several connectors will provide connections between the two layers.

     

    I wonder which is the best approach in EAGLE to do this.

    The simplest way is of course to make different projects, one for each PCB.

     

    I've done this twice. Note that I'm a hobbyist and there may be better

    ways to do this.

     

    The first time I had one board hosting a microprocessor and a much

    smaller one hosting the front-panel switches. The board with the

    switches mounted above the uP board using standoffs and a pin header and

    socket. I ended up creating one project and milled break-off tabs

    between the two boards. Aligning the pins in one of the two dimensions

    was easier because the two boards shared a common edge.

     

    The second time I made a set of 5 boards that mount in a stack using

    PC/104 style connectors. These were too large and too complicated to

    implement in one project.

     

    What I did was to create a separate sheet in the schematic for the

    common connector interface. It was fairly easy to copy everything on

    that sheet in the first schematic and paste it into the others. It would

    be nice if Eagle allowed you to include a partial schematic into

    multiple projects, but that wasn't possible when I started the project.

    It may be now; I don't know.

     

    To make sure the connectors all aligned properly I created a library

    part that defined the basic board outline including the positioning of

    the connectors and the mounting holes. Each project then pulls in the

    basic board device on the common connector interface schematic sheet. In

    the layout, the lower left corner of this device is placed at the lower

    left corner of the board dimensions. I suspect you could use one of the

    documentation layers of the device to define the location of your tall

    components.

     

    This approach developed over time, so there may be ways to optimize

    this. For example, I didn't define any of the connector pins in the

    device as having particular nets or functions; I did this in the common

    schematic sheet. In retrospect it seems defining them in the device may

    have been better.

     

    -Reece

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 9 years ago in reply to autodeskguest

    Il 28/02/2017 16:07, Reece R. Pollack ha scritto:

     

    The first time I had one board hosting a microprocessor and a much

    smaller one hosting the front-panel switches. The board with the

    switches mounted above the uP board using standoffs and a pin header and

    socket. I ended up creating one project and milled break-off tabs

    between the two boards. Aligning the pins in one of the two dimensions

    was easier because the two boards shared a common edge.

     

     

    Right now I've used this approach, even if my case was more similar to

    your second example.

     

     

    The second time I made a set of 5 boards that mount in a stack using

    PC/104 style connectors. These were too large and too complicated to

    implement in one project.

     

    What I did was to create a separate sheet in the schematic for the

    common connector interface. It was fairly easy to copy everything on

    that sheet in the first schematic and paste it into the others. It would

    be nice if Eagle allowed you to include a partial schematic into

    multiple projects, but that wasn't possible when I started the project.

    It may be now; I don't know.

     

     

    Interesting, but it could work if each layer is independent - sharing

    only the PCB edges and board-to-board connectors.

     

    My current project is composed of only two stacked PCB but I need to

    provide holes in the top one to grant access to the lower PCB (i.e. to

    reach a trimmer or a screw).

     

    I need to inspect the coordinates (and the sizes that are not so easy to

    measure in EAGLE) of the desired components to place slots and the other

    components on the second PCB.

     

    I know it is a different working approach but I'm wondering if any of

    the other suite for electronic designs out there provide tool for

    stacked PCBs.

     

    Freely speaking: of course a complete support requires a lot of work,

    but it could be simple enough to allow the background of an EAGLE Layout

    window to be transparent and keep synced position and zoom of another

    instance.

     

    In this way it would be easier to design with the other(s) PCB in the

    view (with of course a different value of transparency, to avoid to be

    confused!)

     

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 9 years ago in reply to autodeskguest

    Il 28/02/2017 16:07, Reece R. Pollack ha scritto:

     

    The first time I had one board hosting a microprocessor and a much

    smaller one hosting the front-panel switches. The board with the

    switches mounted above the uP board using standoffs and a pin header and

    socket. I ended up creating one project and milled break-off tabs

    between the two boards. Aligning the pins in one of the two dimensions

    was easier because the two boards shared a common edge.

     

     

    Right now I've used this approach, even if my case was more similar to

    your second example.

     

     

    The second time I made a set of 5 boards that mount in a stack using

    PC/104 style connectors. These were too large and too complicated to

    implement in one project.

     

    What I did was to create a separate sheet in the schematic for the

    common connector interface. It was fairly easy to copy everything on

    that sheet in the first schematic and paste it into the others. It would

    be nice if Eagle allowed you to include a partial schematic into

    multiple projects, but that wasn't possible when I started the project.

    It may be now; I don't know.

     

     

    Interesting, but it could work if each layer is independent - sharing

    only the PCB edges and board-to-board connectors.

     

    My current project is composed of only two stacked PCB but I need to

    provide holes in the top one to grant access to the lower PCB (i.e. to

    reach a trimmer or a screw).

     

    I need to inspect the coordinates (and the sizes that are not so easy to

    measure in EAGLE) of the desired components to place slots and the other

    components on the second PCB.

     

    I know it is a different working approach but I'm wondering if any of

    the other suite for electronic designs out there provide tool for

    stacked PCBs.

     

    Freely speaking: of course a complete support requires a lot of work,

    but it could be simple enough to allow the background of an EAGLE Layout

    window to be transparent and keep synced position and zoom of another

    instance.

     

    In this way it would be easier to design with the other(s) PCB in the

    view (with of course a different value of transparency, to avoid to be

    confused!)