Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Re: Details of making custom pad shapes with polygons.
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1 reply
  • Subscribers 188 subscribers
  • Views 700 views
  • Users 0 members are here
Related

Re: Details of making custom pad shapes with polygons.

autodeskguest
autodeskguest over 9 years ago

On 16/04/2017 12:26 a.m., David Alenhag wrote:

Hello.

 

I know of the steps to make a custom shaped pad in Eagle but I can never make one without generating "width" errors.

 

But I can't figure out how I am supposed to draw a polygon shape that is what I want without using a polygon width set to 0.

 

That is also the only way I know of to get sharp corners since if I use any width at all the corners get rounded due to the line width.

 

What am I missing? do you know?

How do you make a certain polygon shape that adheres to such and such dimensions while using a polygon width that isn't 0?

 

As far as I know I can let Eagle generate a hole load of errors and generate gerber's and have those produced and it may turn out just as I want it but I can't imagine that I am supposed to ignore those errors and even if I where they bother me(of course such things can bothered anyone but the fact that I am autistic makes those errors entirely impossible for me to tolerate), any tip or input on this would be greatly appreciated.

 

I saw a video on youtube which was of a quality low enough to make it impossible for me to be completely sure about the following, but it looked like that the person in that video could draw a polygon with a certain width yet the width was starting at the points that he specified and continued the specified width inwards, so that he could use a width without it ruining the dimensions of he's drawing.

But I have reviewed the entire eagle user interface for options to change so that the width isn't put equally on both sides of the points I specify as the shape but I can't find anything like that and I am hoping I am simply missing some feature or aren't realizing some simple way to do this but I am stomped.

 

Regards

 

--

To view any images and attachments in this post, visit:

https://www.element14.com/community/message/220682

 

 

Hi

You seem to have a good understanding of the considerations when dealing

with polygons.

 

To address some of your questions/comments.

 

A polygon is made of wires and those wires are checked for width when

the DRC check is run so polygon wires must be of a width equal or

greater than the minimum width of wires as set in the DRC.

 

Because the coordinates of a wire are located in the centre of its width

you must draw the polygon smaller than the finished dimensions by an

amount of half the wire width on each edge.

 

As you have established, the corners will be rounded due to the end of

the wires being round. Arcs can have a square end so two arcs meeting

could have a sharp corner. In manufacturing the corner will not be sharp

as it will be bounded by the radius of the scanning beam in the lith

process. Older flash aperture processes may have approached square corners.

 

You have to be realistic. CAD lets you zoom in and see detail that is

irrelevant in the finished article.

 

The trick with polygon wire width is to make it as large as possible to

keep the size of the gerber file low, as every wire in the polygon is

another line in the gerber, and yet make the width small enough to get

the detail you need. Another consideration I try for is the make the

wire no smaller than the minimum width the manufacturer can make a

single trace. In that way you remove one more thing that their process

could trip up on.

 

So a technique I use when I need a polygon inside the dimensions

provided is to first draw that polygon with a width of zero on another

user defined layer. This acts as a guide for the real polygon. You can

delete this later.

 

Next set the grid to finest. I would use the alternate grid for this.

 

Then on the signal layer you draw the the real polygon inside the

guiding polygon. Use the same number of segments in the polygon as the

guide has. Use a wire width based on the above considerations.  You

don't need to be accurate as you draw this polygon as it is easier to

make it perfect in a second step.

 

Now, using the move command, move the segments of the polygon up against

the polygon guide. Hence the finished polygon will be the desired size.

 

All done. Change the grid back using GRID LAST if you wish.

 

As for the Youtube video. I don't think it showed what you suggest.

Maybe someone has a ULP that can shrink a polygon by the amount of the

wire width it's made of.

 

HTH

Warren

 

 

--

... use NNTP://news.cadsoft.de and a functional news reader like

Thunderbird!

... or http://www.eaglecentral.ca browser access to CadSoft EAGLE

support forums.

 

---

This email has been checked for viruses by Avast antivirus software.

https://www.avast.com/antivirus

 

 

  • Sign in to reply
  • Cancel
  • david_
    david_ over 9 years ago

    Hello.

     

    I wrote this post and then deleted it shortly after because I thought that I then found other threads about this and that my post would be one of those that there already exists answers for, I am so very happy you saw it though because your answer helped me very much(and those other threads didn't solve my problem at all in the end).

     

    Finding out that polygons is made out of many lines makes the situation much more comprehensible and now I do understand why I am not allowed to use a width of zero, I read some where that a 0 width value isn't actually 0 but some fraction of a µm(can't recall exactly) and it is beyond all common sense to make a polygon with such a size obviously.

     

    I think I am on my way away from Eagle heading for Kicad(not what I actually want to do but I feel it has become a necessity), maybe I can use the same technique there but in any case it feels very good to know of how I can deal with this situation and I have many pads to remake.

     

    Thank you very much.

     

    Regards