Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) track width change
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 189 subscribers
  • Views 1479 views
  • Users 0 members are here
Related

track width change

mrmarple
mrmarple over 9 years ago

Eagle (7.7.0) had me in a corner yesterday, couldn't work out why the auto

router wouldn't connect power and ground to a TQFP package, it showed air

wires for the omitted connections.

 

After some playing with the device, gnd@1, gnd@2, append, any/all etc. it

dawned on me that if air wires were being drawn, the device  and schematic

must be OK, it has be something board related causing the problem

 

It was, 20mil default track width good, 40mil power tracks bad, too wide

for TQFP pins.

 

My solution, auto route with 40mil power, then change to 20mil power and

run the auto router again, works a treat, if not very elegant.

 

My question, is there a correct/better way to change a track's net class to

achieve this?

 

Ken

--

EAGLE support forums at http://www.eaglecentral.ca :: Where the EAGLE community meets.

 

  • Sign in to reply
  • Cancel
Parents
  • rachaelp
    rachaelp over 9 years ago

    Hi Ken,

     

    Changing your net class rules so you can finish the routing isn't really the right way to do it in my opinion. Imagine, you come to make another change some weeks/months/years from now and you forget your changed the net class rule for the power. You press go on the auto router and it routes in a power trace much narrower than intended which for whatever reason goes unnoticed. You could end up with a problem on your board. Now, this may not be an issue for this situation because we have no knowledge of your circuit or requirements, but in general I would avoid doing things that could lead to errors at some point in the future.

     

    Now, what Gerald says above, using power/ground planes is good advice, but sometimes this isn't practical, especially if you are trying to use 1 or 2 layer boards, but it's worth noting, but this could also be an issue with other high current nets other that just power/ground.

     

    What I would say is that you maybe should reset your expectations for what the autorouter should be used for in reality. It is very rare that the auto router should be used for completely routing a board with no manual intervention, EAGLE's autorouter, as with pretty much every other vendors equivalent just aren't good enough to be able to do a complete board and have the finished result that would be 100% satisfactory, unless the board is really very simple e.g. a backplane with pretty much straight 1-to-1 routing.

     

    I think of the auto router more of a routing assistant, so you use it to quickly put in sets of nets which are easy and obvious to route and would otherwise just be a long winded click fest to do manually. It's actually rare that I would do this as I pretty much route everything manually, but on occasion I do if it's obvious that the router will do a good job and it'll save significant time.

     

    So back to your issue, I would sort out the breakout of the IC's manually first to get the traces out, decoupling caps connected up correctly with short traces etc and then try the auto router for the power/ground, then any other important signals and then finally the remainder of the board. I'd then go tidy up anything that was obviously messy from the autorouter and manually finish off anything it was unable to achieve.

     

    Best Regards,

     

    Rachael

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • rachaelp
    rachaelp over 9 years ago

    Hi Ken,

     

    Changing your net class rules so you can finish the routing isn't really the right way to do it in my opinion. Imagine, you come to make another change some weeks/months/years from now and you forget your changed the net class rule for the power. You press go on the auto router and it routes in a power trace much narrower than intended which for whatever reason goes unnoticed. You could end up with a problem on your board. Now, this may not be an issue for this situation because we have no knowledge of your circuit or requirements, but in general I would avoid doing things that could lead to errors at some point in the future.

     

    Now, what Gerald says above, using power/ground planes is good advice, but sometimes this isn't practical, especially if you are trying to use 1 or 2 layer boards, but it's worth noting, but this could also be an issue with other high current nets other that just power/ground.

     

    What I would say is that you maybe should reset your expectations for what the autorouter should be used for in reality. It is very rare that the auto router should be used for completely routing a board with no manual intervention, EAGLE's autorouter, as with pretty much every other vendors equivalent just aren't good enough to be able to do a complete board and have the finished result that would be 100% satisfactory, unless the board is really very simple e.g. a backplane with pretty much straight 1-to-1 routing.

     

    I think of the auto router more of a routing assistant, so you use it to quickly put in sets of nets which are easy and obvious to route and would otherwise just be a long winded click fest to do manually. It's actually rare that I would do this as I pretty much route everything manually, but on occasion I do if it's obvious that the router will do a good job and it'll save significant time.

     

    So back to your issue, I would sort out the breakout of the IC's manually first to get the traces out, decoupling caps connected up correctly with short traces etc and then try the auto router for the power/ground, then any other important signals and then finally the remainder of the board. I'd then go tidy up anything that was obviously messy from the autorouter and manually finish off anything it was unable to achieve.

     

    Best Regards,

     

    Rachael