Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Design block
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 188 subscribers
  • Views 1218 views
  • Users 0 members are here
Related

Design block

autodeskguest
autodeskguest over 9 years ago

Hi, So I made a few design blocks and dropped them into some test

designs. Is there anyway to link back the block to it's source? Can

design blocks be edited independently? If the design block was updated

somehow, how does one refresh that block in another project?

 

Glenn

 

  • Sign in to reply
  • Cancel
  • autodeskguest
    autodeskguest over 9 years ago in reply to rachaelp

    On 5/8/2017 5:55 AM, Rachael wrote:

    Hi Glenn,

     

    The way design blocks work I believe is basically using the existing

    ability to import one EAGLE design into another, but it's been re-packaged

    to make it a more polished feature. This seems to work quite well but it

    has the drawback that they are not actually reuse blocks that are tightly

    coupled with the designs they are used within. Once they are imported to a

    design then they are part of that design and changes can be made within

    that design which are independent of the source design block and cannot be

    back annotated. Similarly, if the source design block is updated then there

    is no method to update instances (as they are not actually separate

    instances referencing the source) of that block in any designs, the only

    way to update them is to delete them out and import them again I believe.

     

    Best Regards,

     

    Rachael

     

    Hi Rachael, so my questions might turn into a nice future enhancement

    then. image

     

    Thanks for the reply.

     

    Glenn

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rachaelp
    rachaelp over 9 years ago

    Hi Glenn,

     

    The way design blocks work I believe is basically using the existing

    ability to import one EAGLE design into another, but it's been re-packaged

    to make it a more polished feature. This seems to work quite well but it

    has the drawback that they are not actually reuse blocks that are tightly

    coupled with the designs they are used within. Once they are imported to a

    design then they are part of that design and changes can be made within

    that design which are independent of the source design block and cannot be

    back annotated. Similarly, if the source design block is updated then there

    is no method to update instances (as they are not actually separate

    instances referencing the source) of that block in any designs, the only

    way to update them is to delete them out and import them again I believe.

     

    Best Regards,

     

    Rachael

    --

    EAGLE support forums at http://www.eaglecentral.ca :: Where the EAGLE community meets.