Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) mystery air wire in my project
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 188 subscribers
  • Views 1174 views
  • Users 0 members are here
  • mystery air wire
Related

mystery air wire in my project

wilykat
wilykat over 9 years ago

https://www.dropbox.com/s/p0y0s7xhj8qqhb7/LED%20cube%20board.brd?dl=0 my current WIP at this point.

 

Can anyone explain the air wire between GND and VCC near the bottom?  Picture: https://imgur.com/on0AMd8 the pink arrow.  There's also a few yellow X's where the trace connects with decoupling capacitor pins, like Eagle doesn't know those traces are connected with capacitor's leg.

 

I don't have the schematic for this one, I got the original one from https://www.oshpark.com/shared_projects/LyWFDL0A   There was some mistakes with the original board, some grounds rails weren't connected, and the decoupling capacitor was in series between VCC rail and the chip's VCC pin, this would have isolated and prevented all 9 chips from getting power. I changed the caps so all VCC pins were connected directly to VCC rail, and the capacitor now connects from VCC to ground. Also fixed a couple missing ground connections to the 16 transistors and to ground pin of one of the chip.  It's almost like the previous person designed the board without using Eagle's schematic for some reason?  Oh and I added text of pin function with the 2 pin headers, marked all 9 chips, and noted all resistor (except one marked 330) and all capacitors are the same value 100 and 0.1uF

 

Anyway can someone double check that I don't have VCC and ground crossed and see why there's air wire trying to connect that 2?  It'd be around $60 down the drain if the board was useless because I missed something.

 

Still to do: replace 16 pin header with 12 as 4 of the pins aren't used and one pin (15) is in the way of the circuit trace.

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 9 years ago

    On 05/09/17 10:16, Eric Chapin wrote:

    Can anyone explain the air wire between GND and VCC near the bottom?  Picture: https://imgur.com/on0AMd8 the pink arrow.  There's also a few yellow X's where the trace connects with decoupling capacitor pins, like Eagle doesn't know those traces are connected with capacitor's leg.

     

     

    As Morten said, that via is associated with the upper trace net, not the

    one it's placed over. If you move the via you should see that the

    airwire follows it, whereas if you move the lower diagonal trace (and

    the unconnected end of the horizontal bit it doesn't connect to) the

    airwire will stay still.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 9 years ago

    On 05/09/17 10:16, Eric Chapin wrote:

    Can anyone explain the air wire between GND and VCC near the bottom?  Picture: https://imgur.com/on0AMd8 the pink arrow.  There's also a few yellow X's where the trace connects with decoupling capacitor pins, like Eagle doesn't know those traces are connected with capacitor's leg.

     

     

    As Morten said, that via is associated with the upper trace net, not the

    one it's placed over. If you move the via you should see that the

    airwire follows it, whereas if you move the lower diagonal trace (and

    the unconnected end of the horizontal bit it doesn't connect to) the

    airwire will stay still.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • wilykat
    wilykat over 9 years ago in reply to autodeskguest

    Yes I got it thank you.  I did manage to find one more sneaky airwire by typing in command "display none unrouted" which hid everything but unrouted.  All other unrouted are tiny and within the hole for component leg so it'd be connected when it's soldered in place.

     

    Checked top layer only for crossed lines, then checked bottom layer for crossed lines.   And finally ran error to find any more issue. Nearly all reported clearance issue with trace at vias and pads but those should be OK since they are supposed to be connected.  I didn't find any trace touching pad or vias where they aren't supposed to be.