Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Eagle 8.6.0 Issue with loading CAM files
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 188 subscribers
  • Views 1230 views
  • Users 0 members are here
Related

Eagle 8.6.0 Issue with loading CAM files

autodeskguest
autodeskguest over 8 years ago

Okay so you folks decided to revamp the whole cam interface ... fine but

I cannot seem to load older cam files - please tell me this is backwards

compatible?

 

It insists on calling it template_empty cam and all the layers names are

pooched

 

 

Attachments:
image
  • Sign in to reply
  • Cancel
  • autodeskguest
    autodeskguest over 8 years ago in reply to rachaelp

    Hi Rachael,

     

    On 2/5/2018 7:25 AM, rachaelp wrote:

    Yes it is backwards compatible. Next to where it says template_empty there is a button which pops up a menu which will allow you to load up your old CAM file. When you do it will put it under the Legacy section and in my tests all the layers etc all remain correctly named and pointing at the correct design layers.

     

    I had one older profile which reacted the way I posted, the others  I

    tried did have the correct layer names.

     

     

    You should just be able to run this as before and I believe it will use

    the old CAM processor. You won't of course get all the benefits of the

    new CAM processor which are Gerber X2 and it using polygons in the

    Gerber instead of raster fills which reduces Gerber size and cuts

    generation time dramatically.

     

    Okay - thanks for that info

     

     

    I think what you are seeing when you think all the layer names are "pooched" is the default template layer names. It tries to be helpful and load up a template which matches your board stackup when it first loads up. If you don't like it then change it and save it as a new style CAM job or just use your old one id you prefer. I created a new CAM job to replicate one of my old 10-layer jobs and it certainly is a lot quicker to output the job on a complex board.

     

     

    I wish it would show the cam filename instead of defaulting to

    template_empty.

     

    One thing to note though, make sure you choose the option to generate multiple drill files explicitly if your stackup has more than just through vias. You need to right click on the Drills section and choose the option called "Generate Excellon outputs based on PCB stackup". If you don't do this then you won't get anything than the through board drills generated.

     

    Thanks

     

     

     

    Best Regards,

     

    Rachael

     

    --

    To view any images and attachments in this post, visit:

    https://www.element14.com/community/message/234666

     

     

     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • rachaelp
    rachaelp over 8 years ago

    EDIT: Just saw your image (missed it at first read). I'm not sure why all your layers are messed up like that. What version of EAGLE was your old CAM file generated in? The CAM's I created in V7 seem to import fine.

     

    Yes it is backwards compatible. Next to where it says template_empty there is a button which pops up a menu which will allow you to load up your old CAM file. When you do it will put it under the Legacy section and in my tests all the layers etc all remain correctly named and pointing at the correct design layers. You should just be able to run this as before and I believe it will use the old CAM processor. You won't of course get all the benefits of the new CAM processor which are Gerber X2 and it using polygons in the Gerber instead of raster fills which reduces Gerber size and cuts generation time dramatically.

     

    I think what you are seeing when you think all the layer names are "pooched" is the default template layer names. It tries to be helpful and load up a template which matches your board stackup when it first loads up. If you don't like it then change it and save it as a new style CAM job or just use your old one id you prefer. I created a new CAM job to replicate one of my old 10-layer jobs and it certainly is a lot quicker to output the job on a complex board.

     

    One thing to note though, make sure you choose the option to generate multiple drill files explicitly if your stackup has more than just through vias. You need to right click on the Drills section and choose the option called "Generate Excellon outputs based on PCB stackup". If you don't do this then you won't get anything than the through board drills generated.

     

    Best Regards,


    Rachael

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 8 years ago

    On 05/02/18 05:25, Glenn Jones wrote:

    Okay so you folks decided to revamp the whole cam interface ... fine but

    I cannot seem to load older cam files - please tell me this is backwards

    compatible?

     

    It insists on calling it template_empty cam and all the layers names are

    pooched

     

    Hmm... I don't see the layer name corruption but I agree the renaming is

    annoying.