Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Re: Change pin name
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 0 replies
  • Subscribers 187 subscribers
  • Views 267 views
  • Users 0 members are here
Related

Re: Change pin name

autodeskguest
autodeskguest over 7 years ago

On 17/06/2019 13:41, s d wrote:

Hi everyone image

I'm switching from Altium and I'm trying to figure out what would be the best solution for this problem.

 

I have 2 LDO Regulator with exactly the same package but different PIN number distribution.

 

   

 

I've made a symbole but I'm wondering If I really do need 2 different symbole just to swap CE and the NC pin

 

 

I couldn't see whether you'd attached images because the element14 link

wasn't working, so I've just got your text of NNTP. However...

 

If the two regulators want the same schematic symbol, and have the same

physical package, then you can actually accommodate both in one library

device with one symbol and one footprint. The trick is to set up two

"variants" in the device, which will need different variant names, but

can both use the same package. Then the "connect" dialog will let you do

different pin-outs for them. I think some of the default libraries do

that - probably some transistor types.

 

However, it may prove easier to manage if you create two devices. You

still won't need more than the one symbol and one package, but using

separate devices makes the naming (and hence finding the right one to

add) slightly easier.