Dear All,
please feel free to share your experience with us on CadSoft Eagle so that engineers around the world can appreciate the simplicity yet powerful Cadsoft.
Cheers
Edmund
Dear All,
please feel free to share your experience with us on CadSoft Eagle so that engineers around the world can appreciate the simplicity yet powerful Cadsoft.
Cheers
Edmund
I think many many user need this tool too...
and we also need a tool to mark the board length, and the other thing... in the measure layer.
another question: how can I measure total length of the wire which I routed on a net ?
Hi,
there is an ULP that lists the lengh of all signals in the layout. See length.ulp for it.
To get more information about your board, just try statistic-brd.ulp. Currently there is no dimensioning tool in EAGLE.
-Richard
Now I've been able to have a go at them, the first one worked more as I would've liked it than the second (which only seemed to produce a rough statistic as to how many there are - the one that looked the most promising was the area consumed by the devices on the board).
The first one does appear to give me a surface area of how much would've been etched away *, and it does have some oddities when a trace goes over a via/pad - most of the time it appears to draw the trace to the centre of the via, but occasionally it'll draw the via with a hole in it. I haven't worked out what it does when though. This is by looking at the bitmaps it generates.
It's also a little slow - but I can understand that (interpreting binary files in the ULP language is going to be slow).
* Looking at the bitmaps, the "plane (Cu)" column appears to be related to the black area, rather than the white area - certainly bitmap ~~~0 has a lot of black, and gives 2092.07mm^2, and bitmap ~~~1 has not much black and gives 22.63mm^2 (there's a big grounding polygon over the area).
I'm guessing the algorithm is effectively converting it to a bitmap at 0.1mm per pixel and then counting the number of black pixels.
So, many thanks for that - although it's a bit too slow for interactive use, so I'll use it as a bit of experimentation so I can get a better idea based on visuals.
Just another ULP comes into my mind. Try statistic-brd.ulp that comes with the EAGLE installation.
Richard
Message was edited by: Richard Hammerl
Thanks for that, I'll take a look at it later (when I'm back home. I'm not sure if it's only the statistics for the polygon, or if it includes the traces, pads and via as well - will experiment).
I've been putting off installing an NNTP client on my machine
That might be the impetus I need to do so.
Hi Jason,
take a look at www.cadsoft.de/download.htm, ULP directory. ==> statistic-copper-plane.zip
This might help.
Suggestions should be posted in the CadSoft newsgroups directly. They can be accessed via news://news.cadsoft.de.
As far as I am informed these groups will become accessible via element-14 soon.
Richard
On a similar note, are there plans to show the area of copper used? (I try to maximise the amount of copper being used, so I don't have to etch as much off
. Sometimes, moving a component around does appear to make a difference, but it's difficult to say how much).
Also, is there an group for suggestions (this appears to be the only Eagle-based group, and the name doesn't seem well-suited to this).
There are plans to show the length of a track directly, but at the moment I can't tell you how it will look like. Maybe we will pack this information into the properties dialog (INFO command).
-Richard
There are plans to show the length of a track directly, but at the moment I can't tell you how it will look like. Maybe we will pack this information into the properties dialog (INFO command).
-Richard
Now I've been able to have a go at them, the first one worked more as I would've liked it than the second (which only seemed to produce a rough statistic as to how many there are - the one that looked the most promising was the area consumed by the devices on the board).
The first one does appear to give me a surface area of how much would've been etched away *, and it does have some oddities when a trace goes over a via/pad - most of the time it appears to draw the trace to the centre of the via, but occasionally it'll draw the via with a hole in it. I haven't worked out what it does when though. This is by looking at the bitmaps it generates.
It's also a little slow - but I can understand that (interpreting binary files in the ULP language is going to be slow).
* Looking at the bitmaps, the "plane (Cu)" column appears to be related to the black area, rather than the white area - certainly bitmap ~~~0 has a lot of black, and gives 2092.07mm^2, and bitmap ~~~1 has not much black and gives 22.63mm^2 (there's a big grounding polygon over the area).
I'm guessing the algorithm is effectively converting it to a bitmap at 0.1mm per pixel and then counting the number of black pixels.
So, many thanks for that - although it's a bit too slow for interactive use, so I'll use it as a bit of experimentation so I can get a better idea based on visuals.
Just another ULP comes into my mind. Try statistic-brd.ulp that comes with the EAGLE installation.
Richard
Message was edited by: Richard Hammerl
Thanks for that, I'll take a look at it later (when I'm back home. I'm not sure if it's only the statistics for the polygon, or if it includes the traces, pads and via as well - will experiment).
I've been putting off installing an NNTP client on my machine
That might be the impetus I need to do so.
Hi Jason,
take a look at www.cadsoft.de/download.htm, ULP directory. ==> statistic-copper-plane.zip
This might help.
Suggestions should be posted in the CadSoft newsgroups directly. They can be accessed via news://news.cadsoft.de.
As far as I am informed these groups will become accessible via element-14 soon.
Richard
On a similar note, are there plans to show the area of copper used? (I try to maximise the amount of copper being used, so I don't have to etch as much off
. Sometimes, moving a component around does appear to make a difference, but it's difficult to say how much).
Also, is there an group for suggestions (this appears to be the only Eagle-based group, and the name doesn't seem well-suited to this).