Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
Forum Share your experience with us on CadSoft Eagle
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 14 replies
  • Subscribers 192 subscribers
  • Views 1308 views
  • Users 0 members are here
  • eagle
Related

Share your experience with us on CadSoft Eagle

edmund
edmund over 16 years ago

Dear All,

 

please feel free to share your experience with us on CadSoft Eagle so that engineers around the world can appreciate the simplicity yet powerful Cadsoft.

 

Cheers

Edmund

  • Sign in to reply
  • Cancel
  • e14 Contributor
    e14 Contributor over 16 years ago in reply to Richard_H

    Now I've been able to have a go at them, the first one worked more as I would've liked it than the second (which only seemed to produce a rough statistic as to how many there are - the one that looked the most promising was the area consumed by the devices on the board).

     

    The first one does appear to give me a surface area of how much would've been etched away *, and it does have some oddities when a trace goes over a via/pad - most of the time it appears to draw the trace to the centre of the via, but occasionally it'll draw the via with a hole in it. I haven't worked out what it does when though. This is by looking at the bitmaps it generates.

     

    It's also a little slow - but I can understand that (interpreting binary files in the ULP language is going to be slow).


    * Looking at the bitmaps, the "plane (Cu)" column appears to be related to the black area, rather than the white area - certainly bitmap ~~~0 has a lot of black, and gives 2092.07mm^2, and bitmap ~~~1 has not much black and gives 22.63mm^2 (there's a big grounding polygon over the area).

     

    I'm guessing the algorithm is effectively converting it to a bitmap at 0.1mm per pixel and then counting the number of black pixels.

     

    So, many thanks for that - although it's a bit too slow for interactive use, so I'll use it as a bit of experimentation so I can get a better idea based on visuals.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Richard_H
    Richard_H over 16 years ago in reply to e14 Contributor

    Just another ULP comes into my mind. Try statistic-brd.ulp that comes with the EAGLE installation.

     

    Richard

     

    Message was edited by: Richard Hammerl

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 16 years ago in reply to Richard_H

    Thanks for that, I'll take a look at it later (when I'm back home. I'm not sure if it's only the statistics for the polygon, or if it includes the traces, pads and via as well - will experiment).

     

    I've been putting off installing an NNTP client on my machine image That might be the impetus I need to do so.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Richard_H
    Richard_H over 16 years ago in reply to e14 Contributor

    Hi Jason,

     

    take a look at www.cadsoft.de/download.htm, ULP directory. ==> statistic-copper-plane.zip

    This might help.

     

    Suggestions should be posted in the CadSoft newsgroups directly. They can be accessed via news://news.cadsoft.de.

    As far as I am informed these groups will become accessible via element-14 soon.

     

    Richard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 16 years ago in reply to Richard_H

    On a similar note, are there plans to show the area of copper used? (I try to maximise the amount of copper being used, so I don't have to etch as much off image. Sometimes, moving a component around does appear to make a difference, but it's difficult to say how much).

     

    Also, is there an group for suggestions (this appears to be the only Eagle-based group, and the name doesn't seem well-suited to this).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Richard_H
    Richard_H over 16 years ago in reply to huayuliang

    There are plans to show the length of a track directly, but at the moment I can't tell you how it will look like. Maybe we will pack this information into the properties dialog (INFO command).

     

    -Richard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • huayuliang
    huayuliang over 16 years ago in reply to Richard_H

    I think if when we use "SHOW" command to display a wire's length, it will be very easily for user.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Richard_H
    Richard_H over 16 years ago in reply to huayuliang

    Hi,

     

    there is an ULP that lists the lengh of all signals in the layout. See length.ulp for it.

    To get more information about your board, just try statistic-brd.ulp. Currently there is no dimensioning tool in EAGLE.

     

    -Richard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • huayuliang
    huayuliang over 16 years ago in reply to ellisgl

    I think many many user need this tool too...

     

    and we also need a tool to mark the board length, and the other thing... in the measure layer.

     

    another question: how can I measure total length of the wire which I routed on a net ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mywave82
    mywave82 over 16 years ago in reply to edmund
    Should be easy to write an ULP that dumps all trace-lengths.. But an UI element inside eagle would be nice aswell. Like one button "set start point", and as you then move the mouse cursor, it snaps to points on the relevant trace and displays distance, and calculated ohm, etc.
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
>