Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
Forum Using Net in Eagle
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 188 subscribers
  • Views 905 views
  • Users 0 members are here
  • eagle
Related

Using Net in Eagle

edmund
edmund over 16 years ago

Hi All,

 

am I right to say that the wire fucntion in Eagle is used to draw symbol in schematic sheet but when it is used in Board Level drawings, it acts like a Net. Correct me if I am wrong as if I am not mistaken, I saw that in Eagle Manual.

 

Cheers

Edmund

  • Sign in to reply
  • Cancel
Parents
  • Richard_H
    Richard_H over 16 years ago

    Hi Edmund,

     

    the WIRE command is meant to draw simple lines as for symbols or a frame in the schematic drawing. You can use it in any layer, even in layer Nets. If the wire starts and ends exactly in a pin's conection point and is drawn in layer Nets, it behaves like an electrical connection.

    But originally the NET is meant to draw  electrical connections. The benefit of NET is that the connection is always drawn in layer Nets. If you end a net at a pin connection point the net drops from the mouse cursor (a wire wouldn't). This indicates that the net is connected to the pin. Second option is that a junction (a connection point) is automtically set, if you connect two nets.

     

    The WIRE command in the board editor is meant to draw lines in any layer. It is possible to connect two pads with a WIRE if it begins and ens exactly in the pads/smds origin, but the correct way is to use the ROUTE command, provided that you have drawn a schemtic before and that there are already signals (airwires) connecting pads/smds in your layout. ROUTE grabs/jumps automtically into the center of the pad/smd and so we are sure to have a well-defined connection between them.

    If you don't have a schematic and started designing only a  board, you can use the SIGNAL command first to establish the connection (airwires) between your components. Then use ROUTE for laying out the tracks.

     

     

    Hope this info helps.

    Richard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • edmund
    edmund over 16 years ago in reply to Richard_H

    Dear Richard,

     

    thanks for the reply. But I am confused by the Eagle Tutorial Page 27 which states the following point:

     

    Do not use the WIRE command to draw net or bus lines in the schematic.
    Use NET or BUS instead!


    Use ROUTE and not WIRE to dissolve airwires to tracks in the Layout
    editor. Otherwise EAGLE would not set vias automatically when changing
    signal layers.

     

    But from your reply. you were saying that " If the wire starts and ends exactly in a pin's conection point and is drawn in layer Nets, it behaves like an electrical connection."

     

     

    Please do enlighten me on this and appreciate your efforts.

     

    Cheers

    Edmund

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • edmund
    edmund over 16 years ago in reply to Richard_H

    Dear Richard,

     

    thanks for the reply. But I am confused by the Eagle Tutorial Page 27 which states the following point:

     

    Do not use the WIRE command to draw net or bus lines in the schematic.
    Use NET or BUS instead!


    Use ROUTE and not WIRE to dissolve airwires to tracks in the Layout
    editor. Otherwise EAGLE would not set vias automatically when changing
    signal layers.

     

    But from your reply. you were saying that " If the wire starts and ends exactly in a pin's conection point and is drawn in layer Nets, it behaves like an electrical connection."

     

     

    Please do enlighten me on this and appreciate your efforts.

     

    Cheers

    Edmund

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • edmund
    edmund over 16 years ago in reply to Richard_H

    Dear Richard,

     

    thanks for the great information. Now I get what you mean.

     

    Thanks for the insight.

     

    Appreciate that.

     

    Cheers

    Edmund

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Richard_H
    Richard_H over 16 years ago in reply to edmund

    Hello Edmund,

     

    NET in the schematic and ROUTE in the board offer some simple benefits compared to WIRE.

     

    NET:

    It is always in the Nets layer - you don't have to care about the layer you draw in

    The line width is always the same - you don't have to care about

    Ending a net exactly in the pin connection point let the net drop from the mouse cursor - you can be sure that the connection is established

    Connecting two nets results in a junctino - you can be sure that your schematic is proper readable

     

    We do not forbid to use the WIRE command,  we strongly recommend to use NET. It makes things easier and gives more reliability in what you do.

    It's less error-prone.

     

    The same with ROUTE:

    The trace always begins and ends in the center of the pad or SMD - you don't have to care about grid

    You can use the magnetic pads functionality - results in a proper layout

    If you change layers, vias will be set automatically - you don't have to deal with them separately

    The same as in the schematic here. ROUTE offers benefits and assurance.

     

     

    Richard