Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
Forum Have a question about CadSoft EAGLE?  Ask our Expert, Richard! (Archive)
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1129 replies
  • Subscribers 245 subscribers
  • Views 51380 views
  • Users 0 members are here
  • eagle
  • expert
  • richard_hammerl
  • cadsoft
Related

Have a question about CadSoft EAGLE?  Ask our Expert, Richard! (Archive)

nlarson
nlarson over 16 years ago

This thread is now locked - but you can still ask Richard by posting your questions here.  If you'd rather browse other member's questions you can read the CadSoft EAGLE Forums for past questions and answers. Enjoy!

 

Browse past Q&A help on anything technical relating to CadSoft EAGLE!


image

 

Richard Hammerl

Richard is an engineer with 16 years experience in EAGLE customer support and is waiting for your questions.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 15 years ago

    I have a situation here that I have not encountered before...and I have made dozens of library devices/packages/symbols with no problem until now.  I made a new package (a Bluetooth module) and new symbol, but when I try to use "New" package in making the device, it seems to default to a 0805 SMD package (shows in the window), the rest of the list is grayed out, and when I try to select something, it comes back with error message of not enough pins on package (no kidding!).

     

    No packages are shown as defined for this device and it will not allow me to place the symbol in a .sch (says no package).  I've tried deleting the .dev file and started anew, no change.

     

    Any suggestions?  Thanks...

     

    Using Linux version 5.11.0 professional.

     

    Don

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Richard_H
    Richard_H over 15 years ago in reply to e14 Contributor

    azark7 wrote:

     

    ........., but when I try to use "New" package in making the device, it seems to default to a 0805 SMD package (shows in the window), the rest of the list is grayed out, and when I try to select something, it comes back with error message of not enough pins on package (no kidding!).

     

     

    Hi Don,

     

    if a package has not enough pads or smds that you can connect all the pins of the symbol EAGLE does not allow to use such a package. this is the reason why the package listed are not selectable.

    Could you please send me the library file by private email to support@cadsoft.de ? So I could take a look into it.

     

    Regards,

    Richard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Richard_H
    Richard_H over 15 years ago in reply to e14 Contributor

    azark7 wrote:

     

    ........., but when I try to use "New" package in making the device, it seems to default to a 0805 SMD package (shows in the window), the rest of the list is grayed out, and when I try to select something, it comes back with error message of not enough pins on package (no kidding!).

     

     

    Hi Don,

     

    if a package has not enough pads or smds that you can connect all the pins of the symbol EAGLE does not allow to use such a package. this is the reason why the package listed are not selectable.

    Could you please send me the library file by private email to support@cadsoft.de ? So I could take a look into it.

     

    Regards,

    Richard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to Richard_H

    Thanks Richard ... no need to send you the file as I've found the problem ... it was a case of 35 pins defined in the symbol and 34 pins in the package, due mainly (besides my oversight) to the data sheet for the part showing a NC pin in the pin list but no pad for it in the suggested footprint. Quite frustrating to find this the first time, would suggest some kind of more intelligent error message.

     

    Regards,

    Don